Test mode#
There is an alternate way to test CS feature that does not require a BLE connection to be established between the boards. This is called “test mode”, and it relies on the LE_CS_Test HCI command from the standard.
Hardware setup#
This mode requires that both boards are connected to the controller PC to collect and combine data from both initiator and reflector.
Parent topic:Test mode
Operating test mode#
This chapter provides information on how to use wireless application in test mode.
Using Python host application#
When using test mode from Python host application, the following parameter must be added to the command:
--testmode
Parent topic:Operating test mode
Using the console#
To start the measurement on the reflector side:
\> test rx
To start the measurement on the initiator side:
\> test tx
Both devices synchronize to each other and perform a CS test procedure using default settings.
The expected output (on both devices) is a JSON-like structure similar to the following:
items:[{hadm:{cfg:{rtyp:0,rphy:0,txpwr:0,fcs:150,ip1:145,ip2:145,tpm:20,ant:7},sts:0,stp:{nb:101,md:'00022221222212222122221222212222122221222212222122221222212222122221222212222122221222212222122221222',ch:'0001020001020303040506070708090A0B0B0C0D0E0F0F1011121313141516171718191A1B1B1C1D1E1F1F2021222323242526272728292A2B2B2C2D2E2F2F3031323333343536373738393A3B3B3C3D3E3F3F4041424343444546474748494A4B4B4C4D4E',evt:'00',se:'65'}},md0:{cfg:{n_stp:3},init:{r:'808080',c:'800080008000'},refl:{r:'5A555D',c:'7FFF7FFF7FFF'}},mciq:{cfg:{n_ap:4,n_stp:79},refl:{i:['lMjijwmvkNmoZOjCmxkglIcvkIZebvgqiMnAZGj1eFb+l1ZbjSkIljmMhDcgmEe9mQbNfTegk8azh1aWfFcvmEdobceLe8iEizfle1lWcCbYg1eWdKdRZtgeiqcrZ6hSgtdGlbeVhelSazfdg6lRjvjic3i3kT','kBgKgOj6gzkacUjpkUkJhmf4g4cEcGiKfQj0c9kChpgDh6b/kik4iJjjeDbakFhKlCdVeKgBkHdPiMb/gqfOkJf/eIdVd0iogzgxeLkEd9djhHeTdtfLcmhNgafUcuh/fKfcjfd9fyjUcvgufVi/iyiudXgwiT','XVmVmLdZlUbKhgWvb+XfkDZcltiaohXLnMdHgiYiYzakifhdZcaIjRhtmolXiSZIgtaanBYicyaoZVheYTYofaYWZhmdm9Zon9X/nZeZYhZUYam3l3YVeYY6nVY8efaNmjZZgnksmMhDfQaRlvihe3e5hglOkE','w6X7X8oYaZr/Y4xKrBwtcyoVZyX1PYvAVKpBa6wTr5m6fyX4vovEeyijTtRXiksimrkiRqsJs/i0u+UtsPoWpfqRlMRzR9uQW5srSEq8mSkUtNSaSlpUaXsMW2n+bdr9VFoMmPU8WdlVaWp+WUimnXneYZY8dl',],q:['bGmDlwgNlUegfHZ3exa1kfaMlMf5lHZSmlfnepaKZdaojTgVaWa/jThwmXlYh9ZwffcCmLaDcYcwaIiYZ7ateQaJbtl+mIaHlpZzmFdAbVb4ZymIltaTgVZvluaxfiaGl7bBeQlbldeLiBailXfZcdcdjtjthX','ezkUkdiSkfhFdcdYhUeUkNbhkceDh3cYkNh6dEebb6bdkVdZeKeukvj6lBiyjea2hhbpkobVeRc4cfgkcCcBgWbzcKjdj2cgkXbvj7e1cfc7cWjWi3cjfWc1jbcpezdIjbcjgGixjagBgOc6jGgse8e0hbi7h+','bvY4YwW4YMX6pZeCXecAXmmpYnpAjeh1bBYCoSc4jXloY2nUdCcHZ9ZffTkGZpgGZDkiiNgZZNlYcYnifpieYRhNkJkUjpbUeleRjwX4jjkwdNkFlRhMniddfChkm/cIiAg1ZikchXZ0mPdniYafaQadlRfxdI','kJvVvUvHwTsbQVfKtDjLwpRRvzRPdlYsslt6QViLUyRYwDSZhMjivNu1oYeVujYHtaRvkgXHnpRjePWZXmT5rIVzSmhuive6rBZdi7pKTWSrb2hhe9WlUTcLorWgUtfFkcX6pdfXlWpbXEdFjNpqmamGaUmMpA',],tqi:['00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000','00000000000000000000000000000000000000000000000200000000000000000000000000020202000000000000000000000000000000000000000000000000000000000000000000000000000000','00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000','00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000',],},},tof:{cfg:{n_stp:19},refl:{d:'AP+AAP+EAP+NAP+YAP+hAP+qAP+vAP/BAP/DAP/RAP/YAP/kAP/oAP/yAAAAAAAIAAASAAAVAAAl',r:'625A565C6159585A6159565B6059545A5E5853',nadm:'FFFFFFFFFFFFFFFFFFF'},},info:{init:{},refl:{syn:0,syg:0,syr:0,syc:0,f:0x0000,x:0,ta:0,te:0,},},},]
CRC32:17002f48
marker:[DONE]
It contains all the CS results returned locally by HCI events and debug data, but does not show the final distance. In this mode, the host PC can only compute the final distance.
See Command response for how to interpret these results.
Parent topic:Operating test mode
Parent topic:Test mode
Parent topic:Appendices