MCUXpresso SDK Documentation

Operating test mode

Operating test mode#

This chapter provides information on how to use wireless application in test mode.

Using Python host application#

When using test mode from Python host application, the following parameter must be added to the command:

--testmode

Parent topic:Operating test mode

Using the console#

To start the measurement on the reflector side:

\> test rx

To start the measurement on the initiator side:

\> test tx

Both devices synchronize to each other and perform a CS test procedure using default settings.

The expected output (on both devices) is a JSON-like structure similar to the following:

items:[{hadm:{cfg:{rtyp:0,rphy:0,txpwr:0,fcs:150,ip1:145,ip2:145,tpm:20,ant:7},sts:0,stp:{nb:101,md:'00022221222212222122221222212222122221222212222122221222212222122221222212222122221222212222122221222',ch:'0001020001020303040506070708090A0B0B0C0D0E0F0F1011121313141516171718191A1B1B1C1D1E1F1F2021222323242526272728292A2B2B2C2D2E2F2F3031323333343536373738393A3B3B3C3D3E3F3F4041424343444546474748494A4B4B4C4D4E',evt:'00',se:'65'}},md0:{cfg:{n_stp:3},init:{r:'808080',c:'800080008000'},refl:{r:'5A555D',c:'7FFF7FFF7FFF'}},mciq:{cfg:{n_ap:4,n_stp:79},refl:{i:['lMjijwmvkNmoZOjCmxkglIcvkIZebvgqiMnAZGj1eFb+l1ZbjSkIljmMhDcgmEe9mQbNfTegk8azh1aWfFcvmEdobceLe8iEizfle1lWcCbYg1eWdKdRZtgeiqcrZ6hSgtdGlbeVhelSazfdg6lRjvjic3i3kT','kBgKgOj6gzkacUjpkUkJhmf4g4cEcGiKfQj0c9kChpgDh6b/kik4iJjjeDbakFhKlCdVeKgBkHdPiMb/gqfOkJf/eIdVd0iogzgxeLkEd9djhHeTdtfLcmhNgafUcuh/fKfcjfd9fyjUcvgufVi/iyiudXgwiT','XVmVmLdZlUbKhgWvb+XfkDZcltiaohXLnMdHgiYiYzakifhdZcaIjRhtmolXiSZIgtaanBYicyaoZVheYTYofaYWZhmdm9Zon9X/nZeZYhZUYam3l3YVeYY6nVY8efaNmjZZgnksmMhDfQaRlvihe3e5hglOkE','w6X7X8oYaZr/Y4xKrBwtcyoVZyX1PYvAVKpBa6wTr5m6fyX4vovEeyijTtRXiksimrkiRqsJs/i0u+UtsPoWpfqRlMRzR9uQW5srSEq8mSkUtNSaSlpUaXsMW2n+bdr9VFoMmPU8WdlVaWp+WUimnXneYZY8dl',],q:['bGmDlwgNlUegfHZ3exa1kfaMlMf5lHZSmlfnepaKZdaojTgVaWa/jThwmXlYh9ZwffcCmLaDcYcwaIiYZ7ateQaJbtl+mIaHlpZzmFdAbVb4ZymIltaTgVZvluaxfiaGl7bBeQlbldeLiBailXfZcdcdjtjthX','ezkUkdiSkfhFdcdYhUeUkNbhkceDh3cYkNh6dEebb6bdkVdZeKeukvj6lBiyjea2hhbpkobVeRc4cfgkcCcBgWbzcKjdj2cgkXbvj7e1cfc7cWjWi3cjfWc1jbcpezdIjbcjgGixjagBgOc6jGgse8e0hbi7h+','bvY4YwW4YMX6pZeCXecAXmmpYnpAjeh1bBYCoSc4jXloY2nUdCcHZ9ZffTkGZpgGZDkiiNgZZNlYcYnifpieYRhNkJkUjpbUeleRjwX4jjkwdNkFlRhMniddfChkm/cIiAg1ZikchXZ0mPdniYafaQadlRfxdI','kJvVvUvHwTsbQVfKtDjLwpRRvzRPdlYsslt6QViLUyRYwDSZhMjivNu1oYeVujYHtaRvkgXHnpRjePWZXmT5rIVzSmhuive6rBZdi7pKTWSrb2hhe9WlUTcLorWgUtfFkcX6pdfXlWpbXEdFjNpqmamGaUmMpA',],tqi:['00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000','00000000000000000000000000000000000000000000000200000000000000000000000000020202000000000000000000000000000000000000000000000000000000000000000000000000000000','00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000','00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000',],},},tof:{cfg:{n_stp:19},refl:{d:'AP+AAP+EAP+NAP+YAP+hAP+qAP+vAP/BAP/DAP/RAP/YAP/kAP/oAP/yAAAAAAAIAAASAAAVAAAl',r:'625A565C6159585A6159565B6059545A5E5853',nadm:'FFFFFFFFFFFFFFFFFFF'},},info:{init:{},refl:{syn:0,syg:0,syr:0,syc:0,f:0x0000,x:0,ta:0,te:0,},},},]
CRC32:17002f48
marker:[DONE]

It contains all the CS results returned locally by HCI events and debug data, but does not show the final distance. In this mode, the host PC can only compute the final distance.

See Command response for how to interpret these results.

Parent topic:Operating test mode

Parent topic:Test mode