CS Wireless Ranging Demo Application User Guide# Table of Contents Introduction Requirements Hardware and software requirements Toolchain requirements Wireless ranging demo application setup Hardware set up with single antenna configuration Hardware set up with antenna diversity Firmware setup Serial console setup Python host application setup Running wireless ranging demo application Using the console Configuring the ranging service client Triggering one CS measurement Changing CS configuration Using Python host application Application parameters Performing CS measurements with only step mode 2’s Performing distance estimation using mode 2’s as main mode and mode 1 as submode Configuring embedded algorithms Troubleshooting Embedded firmware command reference Firmware shell commands Command syntax Implicit commands Command response Boot message Main menu “parameter” - CS parameters “ch_list” parameter “timings” – CS timings configuration “system” – system commands “misc” – miscellaneous commands Firmware response interpretation Appendices Test mode Hardware setup Operating test mode Using Python host application Using the console Wireless ranging and channel sounding standardization Acronyms Related documentation Note about the source code in the document Revision history