Pixel buffers
This chapter provides an overview of the pixel buffer alignment, cache, internal representation, enumerations, structures, and functions.
Pixel buffer alignment
The VGLite hardware requires the pixel buffer start address and stride to be properly byte-aligned to work correctly. The start address and stride alignment requirement for a pixel buffer depends on the specific pixel format, and gcFEATURE_VG_16PIXELS_ALIGNED value (0/1) in vg_lite_options.h file.
Parent topic:Pixel buffers
Pixel cache
The Vivante Imaging Engine (IM) includes two fully associative caches. Each cache has 8 lines. Each line has 64 bytes. In this case, one cache line can hold either a 4x4-pixel tile or a 16x1-pixel row.
Parent topic:Pixel buffers
Internal representation
For non-32-bit color formats, each pixel is extended to 32 bits as follows:
If the source and destination formats have the same color format, but differ in the number of bits per color channel, the source channel is multiplied by (2d- 1)/(2s– 1) and is rounded to the nearest integer, where:
d is the number of bits in the destination channel
s is the number of bits in the source channel
Example: a b11111 5-bit source channel gets converted to an 8-bit destination b11111000.
The YUV formats are internally converted to RGB. The pixel selection is unified for all formats by using the LSB of the coordinate.
Parent topic:Pixel buffers
Pixel buffer enumerations
This section provides an overview of the pixel buffer enumerations.
vg_lite_buffer_format_t enumeration
This enumeration specifies the color format to use for a buffer. This applies to both image and Render Target. Formats include supported swizzles for RGB. For YUV swizzles, use the related values and parameters in vg_lite_swizzle_t.
The application shall use the vg_lite_query_feature API to determine support for some hardware-specific formats. For example, related vg_lite_feature_t enum values include gcFEATURE_BIT_VG_RGBA2_FORMAT and gcFEATURE_BIT_VG_IM_INDEX_FORMAT.
(Alignment columns refined March and Sept 2023)
Used in structure: vg_lite_buffer_t.
See also vg_lite_blit, vg_lite_clear, vg_lite_draw.
Attention: OpenVG VGImageFormat Note: The bits for each color channel are stored within a machine word from MSB to LSB in the order indicated by the pixel format name. This is the opposite of the original VG_LITE_* formats that are ordered from LSB to MSB. The formats with the same organization are listed in the same row as their VG_Lite counterparts.
Attention: Original VGLite API Image Format Note: The bits for each color channel are stored within a machine word from LSB to MSB in the order indicated by the pixel format name. This is the opposite of the OPENVG VG_* formats that are ordered from MSB to LSB.
The following codes, as also used in OpenVG 1.1 Specification Table 11, are used for format description:
A - Alpha channel
B - Blue color channel
G - Green color channel
R - Red color channel
X - Uninterpreted padding byte or bit
L - Grayscale
BW - 1-bit black and white
l - Linear color space
s - Non-linear (sRGB) color space
PRE - Alpha values are premultiplied
vg_lite_buffer_format_t String Value |
Description |
Supported as source |
Supported as destination |
Start address/ Stride alignment: bytes |
|---|---|---|---|---|
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 64B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
No |
Start 4B / Stride 32B |
|
|
Yes |
No |
Start 4B / Stride 8B |
|
|
Yes |
Yes |
Start 4B / Stride 16B |
|
|
Yes |
Yes |
Start 4B / Stride 16B |
Hardware-dependent formats for vg_lite_buffer_format_t |
Description |
Supported as source |
Supported as destination |
Alignment (bytes) |
|---|---|---|---|---|
|
|
Yes |
Yes |
Start 4B / Stride 16B |
|
|
Yes |
Yes |
Start 4B / Stride 16B |
|
|
Yes |
Yes |
Start 4B / Stride 16B |
|
|
Yes |
No |
8B |
|
1-bit index format |
Yes |
No |
8B |
|
2-bit index format |
Yes |
No |
both 8B |
|
4-bit index format |
Yes |
No |
both 8B |
|
8-bit index format |
Yes |
No |
both 16B |
|
|
Yes |
No |
Y: both 16 Bytes UV: both 8 Bytes |
|
|
Yes |
No |
A, Y: both 16 Bytes UV: both 8 Bytes |
|
|
Yes |
No |
both 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
|
|
|
Yes |
Yes |
|
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
|
|
Yes |
Yes |
Start 4B / Stride 32B |
Parent topic:Pixel buffer enumerations
Image buffer alignment requirement
The image (or source) buffer alignment requirement depends on the specific pixel format, and some gcFEATURE_*_ALIGNED defines in the vg_lite_options.h file.
Image format |
Bits per pixel |
Source tile mode |
Start address alignment requirement in bytes |
Stride alignment requirement in bytes |
Buffer height alignment requirement |
Supported for destination |
|---|---|---|---|---|---|---|
VG_LITE_INDEX1 |
1 |
linear |
8B |
2B |
1 |
|
VG_LITE_INDEX1 |
1 |
tile |
8B |
1B |
4 |
|
VG_LITE_INDEX2 |
2 |
linear |
8B |
4B |
1 |
|
VG_LITE_INDEX2 |
2 |
tile |
8B |
1B |
4 |
|
VG_LITE_INDEX4 |
4 |
linear |
8B |
8B |
1 |
|
VG_LITE_INDEX4 |
4 |
tile |
8B |
2B |
4 |
|
VG_LITE_INDEX8 |
8 |
linear |
16B |
16B |
1 |
|
VG_LITE_INDEX8 |
8 |
tile |
16B |
4B |
4 |
|
VG_LITE_A4 |
4 |
linear |
8B |
8B |
1 |
|
VG_LITE_A4 |
4 |
tile |
8B |
2B |
4 |
|
VG_LITE_A8 |
8 |
linear |
16B |
16B |
1 |
Yes |
VG_LITE_A8 |
8 |
tile |
16B |
4B |
4 |
Yes |
VG_LITE_L8 |
8 |
linear |
16B |
16B |
1 |
Yes |
VG_LITE_L8 |
8 |
tile |
16B |
4B |
4 |
Yes |
VG_LITE_ARGB2222 |
8 |
linear |
16B |
16B |
1 |
Yes |
VG_LITE_ARGB2222 |
8 |
tile |
16B |
4B |
4 |
Yes |
VG_LITE_RGB565 |
16 |
linear |
32B |
32B |
1 |
Yes |
VG_LITE_RGB565 |
16 |
tile |
32B |
8B |
4 |
Yes |
VG_LITE_ARGB1555 |
16 |
linear |
32B |
32B |
1 |
Yes |
VG_LITE_ARGB1555 |
16 |
tile |
32B |
8B |
4 |
Yes |
VG_LITE_ARGB4444 |
16 |
linear |
32B |
32B |
1 |
Yes |
VG_LITE_ARGB4444 |
16 |
tile |
32B |
8B |
4 |
Yes |
VG_LITE_ARGB8888 |
32 |
linear |
64B |
64B |
1 |
Yes |
VG_LITE_ARGB8888 |
32 |
tile |
64B |
16B |
4 |
Yes |
VG_LITE_XRGB8888 |
32 |
linear |
64B |
64B |
1 |
Yes |
VG_LITE_XRGB8888 |
32 |
tile |
64B |
16B |
4 |
Yes |
VG_LITE_ARGB8565 |
24 |
linear |
64B |
48B* |
1 |
Yes |
VG_LITE_ARGB8565 |
24 |
tile |
64B |
12B* |
4 |
Yes |
VG_LITE_RGB888 |
24 |
linear |
64B |
48B* |
1 |
Yes |
VG_LITE_RGB888 |
24 |
tile |
64B |
12B* |
4 |
Yes |
VG_LITE_YUY2/UYVY |
16 |
linear |
32B |
32B |
1 |
|
VG_LITE_YUY2/UYVY |
16 |
tile |
32B |
8B |
4 |
|
VG_LITE_NV12 |
12 |
linear |
Y: 32B UV: 32B |
Y: 32B UV: 32B |
1 |
|
VG_LITE_YV12 |
12 |
linear |
Y: 32B U: 16B V: 16B |
Y: 32B U: 16B V: 16B |
1 |
|
VG_LITE_NV16 |
16 |
linear |
Y: 32B UV: 32B |
Y: 32B UV: 32B |
1 |
|
VG_LITE_YV16 |
16 |
linear |
Y: 32B U: 16B V: 16B |
Y: 32B U: 16B V: 16B |
1 |
|
VG_LITE_YV24 |
24 |
linear |
Y: 32B U: 32B V: 32B |
Y: 32B U: 32B V: 32B |
1 |
|
VG_LITE_ETC2 |
8 |
tile |
16B |
4B |
4 |
Note:
The values in the table reflect the alignment requirements of the data in memory. The stride of ARGB8888 / ARGB8565 is seen as 4Byte per pixel when configuring the hardware.
For tile mode, the stride is still the byte size of a row of pixels in the buffer instead of 4 rows.
When DECNano function is enabled for the buffer, the total buffer size need align to 64Byte*compression rate for ARGB8888 or XRGB8888 format, align to 48Byte*compress rate for RGB888 format.
Additional Alignment Requirement
Buffer starting address must be 16 pixel-byte-size aligned, that is 8 bit-per-pixel format buffer must be 16 bytes aligned; 16 bit-per-pixel format buffer must be 32 bytes aligned; 24 and 32 bit-per-pixel format buffer must be 64 bytes aligned.
For linear mode buffer, the buffer stride must be 16 pixel-byte-size aligned.
For tile mode buffer, buffer width and height must be 4 pixel aligned so buffer width and height end at tile boundary.
Parent topic:Pixel buffer enumerations
Destination buffer alignment requirement
The destination (or render target) buffer alignment requirement depends on the specific pixel format, and some gcFEATURE_*_ALIGNED defines in the vg_lite_options.h file.
Target format |
Bits per pixel |
Target tile mode |
VG tile mode |
Start address alignment requirement in bytes |
Stride alignment requirement in bytes |
Buffer height alignment requirement |
|---|---|---|---|---|---|---|
VG_LITE_A8 |
8 |
linear |
linear |
4B |
1B |
1 |
VG_LITE_A8 |
8 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_A8 |
8 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_A8 |
8 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_L8 |
8 |
linear |
linear |
4B |
1B |
1 |
VG_LITE_L8 |
8 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_L8 |
8 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_L8 |
8 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_ARGB2222 |
8 |
linear |
linear |
4B |
1B |
1 |
VG_LITE_ARGB2222 |
8 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_ARGB2222 |
8 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_ARGB2222 |
8 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_RGB565 |
16 |
linear |
linear |
4B |
2B |
1 |
VG_LITE_RGB565 |
16 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_RGB565 |
16 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_RGB565 |
16 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_ARGB1555 |
16 |
linear |
linear |
4B |
2B |
1 |
VG_LITE_ARGB1555 |
16 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_ARGB1555 |
16 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_ARGB1555 |
16 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_ARGB4444 |
16 |
linear |
linear |
4B |
2B |
1 |
VG_LITE_ARGB4444 |
16 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_ARGB4444 |
16 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_ARGB4444 |
16 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_ARGB8888 |
32 |
linear |
linear |
4B |
4B |
1 |
VG_LITE_ARGB8888 |
32 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_ARGB8888 |
32 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_ARGB8888 |
32 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_XRGB8888 |
32 |
linear |
linear |
4B |
4B |
1 |
VG_LITE_XRGB8888 |
32 |
linear |
tile |
64B |
64B |
4 |
VG_LITE_XRGB8888 |
32 |
tile |
linear |
64B |
64B |
4 |
VG_LITE_XRGB8888 |
32 |
tile |
tile |
64B |
16B |
4 |
VG_LITE_ARGB8565 |
24 |
linear |
linear |
64B |
3B* |
1 |
VG_LITE_ARGB8565 |
24 |
linear |
tile |
64B |
48B* |
4 |
VG_LITE_ARGB8565 |
24 |
tile |
linear |
64B |
48B* |
4 |
VG_LITE_ARGB8565 |
24 |
tile |
tile |
64B |
12B* |
4 |
VG_LITE_RGB888 |
24 |
linear |
linear |
64B |
3B* |
1 |
VG_LITE_RGB888 |
24 |
linear |
tile |
64B |
48B* |
4 |
VG_LITE_RGB888 |
24 |
tile |
linear |
64B |
48B* |
4 |
VG_LITE_RGB888 |
24 |
tile |
tile |
64B |
12B* |
4 |
Note:
The values in the table reflect the alignment requirements of pixel data in memory. The stride of ARGB8888/ARGB8565 is seen as 4 Bytes per pixel when configuring the hardware.
For tile mode, the buffer stride is still the byte size of a row of pixels instead of 4 rows of pixels.
For PE clear function, the clear size must align to 48 Bytes for the RGB888 or ARGB8565 format.
For PE clear function with DECNano enabled, the clear size must align to 48 Bytes for RGB888, align to 64 Bytes for ARGB8888 or XRGB8888.
If the DECNano function is enabled for the buffer, the target buffer start address needs to align to 64 Bytes.
If the DECNano function is enabled for the buffer, the total buffer size needs to align to a 64-byte compression rate for ARGB8888 or XRGB8888 format and align to a 48 Byte*compression rate for RGB888 format.
Additional Alignment Requirement
Buffer starting address must be at least 4-byte aligned. Buffer stride must be at least one pixel size aligned.
Buffer starting address must be 64-byte aligned for 24 bit-per-pixel format, or tile mode, or DECNano enabled.
Buffer height must be 4-pixel aligned for tile mode buffer.
For tile mode buffer, the buffer stride must be 16-byte aligned for non-24bit-per-pixel formats. So, 8 bits-per-pixel format buffer width must be 16-pixel aligned; 16 bits-per-pixel format buffer width must be 8-pixel aligned; 32 bit-per-pixel format buffer width must be 4 pixel aligned.
For tile mode buffer, the buffer stride must be 12-byte aligned for 24 bits-per-pixel formats, that is, the buffer width must be 4-pixel aligned.
For PE clear function, the clear size must align to 48 Bytes for 24-bits-per-pixel formats.
For PE clear function with DECNano enabled, the clear size must align to 48 Bytes for 24 bits-per-pixel formats and align to 64 Bytes for 32 bits-per-pixel formats.
If source buffer tile mode is different from destination buffer tile mode, buffer starting address must be 64 Byte aligned, buffer stride must be 64 Byte aligned for non-24 bits-per-pixel formats, buffer stride must be 48-Byte aligned for 24 bits-per-pixel formats.
VGLite hardware requires the raster image width to be a multiple of 16 pixels for linear gradient and radial gradient operations. This requirement applies to all image formats. Therefore, the user must pad an arbitrary image width to a multiple of 16 pixels for VGLite linear gradient and radial gradient APIs.
Parent topic:Pixel buffer enumerations
vg_lite_buffer_layout_t enumeration
Specifies the buffer data layout in memory.
Used in structure: vg_lite_buffer.
vg_lite_buffer_layout_t String Value |
Description |
|---|---|
|
Linear (scanline) layout. |
|
Data is organized in 4x4 pixel tiles. Note: for this layout, the buffer start address and stride must be 64-byte aligned |
Parent topic:Pixel buffer enumerations
vg_lite_compress_mode_t enumeration
Specifies the DECNano comprssion mode. (from March 2023)
Used in structure: vg_lite_buffer_t.
vg_lite_compress_mode_t string value |
Description |
|---|---|
|
Disable compression. |
|
compression ratio is 1.6 for ARGB8888, 2.0 for XRGB8888 |
|
compression ratio is 2.0 for ARGB8888, 2.6 for XRGB8888 |
|
compression ratio is 2.6 for ARGB8888, 4.0 for XRGB8888 |
Parent topic:Pixel buffer enumerations
vg_lite_gamma_conversion_t enumeration
Specifies the gamma conversion mode (from Sept 2022)
Used in function: vg_lite_set_gamma.
vg_lite_gamma_conversion_t string value |
Description |
|---|---|
|
Leave the color as it is. |
|
Convert from sRGB to linear. |
|
Convert from linear to sRGB space. |
Parent topic:Pixel buffer enumerations
vg_lite_index_endian_t enumeration
Specifies the endian order parsing mode for index formats (from March 2023).
Used in structure: vg_lite_buffer_t.
vg_lite_index_endian_t string value |
Description |
|---|---|
|
Parse the index pixel from low to high, when using index1, the parsing order is bit0~bit7. when using index2, the parsing order is bit0:1,bit2:3,bit4:5.bit6:7. when using index4, the parsing order is bit0:3,bit4:7. |
|
Parse the index pixel from low to high, when using index1, the parsing order is bit7~bit0. when using index2, the parsing order is bit7:6,bit5:4,bit3:2.bit1:0. when using index4, the parsing order is bit4:7,bit0:3. |
Parent topic:Pixel buffer enumerations
vg_lite_image_mode_t enumeration
Specifies how an image is rendered onto a buffer (prior to Sept 2022 name was vg_lite_buffer_image_mode_t).
Used in structure: vg_lite_buffer_t.
vg_lite_image_mode_t string value |
Description |
|---|---|
|
|
|
Image drawn with blending mode |
|
Image is multiplied with paint color |
|
|
|
Image input is ignored. |
|
Parent topic:Pixel buffer enumerations
vg_lite_map_flag_t enumeration
Specifies whether mapping is for user memory or the DMA buffer (from March 2023).
Used in function: vg_lite_map.
vg_lite_map_flag_t string value |
Description |
|---|---|
|
Mapping is for user memory. |
|
Mapping is for the DMA buffer. |
Parent topic:Pixel buffer enumerations
vg_lite_paint_type_t enumeration
Specifies paint type (from May 2023).
Used in structure: vg_lite_buffer_t.
vg_lite_paint_type_t string value |
Description |
|---|---|
|
|
|
Color |
|
Linear Gradient |
|
Radial Gradient |
|
Pattern |
Parent topic:Pixel buffer enumerations
vg_lite_transparency_t enumeration
Specifies the transparency mode for a buffer (prior to Sept 2022 name was vg_lite_buffer_transparency_mode_t).
Used in structure:vg_lite_buffer.
vg_lite_transparency_t string value |
Description |
|---|---|
|
Opaque image: all image pixels are copied to the VG PE for rasterization |
|
Transparent image: only the non-transparent image pixels are copied to the VG PE. Note: This mode is only valid when |
Parent topic:Pixel buffer enumerations
vg_lite_swizzle_t enumeration
This enumeration specifies the swizzle for the UV components of YUV data.
Used in structure: vg_lite_yuvinfo.
vg_lite_swizzle_t string value |
Description |
|---|---|
|
U in lower bits, V in upper bits |
|
V in lower bits, U in upper bits |
Parent topic:Pixel buffer enumerations
vg_lite_yuv2rgb_t enumeration
This enumeration specifies the standard for conversion of YUV data to RGB data.
Used in structure: vg_lite_yuvinfo.
vg_lite_yuv2rgb_t string value |
Description |
|---|---|
|
YUV Converting with ITC.BT-601 standard |
|
YUV Converting with ITC.BT-709 standard |
Parent topic:Pixel buffer enumerations
Parent topic:Pixel buffers
Pixel buffer structures
This section provides an overview on the pixel buffer structures.
vg_lite_buffer_t structure
This structure defines the buffer layout for a VGLite image or memory data.
Used in structures: vg_lite_linear_gradient_t, vg_lite_radial_gradient_t.
Used in init functions: vg_lite_allocate, vg_lite_free, vg_lite_upload_buffer, vg_lite_map, vg_lite_unmap.
Used in blit functions:vg_lite_blit, vg_lite_blit_rect, vg_lite_clear, vg_lite_create_masklayer, vg_lite_fill_masklayer, vg_lite_blend_masklayer, vg_lite_set_masklayer, vg_lite_render_masklayer, vg_lite_destroy_masklayer
Used in draw functions: vg_lite_draw, vg_lite_draw_pattern, vg_lite_draw_grad, vg_lite_draw_radial_grad
vg_lite_buffer_t member |
Type |
Description |
|---|---|---|
|
vg_lite_int32_t |
Width of buffer in pixels |
|
vg_lite_int32_t |
Height of buffer in pixels |
|
vg_lite_int32_t |
Stride in bytes |
|
Linear or tiled format for buffer enum |
|
|
color format enum |
|
|
vg_lite_pointer |
memory handle |
|
vg_lite_pointer |
pointer to the start address of the memory |
|
vg_lite_uint32_t |
GPU address |
|
YUV format info struct |
|
|
Blit image mode enum |
|
|
Image transparency mode enum |
|
|
vg_lite_fc_buffer_t |
Three (3) fast clear buffers, reserved YUV format (from March 2023) |
|
vg_lite_compress_mode |
Compression mode (from March 2023) |
|
vg_lite_index_endian_t |
Big/Little Endian setting for index formats (from March 2023) |
|
Paint type enum (from May 2023) |
|
|
vg_lite_int8_t |
Enable Image fast clear (moved from Aug 2023) |
|
vg_lite_int8_t |
Get paintcolor from different paint types (from Aug 2023) |
|
vg_lite_int8_t |
The RGB pixel values are alpha-premultipled (from Aug 2023) |
Parent topic:Pixel buffer structures
vg_lite_fc_buffer_t structure
This structure defines the organization of a fast clear buffer. (from March 2023)
Used in structure: vg_lite_buffer_t.
vg_lite_fc_buffer_t members |
Type |
Description |
|---|---|---|
width |
vg_lite_int32_t |
Width of buffer in pixels |
height |
vg_lite_int32_t |
Height of buffer in pixels |
stride |
vg_lite_int32_t |
Stride in bytes |
handle |
vg_lite_pointer |
memory handle as allocated by the VGLite kernel |
memory |
vg_lite_pointer |
logical pointer to the start address of the memory for the CPU |
address |
vg_lite_uint32_t |
address to the buffer’s memory for the GPU hardware |
color |
vg_lite_uint32_t |
The fast clear color value |
Parent topic:Pixel buffer structures
vg_lite_yuvinfo_t structure
This structure defines the organization of VGLite YUV data.
Used in structure: vg_lite_buffer_t.
vg_lite_yuvinfo_t member |
Type |
Description |
|---|---|---|
|
UV swizzle enum |
|
|
YUV conversion standard enum |
|
`uv_planar |
vg_lite_uint32_t |
UV (U) planar address for GPU, generated by driver |
|
vg_lite_uint32_t |
V planar address for GPU, generated by driver |
`alpha_planar |
vg_lite_uint32_t |
Alpha planar address for GPU, generated by driver |
`uv_stride |
vg_lite_uint32_t |
UV (U) stride in bytes |
`v_stride |
vg_lite_uint32_t |
V planar stride in bytes |
|
vg_lite_uint32_t |
Alpha stride in bytes |
`uv_height |
vg_lite_uint32_t |
UV (U) height in pixels |
`v_height |
vg_lite_uint32_t |
V stride in bytes |
|
vg_lite_pointer |
Logical pointer to the UV (U) planar memory |
`v_memory |
vg_lite_pointer |
Logical pointer to the V planar memory |
|
vg_lite_pointer |
Memory handle of the UV (U) planar, generated by the driver |
|
vg_lite_pointer |
Memory handle of the V planar, generated by the driver |
Parent topic:Pixel buffer structures
Parent topic:Pixel buffers
Pixel buffer functions
This section provides an overview of the pixel buffer functions.
vg_lite_allocate function
Description:
This function is used to allocate a buffer before it is used in either blit or draw functions.
To allow the hardware to access some memory, such as a source image or target buffer, you must first allocate the memory. The supplied vg_lite_buffer_t structure must be initialized with the size (width and height) and format of the requested buffer. If the stride is set to zero, then this function fills it in. The only input parameter to this function is the pointer to the buffer structure. If the structure has all the information needed, then appropriate memory is allocated for the buffer.
This function calls the kernel to allocate the memory. The kernel fills in the memory handle, logical address, and hardware addresses in the vg_lite_buffer_t structure.
Alignment note:
Vivante GPUs have an alignment requirement of 64 bytes. However, to meet the alignment requirements of the Vivante display controller, the VGLite driver sets the render target buffer alignment to 128 bytes. For source image buffer alignment requirements, see the alignment notes available in Table 1.
The vg_lite_buffer_format_t value descriptions:
Syntax:
vg_lite_error_t vg_lite_allocate (
vg_lite_buffer_t *buffer
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to the buffer that holds the size and format of the buffer being allocated. Either the memory or address field must be set to a non-zero value to map either a logical or physical address into hardware accessible memory. |
Returns:
VG_LITE_SUCCESSif the contiguous buffer was allocated successfully.VG_LITE_OUT_OF_RESOURCESif there is insufficient memory in the host OS heap for the buffer.VG_LITE_OUT_OF_MEMORYif allocation of a contiguous buffer failed.
Parent topic:Pixel buffer functions
vg_lite_free function
Description:
This function is used to deallocate the buffer that was previously allocated. It frees up the memory for that buffer.
Syntax:
vg_lite_error_t vg_lite_free (
vg_lite_buffer_t *buffer
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to a buffer structure that was filled in by calling the vg_lite_allocate() function. |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
vg_lite_upload_buffer function
Description:
The function uploads the pixel data to a GPU memory buffer object. The format of the data (pixel) to be uploaded must match the format defined for the buffer object. The input data memory buffer should contain enough data to be uploaded to the GPU buffer pointed by the input parameter buffer.
Note: Vivante Vector Graphics IP only uses data[0] and stride[0] as it does not support planar YUV formats..
Syntax:
vg_lite_error_t vg_lite_upload_buffer (
vg_lite_buffer_t *buffer,
vg_lite_uint8_t *data[3],
vg_lite_uint32_t stride[3]
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to a buffer structure that was filled in by calling the vg_lite_allocate() function |
|
Pointer to pixel data. For the YUV format, there may be up to 3 pointers. |
|
Stride for the pixel data |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
vg_lite_map function
Description:
This function is used to map the memory appropriately for a particular buffer. For some operating systems, it is used to get proper translation to the physical or logical address of the buffer needed by the GPU.
To use a frame buffer directly as a target buffer:
Wrap a vg_lite_buffer_t structure around the buffer
Call the kernel to map the supplied logical or physical address into hardware accessible memory
For example, if you know the logical address of the frame buffer, set the memory field of the vg_lite_buffer_t structure with that address and call this function. If you know the physical address, set the memory field to NULL and program the address field with the physical address.
Syntax:
vg_lite_error_t vg_lite_map (
vg_lite_buffer_t *buffer,
vg_lite_map_flag_t flag,
int32_t fd
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to a buffer structure that was filled in by calling the vg_lite_allocate() function |
|
Enumerate the |
|
File descriptor for |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
vg_lite_unmap function
Description:
This function unmaps the buffer and frees any memory resources allocated by a previous call to the vg_lite_map() function.
Syntax:
vg_lite_error_t vg_lite_unmap (
vg_lite_buffer_t *buffer
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to a buffer structure that was filled in by calling the vg_lite_map() function |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
vg_lite_flush_mapped_buffer function
Description:
This function flushes the CPU cache for the mapped buffer to make sure the buffer contents are written to GPU memory.
Syntax:
vg_lite_error_t vg_lite_flush_mapped_buffer (
vg_lite_buffer_t *buffer
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to a buffer structure that was filled in by calling the vg_lite_map() function |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
vg_lite_set_CLUT function
Description:
This function sets the Color Lookup Table (CLUT) in the context state for index color image. Once the CLUT is set (Not NULL), the image pixel color for index format image rendering is obtained from the Color Lookup Table (CLUT) according to the pixel’s color index value.
Note: Available only for IP with Indexed color support..
Syntax:
vg_lite_error_t vg_lite_set_CLUT (
vg_lite_uint32_t count,
vg_lite_uint32_t *colors
);
Parameters:
Name |
Description |
|---|---|
|
This is the count of the colors in the color look-up table: - For INDEX_1, there can be up to 2 colors in the table - For INDEX_2, there can be up to 4 colors in the table - For INDEX_4, there can be up to 16 colors in the table - For INDEX_8, there can be up to 256 colors in the table |
|
The Color Lookup Table (CLUT) pointed by “colors” will be stored in the context and programmed to the command buffer when needed. The CLUT will not take effect until the command buffer is submitted to HW. The color is in ARGB format with A located in the upper bits. Note: The VGLite driver does not validate the CLUT contents from the application. |
Returns:
VG_LITE_SUCCESS as no checking is done.
Parent topic:Pixel buffer functions
vg_lite_enable_dither function
Description:
This function is used to enable the dither function. Dither is turned off by default. The application can use the VGLite API vg_lite_query_feature (gcFEATURE_BIT_VG_DITHER) to determine HW support for dither.
Syntax:
vg_lite_error_t vg_lite_enable_dither (
);
Parameters: None
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
vg_lite_disable_dither function
Description:
This function is used to disable the dither function. Dither is turned off by default.
Syntax:
vg_lite_error_t vg_lite_disable_dither (
);
Parameters: None
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
vg_lite_set_gamma function
Description:
This function sets a gamma value.
Application can use the VGLite API vg_lite_query_feature(gcFEATURE_BIT_VG_GAMMA) to determine HW support for gamma.
Syntax:
vg_lite_error_t vg_lite_set_gamma (
vg_lite_gamma_conversion_t gamma_value
);
Parameters:
Name |
Description |
|---|---|
|
Sets a gamma value. See enum vg_lite_gamma_conversion_t. |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Pixel buffer functions
Parent topic:Pixel buffers