Matrices
This part of the API provides matrix controls.
Note: All the transformations in the driver/API are actually the final plane/surface coordinate system. There is no transformation of different coordinate systems with VGLite.
Matrix control float parameter type
Name |
Typedef |
Value |
|---|---|---|
|
float |
A single-precision floating-point number |
|
vg_lite_float_t |
|
Parent topic:Matrices
Matrix control structures
This section provides an overview of the graphic transformation matrix control structures.
vg_lite_matrix_t structure
This structure defines a 3x3 floating point matrix.
Used in structures: vg_lite_linear_gradient_t, vg_lite_radial_gradient_t.
Used in blit functions: vg_lite_blit, vg_lite_blit_rect.
Used in draw functions: vg_lite_draw, vg_lite_draw_gradient, vg_lite_draw_radial_gradient, vg_lite_draw_pattern, vg_lite_identity, vg_lite_scale, vg_lite_translate.
vg_lite_matrix_t member |
Type |
Description |
|---|---|---|
|
|
3x3 matrix, in [row] [column] order |
Parent topic:Matrix control structures
vg_lite_pixel_channel_enable_t structure
This structure provides enable disable flags for hardware pixel channels A,R,G,B.
Used in function: vg_lite_set_pixel_matrix_t.
vg_lite_pixel_channel_enable_t members |
Type |
Description |
|---|---|---|
|
|
Enable A channel |
|
|
Enable B channel |
|
|
Enable G channel |
|
|
Enable R channel |
Parent topic:Matrix control structures
Parent topic:Matrices
Matrix control functions
This section provides an overview of the matrix control functions.
vg_lite_identity function
Description:
This function loads an identity matrix into a matrix variable.
Syntax:
vg_lite_error_t vg_lite_identity (
vg_lite_matrix_t *matrix,
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to the vg_lite_matrix_t structure that will be loaded with an identity matrix. |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Matrix control functions
vg_lite_set_pixel_matrix function
Description:
This function sets up a pixel transform matrix m[20] which transforms each pixel as follows:

The pixel transform for the A, R, G, B channels can be enabled/disabled individually with the channel parameter.
Applications can use VGLite API vg_lite_query_feature (gcFEATURE_BIT_VG_PIXEL_MATRIX) to determine HW support for gaussian blur.
Syntax:
vg_lite_error_t vg_lite_set_pixel_matrix (
vg_lite_pixel_matrix_t matrix,
vg_lite_pixel_channel_enable_t *channel
);
Parameters:
Name |
Description |
|---|---|
|
Specifies the |
|
Pointer to the |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Matrix control functions
vg_lite_rotate function
Description:
This function rotates a matrix a specified number of degrees.
Syntax:
vg_lite_error_t vg_lite_rotate (
vg_lite_float_t degrees,
vg_lite_matrix_t *matrix
);
Parameters:
Name |
Description |
|---|---|
|
Number of degrees to rotate the matrix. Positive numbers rotate clockwise.The coordinates for the transformation are given in the surface coordinate system (top-to-bottom orientation). Rotations with positive angles are in the clockwise direction. |
|
Pointer to the vg_lite_matrix_t structure that has to be rotated |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Matrix control functions
vg_lite_scale function
Description:
This function scales a matrix in both horizontal and vertical directions.
Syntax:
vg_lite_error_t vg_lite_scale (
vg_lite_float_t scale_x,
vg_lite_float_t scale_y,
vg_lite_matrix_t *matrix
);
Parameters:
Name |
Description |
|---|---|
|
Horizontal scale |
|
Vertical scale |
|
Pointer to the vg_lite_matrix_t structure that will be scaled. |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Matrix control functions
vg_lite_translate function
Description:
This function translates a matrix to a new location.
Syntax:
vg_lite_error_t vg_lite_translate (
vg_lite_float_t x,
vg_lite_float_t y,
vg_lite_matrix_t *matrix
);
Parameters:
Name |
Description |
|---|---|
|
X location of the transformation. |
|
Y location of the transformation. |
|
Pointer to the vg_lite_matrix_t structure that will be translated. |
Returns:
Returns VG_LITE_SUCCESS if the function is successful. See vg_lite_error_t enum for other return codes.
Parent topic:Matrix control functions
Parent topic:Matrices