MCUXpresso SDK Documentation

Version 2.1.0#

New major features#

New security advisories#

A new security vulnerability has been fixed in v2.1.0. Refer to TFMV-7 for more details. The mitigation is included in this release.

New platforms supported#

Tested platforms#

The following platforms are successfully tested in this release.

  • Arm

    • AN519

    • AN521

    • AN555

    • Corstone-300

    • Corstone-310

    • Corstone-315

    • Corstone-1000

    • Musca-B1

    • Musca-S1

  • ArmChina

    • Alcor (AN557)

  • STM

    • NUCLEO-L552ZE-Q

    • STM32H573idk

  • Infineon/Cypress

    • PSoC 64

  • NXP

    • LPCXpresso55S69

Reference memory footprint#

All measurements below are made for AN521 platform, built TF-Mv2.1.0-RC2 on Windows 10 using Armclang v6.18 and build type MinSizeRel.

All modules are measured in bytes. Some minor modules are not shown in the table below.

Note

Profile Medium-ARoT-less built with disabled Firmware Update service to align with other TF-M Profiles.

Module

Base

Small

ARoT-less

Medium

Large

Flash

RAM

Flash

RAM

Flash

RAM

Flash

RAM

Flash

RAM

Generated

112

3184

160

3184

160

3184

208

3184

272

3184

Objects

972

1056

1282

5444

1379

6128

1517

1468

1588

1468

c_w.l

190

0

568

0

568

0

568

0

808

0

platform_s.a

5142

288

5474

288

5826

288

6198

288

6328

288

spm.a

3640

173

4522

173

4012

173

6616

1385

6782

1390

sprt.a

274

0

1438

0

1284

0

2438

4

2418

4

mbedcrypto.a

0

0

25588

2108

30104

2104

30104

2104

78012

1988

PROT_attestation.a

0

0

2341

557

2571

1218

2571

3010

2687

3010

PROT_crypto.a

0

0

3336

2046

3846

16002

3846

22914

4318

25794

PROT_its.a

0

0

4830

80

4894

112

5064

1988

5068

2468

PROT_platform.a

0

0

0

0

486

0

526

1280

526

1280

AROT_ps.a

0

0

0

0

0

0

3280

4364

3280

4364

Padding

34

35

113

44

114

15

120

47

171

38

platform_crypto_keys.a

0

0

246

0

252

0

252

0

252

0

qcbor.a

0

0

854

0

854

0

854

0

854

0

crypto_service_p256m.a

0

0

0

0

3534

0

3534

0

0

0

Total inc. Padding

10364

4736

50752

13924

59884

29224

67696

42036

113364

45276

Known issues#

Some open issues are not fixed in this release.

Descriptions

Issue links

TF-M Kconfig is broken due to build split. It will be recovered in a future release.

Not tracked

The message rhandle is overridden in the backend for ns_agent_mailbox. PSA ACK tests in IPC mode on platforms using ns_agent_mailbox fail for this reason.

Not tracked

Issues fixed since v2.0.0#

The following issues have been fixed since the v2.0.0 release.

Descriptions

Issue links

<None>

<None>

Reference#


Copyright (c) 2024, Arm Limited. All rights reserved.