Version 2.0.0#
New major features#
TF-M secure build process and non-secure build process are split to simplify and enhance non-secure integration with TF-M.
Refer to TF-M Build Instruction to build SPE image.
Refer to Building Tests to build non-secure tests.
Decouple the specific application Mailbox from SPM, make it an application in Secure Partition.
Unify the interfaces between partitions and SPM, and reduces the interaction interface between them.
Multi-core support in the Secure Function (SFN) model.
Optimize SPM critical section implementation to reduce time cost in isolation level 2&3.
- 1P256-M
Use local variables for connection handles instead of dynamic allocation when there is only synchronous service access routine in the SFN model.
P256-M 1P256-M component is enabled on the TF-M side in profile medium which has a much smaller code size and RAM footprint.
MCUboot upgrade to v2.0.0.
- 2TF-M QA Reports SQUAD3TF-M performance profiling tool
Mbed TLS upgrade to v3.5.0.
- 4Read the Docs
TF-M PSA client API performance profiling is tracked in SQUAD 2TF-M QA Reports SQUAD and the profiling tool 3TF-M performance profiling tool is updated.
TF-M integrates Read the Docs 4Read the Docs to support finding documentation versions by the released tags and downloading PDFs. External links are supported for documentation in TF-M Tests, Tools and Extras repositories.
New security advisories#
A Security vulnerability fixed in v1.8.1 Refer to TFMV-6 for more details. The mitigation is included in this release.
New platforms supported#
Tested platforms#
The following platforms are successfully tested in this release.
Arm
AN519
AN521
AN555
Corstone-1000
Corstone-300
Corstone-310
Musca-B1
Musca-S1
Infineon/Cypress
PSoC 64
STM
B-U585I-IOT02A
NUCLEO-L552ZE-Q
STM32H573idk
Nordic
nRF5340
nRF9160
NuMaker-PFM
M2351
M2354
NXP
LPCXpresso55S69
Reference memory footprint#
All measurements below are made for AN521 platform, built TF-Mv2.0.0-RC2 on Windows 10 using Armclang v6.18 and build type MinSizeRel.
All modules are measured in bytes. Some minor modules are not shown in the table below.
Note
Profile Medium-ARoT-less built with disabled Firmware Update service to align with other TF-M Profiles.
Module |
Base |
Small |
ARoT-less |
Medium |
Large |
|||||
|---|---|---|---|---|---|---|---|---|---|---|
Flash |
RAM |
Flash |
RAM |
Flash |
RAM |
Flash |
RAM |
Flash |
RAM |
|
Generated (stack, stc) |
112 |
3184 |
160 |
3184 |
160 |
3184 |
208 |
3184 |
272 |
3184 |
Objects |
940 |
1064 |
1224 |
5464 |
1313 |
6152 |
1443 |
1496 |
1518 |
1496 |
c_w.l |
190 |
0 |
690 |
0 |
690 |
0 |
690 |
0 |
930 |
0 |
platform (Secure) |
5098 |
284 |
5430 |
284 |
5782 |
284 |
6154 |
284 |
6284 |
284 |
SPM |
3574 |
165 |
4456 |
165 |
3946 |
165 |
6330 |
1353 |
6484 |
1358 |
sprt |
274 |
0 |
1470 |
0 |
1308 |
0 |
2470 |
4 |
2454 |
4 |
MbedCrypto |
N/A |
N/A |
25220 |
2108 |
29964 |
2104 |
29968 |
2104 |
78938 |
1996 |
PROT_attestation |
N/A |
N/A |
2341 |
557 |
2571 |
1218 |
2571 |
3010 |
2687 |
3010 |
PROT_crypto |
N/A |
N/A |
3866 |
2070 |
4420 |
16026 |
4420 |
22938 |
4552 |
25818 |
PROT_ITS |
N/A |
N/A |
4830 |
80 |
4894 |
112 |
5064 |
1988 |
5068 |
2498 |
PROT_platform |
N/A |
N/A |
N/A |
N/A |
478 |
0 |
520 |
1280 |
520 |
1280 |
AROT_PS |
N/A |
N/A |
N/A |
N/A |
N/A |
N/A |
3276 |
4364 |
3276 |
4364 |
platform_crypto_keys |
N/A |
N/A |
248 |
0 |
256 |
0 |
256 |
0 |
256 |
0 |
qcbor |
N/A |
N/A |
854 |
0 |
854 |
0 |
854 |
0 |
854 |
0 |
crypto_service_p256m |
N/A |
N/A |
N/A |
N/A |
3534 |
0 |
3534 |
0 |
N/A |
N/A |
Padding |
32 |
39 |
111 |
16 |
118 |
19 |
126 |
47 |
187 |
38 |
Total incl. padding |
10220 |
4736 |
50900 |
13928 |
60288 |
29264 |
67884 |
42052 |
114280 |
45300 |
Known issues#
Some open issues are not fixed in this release.
Descriptions |
Issue links |
|---|---|
TF-M Kconfig is broken due to build split. It will be recovered in a future release. |
Not tracked |
Issues fixed since v1.8.0#
The following issues have been fixed since the v1.8.0 release.
Descriptions |
Issue links |
|---|---|
Arm GNU toolchain version greater than 11.2 has a linker issue in syscall. |
Reference#
Copyright (c) 2023, Arm Limited. All rights reserved.