Trusted Firmware M#
Trusted Firmware-M (TF-M) implements the Secure Processing Environment (SPE) for Armv8-M, Armv8.1-M architectures (e.g. the Cortex-M33, Cortex-M23, Cortex-M55, Cortex-M85 processors) and dual-core platforms. It is the platform security architecture reference implementation aligning with PSA Certified guidelines, enabling chips, Real Time Operating Systems and devices to become PSA Certified.
TF-M relies on an isolation boundary between the Non-secure Processing Environment (NSPE) and the Secure Processing Environment (SPE). It can but is not limited to using the Arm TrustZone technology on Armv8-M and Armv8.1-M architectures. In pre-Armv8-M architectures physical core isolation is required.
TF-M consists of:
Secure Boot to authenticate NSPE and SPE images
TF-M Core for controlling the isolation, communication and execution within SPE and with NSPE
Crypto, Internal Trusted Storage (ITS), Protected Storage (PS), Firmware Update and Attestation secure services
TF-M implements PSA-FF-M defined IPC and SFN mechanisms to allow communication between isolated firmware partitions. TF-M is highly configurable allowing users to only include the required secure services and features. Project provides Base Configuration build with just TF-M core and platform drivers and 4 predefined configurations known as TF-M Profiles. TF-M Profiles or TF-M base can be configured to include required services and features as described in the Configuration section.
FF-M compliant design with TF-M#
Applications and Libraries in the Non-secure Processing Environment can utilize these secure services with a standardized set of PSA Functional APIs. Applications running on Cortex-M devices can leverage TF-M services to ensure secure connection with edge gateways and IoT cloud services. It also protects the critical security assets such as sensitive data, keys and certificates on the platform. TF-M is supported on several Cortex-M based Microcontrollers and Real Time Operating Systems (RTOS).
Terms TFM and TF-M are commonly used in documents and code and both
refer to Trusted Firmware M. Glossary has the list
of terms and abbreviations.
Repositories#
TF-M is comprised of multiple repositories that supplement each other in making the project both customisable and maintainable.
Repository |
Description |
|---|---|
Software implementation of TF-M with documentation and essential tools |
|
Tests that focus on the functionalities of TF-M components |
|
Non essential tools used for testing and verification of TF-M |
|
Extension of the main repository to host examples, demonstrations, third-party modules etc |
License#
The software is provided under a BSD-3-Clause License. Contributions to this project are accepted under the same license with developer sign-off as described in the Contributing Guidelines.
This project contains code from other projects as listed below. The code from
external projects is limited to bl2, lib and platform
folders. The original license text is included in those source files.
The
bl2folder contains files imported from MCUBoot project and the files have Apache 2.0 license.The
lib/extfolder may contain 3rd party projects and files with diverse licenses. Here are some that are different from the BSD-3-Clause and may be a part of the runtime image. The source code for these projects is fetched from upstream at build time only.CMSIS_5- Apache 2.0 licensembedcrypto- Apache 2.0 license MbedTLSmcuboot- Apache 2.0 license MCUBootqcbor- Modified BSD-3-Clause licensetf-m-extras- Set of additional components. Please check individually in tf-m-extras repository
The
platformfolder currently contains platforms support imported from the external project and the files may have different licenses.
Supported Platforms#
Cortex-M85 system:
Cortex-M55 system:
Cortex-M33 system:
Cortex-M23 system:
Dual Core Cortex-M system:
Runtime Security Engine (RSE):
The document Platform Deprecation and Removal lists the deprecated platforms, removed from the upstream.
The document Supported Platforms lists the details.
Release Notes and Process#
The Release Cadence and Process provides release cadence and process information.
The Releases provides details of major features of the release and platforms supported.
Feedback and Support#
For this release, feedback is requested via email to tf-m@lists.trustedfirmware.org.
A bi-weekly technical forum is available for discussion on any technical topics online. Welcome to join TF-M Forum.
Copyright (c) 2017-2022, Arm Limited. All rights reserved.