MCUXpresso SDK Documentation

Configuration#

TF-M is highly configurable project with many configuration options to meet a user’s needs. A user can select the desired set of services and fine-tune them to their requirements. There are two types of configuration options

Build configuration

Specifies which file or component to include into compilation and build. These are options, usually used by a build system to enable/disable modules, specify location of external dependency or other selection, global to a project. These option set shall be considered while adopting TF-M to other build systems. In the Base Configuration table these options have Build type.

Component configuration

To adjust a particular parameter to a desired value. Those options are local to a component or externally referenced when components are coupled. Options are in C header file. The The Header File Config System has more details about it. In the Base Configuration table these options have Component type.

Note

Originally, TF-M used CMake variables for both building and component tuning purposes. It was convenient to have a single system for both building and component’s configurations. To simplify and improve configurability and better support build systems other than a CMake, TF-M introduced a The Header File Config System and moved component options into a dedicated config headers.

How to configure#

TF-M Project provides a base build, defined in /config/config_base.cmake and /config/config_base.h. Starting from the base, users can enable required services and features using several independent methods to configure TF-M.

Use TF-M Profiles.

There are 4 sets of predefined configurations for a elected use cases, called profiles. A user can select a profile by providing -DTFM_PROFILE=<profile file name>. Each profiles represented by a pair of configuration files for Building (CMake) options and Component options (.h file)

Use a custom profile.

Another method is to take an existing TF-M profile and adjust the desired options manually editing CMake and config header files. This is for users familiar with TF-M.

Use The Kconfig System.

This method is recommended for beginners. Starting from the base configuration a user can enable necessary services and options. KConfig ensurers that all selected options are consistent and valid. This is new in v1.7.0 and it covers only SPM and PSA services. As an output KConfig produces a pair of configuration files, similar to a profile.

Note

In contrast, before TF-M v1.7.0, the default build includes all possible features. With growing functionality, such rich default build became unpractical by not fitting into every platform and confusing of big memory requirements.

Priorities#

A project configuration performed in multiple steps with priorities. The list below explains the process but for the details specific to Build configuration or The Header File Config System please check the corresponded document.

  1. The base configuration with default values is used as a starting point

  2. A profile options applied on top of the base

  3. A platform can check the selected configuration and apply restrictions

  4. Finally, command line options can modify the composed set

Note

To ensure a clear intention and conscious choice, all options must be provided explicitly via a project configuration file. Default values on step 1 will generate warnings which are expected to break a build.

Base Configuration#

The base configuration is the ground for configuring TF-M, provided defaults are defined in /config/config_base.cmake and /config/config_base.h. The base build includes SPM and platform code only.

This table lists the config option categorizations of the SPM and Secure Partitions.

Crypto#

Options

Type

Base Value

TFM_PARTITION_CRYPTO

Build

OFF

CRYPTO_TFM_BUILTIN_KEYS_DRIVER

Build

ON

CRYPTO_NV_SEED

Component

ON

CRYPTO_ENGINE_BUF_SIZE

Component

0x2080

CRYPTO_IOVEC_BUFFER_SIZE

Component

5120

CRYPTO_STACK_SIZE

Component

0x1B00

CRYPTO_CONC_OPER_NUM

Component

8

CRYPTO_RNG_MODULE_ENABLED

Component

1

CRYPTO_KEY_MODULE_ENABLED

Component

1

CRYPTO_AEAD_MODULE_ENABLED

Component

1

CRYPTO_MAC_MODULE_ENABLED

Component

1

CRYPTO_HASH_MODULE_ENABLED

Component

1

CRYPTO_CIPHER_MODULE_ENABLED

Component

1

CRYPTO_ASYM_SIGN_MODULE_ENABLED

Component

1

CRYPTO_ASYM_ENCRYPT_MODULE_ENABLED

Component

1

CRYPTO_KEY_DERIVATION_MODULE_ENABLED

Component

1

CRYPTO_SINGLE_PART_FUNCS_ENABLED

Component

1

Initial Attestation#

Options

Type

Base Value

TFM_PARTITION_INITIAL_ATTESTATION

Build

OFF

SYMMETRIC_INITIAL_ATTESTATION

Build

OFF

ATTEST_INCLUDE_TEST_CODE

Build

OFF

ATTEST_KEY_BITS

Build

256

ATTEST_TOKEN_PROFILE

Component

“PSA_IOT_1”

ATTEST_INCLUDE_OPTIONAL_CLAIMS

Component

1

ATTEST_INCLUDE_COSE_KEY_ID

Component

0

ATTEST_STACK_SIZE

Component

0x700

Internal Trusted Storage#

Options

Type

Base Value

TFM_PARTITION_INTERNAL_TRUSTED_STORAGE

Build

OFF

ITS_CREATE_FLASH_LAYOUT

Component

1

ITS_RAM_FS

Component

0

ITS_VALIDATE_METADATA_FROM_FLASH

Component

1

ITS_MAX_ASSET_SIZE

Component

512

ITS_NUM_ASSETS

Component

10

ITS_BUF_SIZE

Component

ITS_MAX_ASSET_SIZE

ITS_STACK_SIZE

Component

0x720

Protected Storage#

Options

Type

Base Value

TFM_PARTITION_PROTECTED_STORAGE

Build

OFF

PS_ENCRYPTION

Build

ON

PS_CRYPTO_AEAD_ALG

Build

PSA_ALG_GCM

PS_CREATE_FLASH_LAYOUT

Component

1

PS_RAM_FS

Component

0

PS_VALIDATE_METADATA_FROM_FLASH

Component

1

PS_MAX_ASSET_SIZE

Component

2048

PS_NUM_ASSETS

Component

10

PS_ROLLBACK_PROTECTION

Component

1

PS_STACK_SIZE

Component

0x700

Firmware Update#

Options

Type

Base Value

PLATFORM_HAS_FIRMWARE_UPDATE_SUPPORT

Build

OFF

TFM_PARTITION_FIRMWARE_UPDATE

Build

OFF

TFM_CONFIG_FWU_MAX_WRITE_SIZE

Build

1024

TFM_CONFIG_FWU_MAX_MANIFEST_SIZE

Build

0

FWU_DEVICE_CONFIG_FILE

Build

“”

FWU_SUPPORT_TRIAL_STATE

Build

Depends on MCUBOOT_UPGRADE_STRATEGY

TFM_FWU_BOOTLOADER_LIB

Build

“mcuboot”

TFM_FWU_BUF_SIZE

Component

PSA_FWU_MAX_BLOCK_SIZE

FWU_STACK_SIZE

Component

0x600

Platform Secure Partition#

Options

Type

Base Value

TFM_PARTITION_PLATFORM

Build

OFF

PLATFORM_SERVICE_INPUT_BUFFER_SIZE

Component

64

PLATFORM_SERVICE_OUTPUT_BUFFER_SIZE

Component

64

PLATFORM_SP_STACK_SIZE

Component

0x500

PLATFORM_NV_COUNTER_MODULE_DISABLED

Component

0

NS Agent Mailbox Secure Partition#

Options

Type

Base Value

NS_AGENT_MAILBOX_STACK_SIZE

Component

0x800

Secure Partition Manager#

Options

Type

Base Values

TFM_ISOLATION_LEVEL

Build

1

PSA_FRAMEWORK_HAS_MM_IOVEC

Build

OFF

CONFIG_TFM_SPM_BACKEND

Build

“SFN”

TFM_SPM_LOG_LEVEL

Build

1

CONFIG_TFM_CONN_HANDLE_MAX_NUM

Component

8

CONFIG_TFM_DOORBELL_API

Component

0

CONFIG_TFM_SCHEDULE_WHEN_NS_INTERRUPTED

Component

0


Copyright (c) 2022,2024, Arm Limited. All rights reserved. Copyright (c) 2023 Cypress Semiconductor Corporation (an Infineon company) or an affiliate of Cypress Semiconductor Corporation. All rights reserved.