The Kconfig System#
The Kconfig system is an alternative tool to the CMake config system for users to change config options of TF-M.
It handles dependencies and validations automatically when you change configurations so that the generated configuration options are always valid.
To use the Kconfig system, enable USE_KCONFIG_TOOL in command line.
And enable MENUCONFIG to launch configuration GUI.
The Kconfig system consists of The Kconfig tool and the The Kconfig files.
The Kconfig tool#
The Kconfig tool is a python script based on Kconfiglib to generate the following config files:
CMake config file
Contains CMake cache variables of building options.
Header file
Contains component options in the header file system. Component options are gathered together in a separate menu
TF-M component configsin The Kconfig files.The .config and .config.old files
The
.configfile which contains all the above configurations in the Kconfig format. It will be created after the first execution of the script. It is only used to allow users to make adjustments basing on the previous settings. The Kconfig tool will load it if it exists and.config.oldwill be created to save the previous configurations.
The tool supports loading multiple pre-set configuration files merging into a single one.
The first loaded options are overridden by later ones if the config files contain duplicated
options.
And dependencies between config options are taken care of.
It then launches a configuration GUI for users to change any config options if the MENUCONFIG is
enabled in build command line.
Integration with TF-M build system#
TF-M build system includes kconfig.cmake to integrate this tool.
It prepares the parameters for the script and invokes it to load multiple configuration files basing
on your build setup, including but not limited to
Build type bound configurations, decided by
CMAKE_BUILD_TYPEProfile configurations, decided by
TFM_PROFILE
Customizing config options#
By default, the Kconfig system only merges configuration files and generated the final config files. To customize the config options, there are several approaches.
Command line options#
The support of passing configurations via command line is kept for the Kconfig system.
cmake -S . -B cmake_build -DTFM_PLATFORM=arm/mps2/an521 \
-DUSE_KCONFIG_TOOL=ON \
-DTFM_ISOLATION_LEVEL=2
Kconfig file#
You can also put the frequently used config options into a Kconfig file. When you need to apply the
config options in that file, pass it via command line option -DKCONFIG_CONFIG_FILE
cmake -S . -B cmake_build -DTFM_PLATFORM=arm/mps2/an521 \
-DTFM_ISOLATION_LEVEL=2 \
-DUSE_KCONFIG_TOOL=ON \
-DKCONFIG_CONFIG_FILE=my_config.conf
Note
The command line set options override the ones in the config file. And you can always launch menuconfig to do the final adjustments.
The Kconfig files#
The Kconfig files are the files written by the
Kconfig language
to describe config options.
They also uses some Kconfiglib extensions such as optional source osource and relative source rsource
so they can only work with the Kconfiglib.
Copyright (c) 2022-2023, Arm Limited. All rights reserved.