MCUXpresso SDK Documentation

Adding TF-M Regression Test Suite#

Introduction of TF-M regression tests#

TF-M regression tests test whether changes to TF-M code work as expected. A new regression test can consist of following 3 components:

  1. test suite: A series of tests of a certain function.

  2. test case: A specific test instance in test suites.

  3. test service or partition: Optional secure services or partitions to support related test suites.

Source structure#

Folder name

Description

test/bl1

TF-M bl1 test suites source code.

test/bl2

TF-M bL2 test suites source code.

test/config

The CMAKE test configurations files.

test/framework

Source code for test framework code, managing test suites.

test/secure_fw/suites

Test suites divided into subdirectories.

test/secure_fw/suites/<suite>/service

Test service divided into corresponding suite subdirectories.

test/secure_fw/common_test_services

Common test services.

Adding a new test suite#

This section introduces how to add a new test suite and control its compilation with a test configuration in tests_reg/test repository.

Source code#

The test suite example subdirectory named <test_name> is located under the path tests_reg/test/secure_fw/suites. If the new test suite includes both non-secure and secure parts, the source code shall be divided shared code and specific code. An example test suite folder can be organized as the figure below.

.
├── <test_name>_tests_common.c
├── non_secure
|   ├── CMakeLists.txt
│   ├── <test_name>_ns_interface_testsuite.c
│   └── <test_name>_ns_tests.h
└── secure
    ├── CMakeLists.txt
    ├── <test_name>_s_interface_testsuite.c
    └── <test_name>_s_tests.h

Creating test configurations#

A test configuration controls whether one or multiple test suites are enabled. The doc TF-M Build Instructions. shows some test configurations which are already supported in current TF-M.

Developers shall assign corresponding test configurations to control the test suites.

Naming test configurations#

The test configurations of example test suites are TEST_NS_<TEST_NAME> in non-secure and TEST_S_<TEST_NAME> in secure.

Note

The test configurations must be named with the prefixes TEST_S_ and TEST_NS_, for secure regression tests and non-secure regression tests respectively. Otherwise, tests_reg/test build system may not recognize it.

Setting test configurations#

When the test configurations have dependencies, the default value need to be set. The setting is performed in following four steps.

  1. Command line input: The configuration can be enabled or disabled by the command -DTEST_NS_<TEST_NAME>=ON/OFF -DTEST_S_<TEST_NAME>=ON/OFF, and the value cannot be changed throughout the whole compilation of TF-M tests.

  2. tests_reg/test/config/config.cmake: The test configurations shall be OFF if its dependencies are not supported. The dependencies are probably from:

    1. TF-M partitions configurations like TFM_PARTITION_CRYPTO, TFM_PARTITION_INITIAL_ATTESTATION, etc.

    2. TF-M build mode configuration like CONFIG_TFM_SPM_BACKEND.

    3. TF-M other configurations like TFM_PARTITION_FIRMWARE_UPDATE, etc.

  3. tests_reg/test/config/default_ns_test_config.cmake or tests_reg/test/config/default_s_test_config.cmake: It is required to give the default value of the new test configuration in these two files when TEST_NS or TEST_S is ON. The recommended value is ON unless the single test’s code or data size is very large.

  4. tests_reg/test/config/default_test_config.cmake: It is required to give the default value of the new test configuration in the file when both TEST_NS and TEST_S are OFF. The default value must be OFF.

Note

The test configurations must be set as CACHE value in CMAKE files. The CACHE set cannot replace the value from command line, see Set Cache Entry.

Checking test configurations#

The new test configurations must be checked by function tfm_invalid_config() if they have any dependence. The value comes from command line may be wrong when the dependencies are conflicting.

Implement necessary checks in tests_reg/test/config/check_config.cmake.

Export TF-M configurations#

If the new test depends on some TF-M configurations, export their value via tests_reg/test/config/config_ns_tests.cmake.in. TF-M secure build will install config_ns_tests.cmake and export configuration values. tf-m-tests non-secure build will include config_ns_tests.cmake and receive TF-M configuration values.

Applying test configurations#

The mission of test configurations is to control the build. They are applied in test/secure_fw/suites/<test_name>/CMakeLists.txt like the example below.

if (NOT TEST_NS_<TEST_NAME> AND NOT TEST_S_<TEST_NAME>)
    return()
endif()

####################### Non Secure #########################################

if (TEST_NS_<TEST_NAME>)
    add_library(tfm_test_suite_<test_name>_ns STATIC EXCLUDE_FROM_ALL)
    # target_sources()
    # target_include_directories()
    target_compile_definitions(tfm_test_suite_<test_name>_ns
        INTERFACE
            TEST_NS_<TEST_NAME>
    )
    # target_link_libraries()
endif()

####################### Secure #############################################

if (TEST_S_<TEST_NAME>)
    add_library(tfm_test_suite_<test_name>_s STATIC EXCLUDE_FROM_ALL)
    # target_sources()
    # target_include_directories()
    target_compile_definitions(tfm_test_suite_<test_name>_s
        INTERFACE
            TEST_S_<TEST_NAME>
    )
    # target_link_libraries()
endif()

The function target_compile_definitions will export the macros TEST_NS_<TEST_NAME> or TEST_S_<TEST_NAME> into source code. and in the file tests_reg/test/framework/non_secure_suites.c or tests/framework/secure_suites.c, the definitions of these macros will be checked, and then the head file will be included and test cases will be registered if the macro is defined.

#ifdef TEST_NS_<TEST_NAME>
#include "<test_name>_ns_tests.h"
#endif

static struct test_suite_t test_suites[] = {
/* Non-secure example test cases */
    // ......
#ifdef TEST_NS_<TEST_NAME>
    {&register_testsuite_ns_<test_name>_interface, 0, 0, 0},
#endif
};
#ifdef TEST_S_<TEST_NAME>
#include "<test_name>_s_tests.h"
#endif

static struct test_suite_t test_suites[] = {
/* Secure example test cases */
    // ......
#ifdef TEST_S_<TEST_NAME>
    {&register_testsuite_s_<test_name>_interface, 0, 0, 0},
#endif
};

Note

On most platforms non-secure tests and secure tests run on the same CPU core, but dual-core platform is an exception. So secure test library and secure services shall be linked together in the file tests_reg/test/test/secure_fw/secure_tests.cmake. Thus they can be built on secure CPU core and non-secure tests library and RTOS are built on non-secure CPU core.

# ...
if (TEST_S_<TEST_NAME>)
    add_library(tfm_test_suite_<test_name>_s STATIC EXCLUDE_FROM_ALL)
endif()

Adding a new test case in test suite#

The test cases usually express as a function in source code. They will be added into an array with structure type called test_t defined in tests_reg/test/test/framework/test_framework.h.

struct test_t {
    TEST_FUN * const test;         /*!< Test function to call */
    const char *name;              /*!< Test name */
    const char *desc;              /*!< Test description */
};

For example, a new test case called TFM_NS_<TEST_NAME>_TEST_1001 is created and the function tfm_<test_name>_test_1001 needs to be defined in file <test_name>_ns_interface_testsuite.c. Then the function shall be appended into the array which will be quoted in function register_testsuite_ns_<test_name>_interface. See the reference code below.

/* List of test cases */
static void tfm_<test_name>_test_1001(struct test_result_t *ret);

/* Append test cases */
static struct test_t <test_name>_tests[] = {
    {&tfm_<test_name>_test_1001, "TFM_NS_<TEST_NAME>_TEST_1001",
    "Example test case"},
};

/* Register test case into test suites */
void register_testsuite_ns_<test_name>_interface(struct test_suite_t *p_test_suite)
{
    uint32_t list_size;

    list_size = (sizeof(<test_name>_tests) / sizeof(<test_name>_tests[0]));

    set_testsuite("<TEST_NAME> non-secure interface test (TFM_NS_<TEST_NAME>_TEST_1XXX)",
                    <test_name>_tests, list_size, p_test_suite);
}

static void tfm_<test_name>_test_1001(struct test_result_t *ret)
{
   /* test case code */
}

Adding test services#

Some test group may need specific test services. These test services may support one or more groups thus developers shall determine the proper test scope. Refer to Adding partitions for regression tests to get more information.

Out-of-tree regression test suites#

TF-M supports out-of-tree regression test suites build, whose source code folder is outside tf-m-tests repo. There are two configurations for developers to include the source code.

  • EXTRA_NS_TEST_SUITE_PATH

    An absolute directory of the out-of-tree non-secure test suite source code folder. TF-M build system searches CMakeLists.txt of non-secure test suite in the source code folder.

  • EXTRA_S_TEST_SUITE_PATH

    An absolute directory of the out-of-tree secure test suite source code folder.

Example usage#

Take non-secure test as an example in tf-m-extras. A single out-of-tree test suite folder can be organized as the figure below:

extra_ns
├── CMakeLists.txt
├── ns_test.c
└── ns_test_config.cmake

In the example above, EXTRA_NS_TEST_SUITE_PATH in the build command can be specified as listed below.

-DEXTRA_NS_TEST_SUITE_PATH=<Absolute-path-extra-test-folder>

Coding instructions#

This is a demo of source code so the structure has been simplified. Files like .c and .h can be expanded to src and include folders respectively. The CMakeLists.txt is required in the root path and ns_test_config.cmake is optional.

Header Files#

The header file extra_ns_tests.h must be included by out-of-tree source code. This file contains the declaration of void register_testsuite_extra_ns_interface(struct test_suite_t *p_test_suite).

Source code#

To connect the out-of-tree source code and regression test framework, the test case function/functions must be defined first. An example format is:

void ns_test(struct test_result_t *ret)
{
    /* Add platform specific non-secure test suites code here. */

    ret->val = TEST_PASSED;
}

This function follows the standard TF-M test case function prototype.

Note

Extra tests can have one or more test cases. This is simplified example so only one test case is added.

After ns_test() is defined, a structure variable need to be created like:

static struct test_t plat_ns_t[] = {
    {&ns_test, "TFM_EXTRA_TEST_1001",
     "Extra Non-Secure test"},
};

It will be used by function register_testsuite_extra_ns_interface() to register the test by calling the set_testsuite() function:

void register_testsuite_extra_ns_interface(struct test_suite_t *p_test_suite)
{
    uint32_t list_size;

    list_size = (sizeof(plat_ns_t) /
                 sizeof(plat_ns_t[0]));

    set_testsuite("Extra Non-Secure interface tests"
                  "(TFM_NS_EXTRA_TEST_1XXX)",
                  plat_ns_t, list_size, p_test_suite);
}

The platform initialization code can be added in this function because it runs before ns_test().

Note

Function register_testsuite_extra_ns_interface() is declared in tf-m-tests repository without definition. It is supplied to out-of-tree source code and need to be defined with no change of its format, like returns error code and parameter name.

CMakeLists.txt#

After extra test suite file were created they must be linked to tfm_test_suite_extra_ns CMAKE target:

target_sources(tfm_test_suite_extra_ns
    PRIVATE
        ${CMAKE_CURRENT_SOURCE_DIR}/ns_test.c
)

ns_test_config.cmake#

The CMAKE configuration file is optional. If out-of-tree source already exists another configuration file, a new one can be ignored.


Copyright (c) 2021-2022, Arm Limited. All rights reserved. Copyright (c) 2022 Cypress Semiconductor Corporation (an Infineon company) or an affiliate of Cypress Semiconductor Corporation. All rights reserved.