MCUXpresso SDK Documentation

Adding partitions for regression tests#

Introduction#

Some test group may need specific test services. These test services may support one or more groups thus developers shall determine the proper test scope. Currently, TF-M test services are located under tf-m-tests/test/secure_fw.

Folder name

Description

test/secure_fw/suites/<suite>/service

Test service divided into corresponding suite subdirectories.

test/secure_fw/common_test_services

Common test services.

Implementation#

Adding a test partition to provide test services is same as adding a secure partition, generally the process can be referenced from the document Adding Secure Partition.

Test Partition Specific Manifest Attributes#

Each test service must have resource requirements declared in a manifest file, the contents of test services are the same as secure partitions, but their locations are different. Test service manifests shall be set in tf-m-tests/test/secure_fw/tfm_test_manifest_list.yaml.

There are some test purpose attributes in Secure Partition manifests that are NOT compatible with FF-M. They should be used in Test Partitions only.

weak_dependencies#

A TF-M regression test Partition calls other RoT services for test. But it can still run other tests if some of the RoT services are disabled. TF-M defines a "weak_dependencies" attribute in partition manifests of regression test partitions to describe test service access to other RoT services. It shall be only used for TF-M regression test services.

model#

A TF-M regression test Partition may support both the SFN and IPC model. The actual model being used follows the SPM backend enabled.

The TF-M build system supports this by allowing Secure Partitions to set the model attribute to dual. The manifest tool will then change it to the corresponding value according to the current backend selected.

The Test Partitions use the following definitions to know what model is being built:

  • <<partition_name>>_MODEL_IPC, 1 if IPC model is used.

  • <<partition_name>>_MODEL_SFN, 1 if SFN model is used.

Test service implementation#

Test service of individual test#

An individual test dedicated test service should be put under the corresponding test folder test/secure_fw/suites/<test_name>.

add_subdirectory(suites/<test_name>/<service_dir>) shall be added into tf-m-tests/test/secure_fw/secure_tests.cmake to make sure that the test service is built with secure side configuration.

Common test service#

If a new test service is required by multiple test suites, the code should be put under test/secure_fw/common_test_services. If the new test suite relies on a common test service, please make sure that the build implementation of the test service is linked correctly, including the header files and libraries.


Copyright (c) 2022, Arm Limited. All rights reserved.