Maestro encoder sample
Description
Tests and demonstrates encoder functionality in Maestro pipeline.
- Supported encoders:
OPUS with OGG envelop - TBD
RAW OPUS - TBD
Input:
Prepared decoded audio data (RAW PCM format, part of Maestro repository)
Prepared encoded audio data (part of Maestro repository)
Function:
Loads RAW data into source buffer stored in RAM
Encodes audio data using selected encoder and stores data in RAM
Compares prepared data with decoded data if same
Prints
Demo result: OKorDemo result: FAILvia UART
Dependencies
Audio voice component library (pulled in by Maestro’s west), containing Encoder libraries
User Input/Output
Input:
None
Output:
UART Output
Demo result: OKif everything went OKDemo result: FAILotherwise
Configuration
See prj.conffor user input sections
Selecting encoder may be done by enabling
CONFIG_MAESTRO_EXAMPLE_ENCODER_SELECTED_<ENCODER_NAME>inprj.conffile. When no encoder is selected, default one (OPUS) is used instead.System settings should be modified (stack size, heap size) based on selected encoder and system capabilities/requirements in
prj.conffile.For other configuration options, see example’s
Kconfigandprj.conf.
Supported platforms
Currently tested for:
RD_RW612_BGA - Working encoders: None.