Maestro decoder sample
Description
Tests and demonstrates decoder functionality in Maestro pipeline.
Supported decoders:
MP3
WAV
AAC
FLAC
OPUS with OGG envelop
(RAW OPUS - TBD)
Data Input:
Prepared encoded audio data (part of Maestro repository, folder
zephyr/audioTracks)Prepared decoded audio data (RAW PCM format, part of Maestro repository, folder
zephyr/audioTracks)
Function:
Loads encoded data into source buffer stored in RAM
Decodes audio data using selected decoder and stores data in RAM
Compares prepared data with decoded data to check if its the same
Prints
Demo result: OKorDemo result: FAILvia UART
User Input/Output
Input:
None
Output:
UART Output
Demo result: OKif everything went OK
Demo result: FAILotherwise
Dependencies
Audio voice component library (pulled in by Maestro’s west), containing Decoder libraries
Configuration
See
prj.conffor user input sections
Selecting decoder may be done by enabling
CONFIG_MAESTRO_EXAMPLE_DECODER_SELECTED_<DECODER_NAME>inprj.conffile. When no decoder is selected, default one (WAV) is used instead.System settings should be modified (stack size, heap size) based on selected decoder and system capabilities/requirements in
prj.conf.For other configuration options, see example’s
Kconfigandprj.conf.
Supported platforms
Currently tested for:
RD_RW612_BGA - Working decoders: FLAC, WAV, OPUS OGG