MCUXpresso SDK Documentation

Enable MCU UARTs

Enable MCU UARTs#

  1. Connect usb typec cable from pc to typec port J15 of board.(It will emulate four serial ports[e.g. COM0 - LPUART8, COM1, COM2 - LPUART1, COM3 - LPUART2] in pc)

    • COM0(LPUART8 - use as uart of cortex-m33 core1), please perform the following steps,

      a. Enable BCU,

      • Change SW7-1 from OFF.(For imx943evk proto2 board, base board version: REV B1)

      • Change SW7-1 from ON.(For imx943evk proto1 board)

      b. Enable the serial port via bcu command,

      • bcu set_gpio fta_jtag_host_en 0 -board=imx943evk19b1 or bcu set_gpio fta_jtag_host_en 0 -board=imx943evk19a0

      • bcu set_gpio fta_jtag_uart_sel 1 -board=imx943evk19b1 or bcu set_gpio fta_jtag_uart_sel 1 -board=imx943evk19a0

    • COM2(LPUART1 - use as uart of Cortex-A)

    • COM3(LPUART2 - use as uart of Cortex-m33 core0)

  2. Connect two usb2uart converter from pc to arduino interface of board.(It will emulate two serial ports[e.g. COM4 - LPUART11, COM5 - LPUART12] in pc)

    • COM4(LPUART11 - use as uart of cortex-m7 core0)

      J48-2(M2_UART11_RXD) – TX of usb2uart converter – pc

      J48-4(M2_UART11_TXD) – RX of usb2uart converter – pc

      GND —————– GND of usb2uart converter – pc

    • COM5(LPUART12 - use as uart of cortex-m7 core1)

      J44-4(M1_UART12_RXD) – TX of usb2uart converter – pc

      J44-2(M1_UART12_TXD) – RX of usb2uart converter – pc

      GND —————– GND of usb2uart converter – pc

    Note:

    • mx943evk for m33_image.bin is used for rpmsg str echo, rpmsg ping pong and power_mode_switch_rtos.

    • mx943alt for m33_image.bin is used for almost other examples.

    • JTAG cannot be used when LPUART8 is used.

    • Pls change uart from LPUART8 to LPUART1 and generate m33_image.bin with command make config=mx94alt all when debugging with jtag.

      • For MCUXPresso SDK

    _boards/imx943evk/board.h
        #define BOARD_DEBUG_UART_INSTANCE 8 -> #define BOARD_DEBUG_UART_INSTANCE 1
    

Parent topic:Run a demo application