MCUXpresso SDK Documentation

MCUXpresso SDK: backoffAlgorithm Library#

This repository is a fork of backoffAlgorithm library (https://github.com/FreeRTOS/backoffalgorithm)(1.3.0). Modifications have been made to adapt to NXP MCUXpresso SDK. CMakeLists.txt and Kconfig added to enable backoffAlgorithm repo sources build in MCUXpresso SDK. It is part of the MCUXpresso SDK overall delivery which is composed of several sub-repositories/projects. Navigate to the top/parent repository mcuxsdk-manifests(https://github.com/nxp-mcuxpresso/mcuxsdk-manifests) for the complete delivery of MCUXpresso SDK.

backoffAlgorithm Library#

This repository contains the backoffAlgorithm library, a utility library to calculate backoff period using an exponential backoff with jitter algorithm for retrying network operations (like failed network connection with server). This library uses the “Full Jitter” strategy for the exponential backoff with jitter algorithm. More information about the algorithm can be seen in the Exponential Backoff and Jitter AWS blog.

The backoffAlgorithm library is distributed under the MIT Open Source License.

Exponential backoff with jitter is typically used when retrying a failed network connection or operation request with the server. An exponential backoff with jitter helps to mitigate failed network operations with servers, that are caused due to network congestion or high request load on the server, by spreading out retry requests across multiple devices attempting network operations. Besides, in an environment with poor connectivity, a client can get disconnected at any time. A backoff strategy helps the client to conserve battery by not repeatedly attempting reconnections when they are unlikely to succeed.

See memory requirements for this library here.

backoffAlgorithm v1.3.0 source code is part of the FreeRTOS 202210.00 LTS release.

backoffAlgorithm v1.0.0 source code is part of the FreeRTOS 202012.00 LTS release.

Reference example#

The example below shows how to use the backoffAlgorithm library on a POSIX platform to retry a DNS resolution query for amazon.com.

#include "backoff_algorithm.h"
#include <stdlib.h>
#include <string.h>
#include <netdb.h>
#include <unistd.h>
#include <time.h>

/* The maximum number of retries for the example code. */
#define RETRY_MAX_ATTEMPTS            ( 5U )

/* The maximum back-off delay (in milliseconds) for between retries in the example. */
#define RETRY_MAX_BACKOFF_DELAY_MS    ( 5000U )

/* The base back-off delay (in milliseconds) for retry configuration in the example. */
#define RETRY_BACKOFF_BASE_MS         ( 500U )

int main()
{
    /* Variables used in this example. */
    BackoffAlgorithmStatus_t retryStatus = BackoffAlgorithmSuccess;
    BackoffAlgorithmContext_t retryParams;
    char serverAddress[] = "amazon.com";
    uint16_t nextRetryBackoff = 0;

    int32_t dnsStatus = -1;
    struct addrinfo hints;
    struct addrinfo ** pListHead = NULL;
    struct timespec tp;

    /* Add hints to retrieve only TCP sockets in getaddrinfo. */
    ( void ) memset( &hints, 0, sizeof( hints ) );

    /* Address family of either IPv4 or IPv6. */
    hints.ai_family = AF_UNSPEC;
    /* TCP Socket. */
    hints.ai_socktype = ( int32_t ) SOCK_STREAM;
    hints.ai_protocol = IPPROTO_TCP;

    /* Initialize reconnect attempts and interval. */
    BackoffAlgorithm_InitializeParams( &retryParams,
                                       RETRY_BACKOFF_BASE_MS,
                                       RETRY_MAX_BACKOFF_DELAY_MS,
                                       RETRY_MAX_ATTEMPTS );


    /* Seed the pseudo random number generator used in this example (with call to
     * rand() function provided by ISO C standard library) for use in backoff period
     * calculation when retrying failed DNS resolution. */

    /* Get current time to seed pseudo random number generator. */
    ( void ) clock_gettime( CLOCK_REALTIME, &tp );
    /* Seed pseudo random number generator with seconds. */
    srand( tp.tv_sec );

    do
    {
        /* Perform a DNS lookup on the given host name. */
        dnsStatus = getaddrinfo( serverAddress, NULL, &hints, pListHead );

        /* Retry if DNS resolution query failed. */
        if( dnsStatus != 0 )
        {
            /* Generate a random number and get back-off value (in milliseconds) for the next retry.
             * Note: It is recommended to use a random number generator that is seeded with
             * device-specific entropy source so that backoff calculation across devices is different
             * and possibility of network collision between devices attempting retries can be avoided.
             *
             * For the simplicity of this code example, the pseudo random number generator, rand()
             * function is used. */
            retryStatus = BackoffAlgorithm_GetNextBackoff( &retryParams, rand(), &nextRetryBackoff );

            /* Wait for the calculated backoff period before the next retry attempt of querying DNS.
             * As usleep() takes nanoseconds as the parameter, we multiply the backoff period by 1000. */
            ( void ) usleep( nextRetryBackoff * 1000U );
        }
    } while( ( dnsStatus != 0 ) && ( retryStatus != BackoffAlgorithmRetriesExhausted ) );

    return dnsStatus;
}

Building the library#

A compiler that supports C90 or later such as gcc is required to build the library.

Additionally, the library uses a header file introduced in ISO C99, stdint.h. For compilers that do not provide this header file, the source/include directory contains stdint.readme, which can be renamed to stdint.h to build the backoffAlgorithm library.

For instance, if the example above is copied to a file named example.c, gcc can be used like so:

gcc -I source/include example.c source/backoff_algorithm.c -o example
./example

gcc can also produce an output file to be linked:

gcc -I source/include -c source/backoff_algorithm.c

Building unit tests#

Checkout Unity Submodule#

By default, the submodules in this repository are configured with update=none in .gitmodules, to avoid increasing clone time and disk space usage of other repositories (like amazon-freertos that submodules this repository).

To build unit tests, the submodule dependency of Unity is required. Use the following command to clone the submodule:

git submodule update --checkout --init --recursive test/unit-test/Unity

Platform Prerequisites#

  • For running unit tests

    • C89 or later compiler like gcc

    • CMake 3.13.0 or later

  • For running the coverage target, gcov is additionally required.

Steps to build Unit Tests#

  1. Go to the root directory of this repository. (Make sure that the Unity submodule is cloned as described above.)

  2. Create build directory: mkdir build && cd build

  3. Run cmake while inside build directory: cmake -S ../test

  4. Run this command to build the library and unit tests: make all

  5. The generated test executables will be present in build/bin/tests folder.

  6. Run ctest to execute all tests and view the test run summary.

Contributing#

See CONTRIBUTING.md for information on contributing.