SecLib_RNG: Security library and random number generator
SecLib Implementation Flavors
Overview
The NXP Connectivity Framework provides multiple SecLib implementations (flavors) to support different hardware capabilities, security requirements, and performance needs. Each flavor offers the same high-level cryptographic APIs but with different underlying implementations optimized for specific use cases.
Available SecLib Flavors
1. Software SecLib (SecLib.c)(RNG.c)
Description: Pure software implementation providing cryptographic operations if no hardware is available.
Platforms: all platforms
Characteristics:
Platform-independent software implementation
No hardware acceleration requirements
Consistent behavior across all platforms
Higher CPU usage and power consumption
Suitable for platforms without crypto hardware
Files: SecLib.c, SecLib_aes_mmo.c, RNG.c
2. EdgeLock SecLib (SecLib_sss.c)(RNG.c)
Description: Hardware-accelerated implementation using NXP’s EdgeLock secure subsystem s200.
Platforms: devices with S200: KW45, KW47, MCXW71, MCXW72
Characteristics:
Hardware-backed security operations
Secure key storage in hardware
Hardware random number generation
Lower CPU usage, better performance
Enhanced security through hardware isolation
Platform-specific (requires Secure Subsystem API)
Files: SecLib_sss.c, RNG.c
3. PSA Crypto SecLib (SecLib_psa.c)(RNG_psa.c)
Description: Implementation based on ARM’s Platform Security Architecture (PSA) Crypto API standard.
Platforms: MCXW23, (MCXW71 and MCXW72 for evaluation)
Characteristics:
Industry-standard API
Hardware acceleration when available
Secure key management
Future-proof and portable
Compliance-ready
Files: SecLib_psa.c, SecLib_psa_config.h RNG_psa.c
4. MbedTLS SecLib (SecLib_mbedtls.c)(RNG_mbedTLS.c)
Description: Implementation using the MbedTLS cryptographic library.
Platforms: all platforms, RW61
Characteristics:
Well-tested and widely adopted
Software and hardware acceleration support
Extensive algorithm support
Good performance optimization
Large memory footprint
Files: SecLib_mbedTLS.c, SecLib_mbedtls_config.h, RNG_mbedTLS.c
Flavor Selection
SecLib flavor is described in ‘Kconfig’ and selected inside prj.conf or defconfig. Define one of this line to override the default configuration for your board:
CONFIG_MCUX_COMPONENT_middleware.wireless.framework.seclib_rng_port.sw=y
CONFIG_MCUX_COMPONENT_middleware.wireless.framework.seclib_rng_port.secure_subsystem=y
CONFIG_MCUX_COMPONENT_middleware.wireless.framework.seclib_rng_port.psa=y
CONFIG_MCUX_COMPONENT_middleware.wireless.framework.seclib_rng_port.mbedtls=y
The necessary configuration files are automatically added inside of CmakeLists.txt
Random number generator
Overview
The RNG module is part of the framework used for random number generation. It uses hardware RNG peripherals as entropy sources (TRNG, Secure Subsystem, …) to provide a true random number generator interface. A Pseudo-Random number generator (PRNG) implementation is available. The PRNG may depend of SecLib services (thus requiring a common mutex) to perform HMAC-SHA256, SHA256, AES-CTR, or alternateively a Lehmer Linear Congruential generator. A prerequisite for the PRNG to function with desired randomness is to be seeded using a proper source of entropy. If no hardware acceleration is present, the RNG may fallback to lesser quality ad-hoc source e.g if present SIM_UID registers, the UIDL is used as the initial seed for the random number generator.
Initialization
The RNG module requires an initialization via a call to RNG_Init. The RNG initialization involves a call to RNG_SetSeed.
In the case of a dual core system consisting of a Host core and an NBU core, the Secure Subsystem is owned by the Host core. The Host core then has a direct access to its TRNG embedded in its secure subssystem. On the NBU code side, a request is emitted via RPMSG to the Host to provide a seed. On receipt of this request, the Host sets a ‘reseed needed’ flag (from the ISR context) If the core running the RNG service owns the TRNG entropy hardware (if any), it can get the seed directly form this hardware synchronously. In the case of an NBU that does not control the devices entropy source, that is owned by the Host, it request a seed from the Host processor via RPMSG exchange. On receipt of this request the Host sets a flag notifying of this request from the RPMSG ISR context.
RNG_ReInit API is to be used at wake up time in the context of LowPower. RNG_DeInit is used for unit tests and coverage purposes but has no useful role in a real application.
Asynchronous Seed Handling Enhancement
The RNG module has been enhanced to use the framework’s work queue system instead of polling from the IDLE thread.
Key Changes:
Work Queue Integration:
RNG_NotifyReseedNeeded()now submits seed operations to the work queue on Host coresNon-blocking: Replaces previous IDLE thread polling with asynchronous work queue scheduling
ISR-Safe: Seed requests from ISR context are safely deferred to work queue execution
Benefits:
Improved system responsiveness by removing IDLE thread dependency
Better resource management through work queue scheduling
Seed handling
RNG_SetSeed: RNG_SetExternalSeed may be used to inject application entropy to RNG context seed using a supplied array of bytes. RNG_IsReseedNeeded used from task in Host core to check whether seed must be sent to NBU core.
RNG_GetTrueRandomNumber is the API used to generate a Random 32 bit number from a HW source of entropy. It is essential if only to seed the pseudo random number generator.
RNG_GetPseudoRandomData is used to generate arrays of random bytes.
RNG_NotifyReseedNeeded Enhanced to use work queue submission on Host cores instead of requiring IDLE thread polling. Sets reseed flag and schedules asynchronous seed generation.
Security Library
Overview
The framework provides support for cryptography in the security module. It supports both software and hardware encryption. Depending on the device, the hardware encryption uses either the S200, MMCAU, LTC, or CAU3 module instruction set or dedicated AES and SHA hardware blocks.
Software implementation is provided in a library format.
Support for security algorithms
SW Seclib : SecLib.c |
EdgeLock SecLib_sss.c |
Seclib_psa.c |
Mbedtls SecLib_mbedtls.c |
nccl (part of SecLib.c) |
Usage example |
|
|---|---|---|---|---|---|---|
AES_128 |
SecLib_aes.c |
x |
x |
x |
||
AES_128_ECB |
x |
x |
x |
|||
AES_128_CBC |
x |
x |
x |
|||
AES_128_CTR encryption |
x |
x |
||||
AES_128_OFB Encryption |
x |
|||||
AES_128_CMAC |
x |
x |
x |
x |
BLE connection, ieee 15.4 |
|
AES_128_EAX |
x |
|||||
AES_128_CCM |
x |
x |
x |
x |
BLE, ieee 15.4 |
|
SHA1 |
SecLib_sha.c |
x |
x |
|||
SHA256 |
x |
x |
x |
x |
||
HMAC_SHA256 |
x |
x |
x |
PRNG, Digest for Matter |
||
ECDH_P256 shared secret generation |
x (by 15 incremental steps) -> SecLib_ecdh.c |
x with MACRO SecLibECDHUseSSS |
x |
x |
x |
BLE pairing, |
EC_P256 key pair generation |
x |
x |
x |
x |
x |
|
EC_P256 public key generation from private key |
x |
x |
Matter (ECDSA) |
|||
ECDSA_P256 hash and msg signature generation / verification |
only if owner of the key pair |
x |
x |
Matter |
||
SPAKE2+ P256 arithmetics |
x |
x |
Matter |
SecLib_psa
The framework provides PSA (Platform Security Architecture) Crypto API support through the SecLib_psa.c implementation. This provides a standardized cryptographic interface that can leverage hardware acceleration when available.
Configuration
PSA support is configured through the SecLib_psa_config.h file, which defines:
Hardware acceleration capabilities via
MBEDTLS_PSA_ACCEL_*macrosMemory management integration with the framework’s memory manager
External RNG integration
Advantages of PSA Crypto API
Standardization and Portability
Vendor Independence: Applications using PSA APIs can be easily ported between different hardware platforms without changing cryptographic code
Industry Standard: PSA Crypto API is an ARM-defined industry standard (PSA Certified), ensuring consistent behavior across different platforms and vendors
Future-Proof: As an evolving standard, PSA provides long-term compatibility and support for emerging cryptographic requirements
Security Benefits
Secure Key Management: PSA provides built-in secure key storage and lifecycle management, reducing the risk of key exposure
Hardware Security Integration: Seamless integration with hardware security modules (HSMs) and secure elements when available
Isolation: Keys and cryptographic operations can be isolated from application code, reducing attack surface
Tamper Resistance: Hardware-backed implementations provide protection against physical attacks
BLE advanced secure mode
New elements in existing structures:
computeDhKeyParam_t::keepInternalBlob - boolean telling if the shared blob is kept in this structure(in .outpoint) after ECDH_P256_ComputeDhKey() or ECDH_P256_ComputeDhKeySeg() call.
New arguments in existing functions:
ECDH_P256_ComputeDhKey keepBlobDhKey - boolean telling ECDH_P256_ComputeDhKey() or ECDH_P256_ComputeDhKeySeg() to keep the shared object after computation for later use (it is required by the SecLib_GenerateBluetoothF5KeysSecure).
New macros:
gSecLibSssUseEncryptedKeys_d - Enable or disable S200 blobs SecLib support. 0 - the Bluetooth Keys are available in plaintext, 1 - the Bluetooth Keys are not available in plaintext, but in secured blobs. Default is disabled.
New functions:
LE Secure connections pairing:
void ECDH_P256_FreeDhKeyDataSecure
This is a function used to free the shared object stored in computeDhKeyParam_t. When user calls ECDH_P256_ComputeDhKeySeg() with keepBlobDhKey set to 1, it should also call ECDH_P256_FreeDhKeyDataSecure .
SecLib_GenerateBluetoothF5Keys
This function is extracted from the Bluetooth LE Host Stack implementation. This corresponds to the legacy implementation without key blobs.
SecLib_GenerateBluetoothF5KeysSecure
Similar to SecLib_GenerateBluetoothF5Keys this function is modified to work with key blobs, the reason is to not use SSS inside the Bluetooth LE Host Stack.
SecLib_DeriveBluetoothSKD
This is a helper function used by the Bluetooth LE Host Stack in the pairing procedure, when receiving the vendor HCI command specifying that the ESK needs to be provided to LL.
ELKE_BLE_SM_F5_DeriveKeys
This is a private function, helper for SecLib_GenerateBluetoothF5KeysSecure. It was provided by the STEC team.
Privacy:
SecLib_ObfuscateKeySecure
This is a function used by the Bluetooth LE Host Stack to obfuscate the IRK before setting it to Bluetooth LE Controller or before saving it to NVM
SecLib_DeobfuscateKeySecure
This is a function used by the Bluetooth LE Host Stack to extract the plaintext IRK key from the saved NVM blob.
SecLib_VerifyBluetoothAh
This function is extracted from the legacy Bluetooth LE Host Stack implementation using plaintext keys.
SecLib_VerifyBluetoothAhSecure
Similar to SecLib_VerifyBluetoothAh with modification to work with S200 key blob.
SecLib_GenerateSymmetricKey
This is a function used by the application to generate the local IRK and local CSRK.
SecLib_GenerateBluetoothEIRKBlobSecure
This is a function used by the application to generate the EIRK needed by Bluetooth LE Controller from the IRK blob.
A2B feature
ECDH_P256_ComputeA2BKey
This function is used to compute the EdgeLock to EdgeLock key. pInPeerPublicKey points to the peer public key, pOutE2EKey is the pointer to where the E2E key object will be stored, this will be freed by the application when it is no longer required by calling ECDH_P256_FreeE2EKeyData().
ECDH_P256_FreeE2EKeyData
This function is used to free the key object given as a parameter. It is used by the application to free the E2E key when is no longer needed.
SecLib_ExportA2BBlobSecure
This function is used to import an ELKE blob or plain text symmetric key in s200 and export an E2E key blob. The input type is identified by the keyType parameter.
SecLib_ImportA2BBlobSecure
This function is used to import an E2E key blob in s200 and export an ELKE blob or plain text symmetric key. The output type is identified by the keyType parameter.
LE Secure connections Pairing flow and SecLib usage:
Each device needs to generate locally the public+private keypair. This is done using ECDH_P256_GenerateKeys.
Devices exchange their public keys.
Upon receiving the peer device’s public key, local device is computing DH key using ECDH_P256_ComputeDhKey.
Each device sends DHKeyCheck packet
Upon receiving DhKeyCheck each device computes LTK blob using SecLib_GenerateBluetoothF5Keys
After computing the each device sends HCI_LeStartEnc (on initiator), HCI_Le_Provide_Long_Term_Key (on responder)
Bluetooth LE Controller sends back SKD report custom event
Bluetooth LE Host Stack computes ESKD based on LTK blob using SecLib_DeriveBluetoothSKD and sends it to Bluetooth LE Controller
Bluetooth LE Controller encrypts the link
IRK flow and SecLib usage:
At startup, when gInitializationComplete_c event is received:
the local IRK is generated using SecLib_GenerateSymmetricKey
the local EIRK is generated using SecLib_GenerateBluetoothEIRKBlobSecure
local CSRK is generated using SecLib_GenerateSymmetricKey
During legacy pairing when receiving bonding keys, IRK is obfuscated using SecLib_ObfuscateKeySecure and stored
When app wants to set the OOB keys using Gap_SaveKeys the IRK is obfuscated using SecLib_ObfuscateKeySecure
When application calls API Gap_VerifyPrivateResolvableAddress IRK is obfuscated using SecLib_ObfuscateKeySecure and verified using SecLib_VerifyBluetoothAhSecure
When a new connection is received in Host with RPA address not resolved by the Bluetooth LE Controller, the Host tries to resolve it by obfuscating it using SecLib_ObfuscateKeySecure and verifying it using SecLib_VerifyBluetoothAhSecure
When adding a peer in Bluetooth LE Controller resolving list, the peer’s IRK is obfuscated using SecLib_ObfuscateKeySecure before setting it using HCI_Le_Add_Device_To_Resolving_List.
When an IRK plaintext is requested by the application using Gap_LoadKeys it is obtained using SecLib_DeobfuscateKeySecure
When legacy pairing completes and LTK needs to be send in the pairing complete event (gConnEvtPairingComplete_c) the SecLib_DeobfuscateKey is used to extract the plaintext.
A2B flow and SecLib usage:
At startup, when gInitializationComplete_c event is received, the application will call ECDH_P256_GenerateKeys to generate the public/private key pair required for the E2E key derivation and send the public key to the peer device.
When the public key is received from the peer device, the application will call ECDH_P256_ComputeA2BKeySecure to generate the EdgeLock to EdgeLock key.
The application will obtain an E2E IRK blob by calling SecLib_ExportA2BBlobSecure with key type gSecElkeBlob_c. The obtained blob is sent to the peer anchor. The peer anchor will call SecLib_ImportA2BBlob with keyType gSecElkeBlob_c and save the resulting ELKE blob in NVM, for Digital Key both anchors must have the same IRK.
After pairing, in order to send the LTK and IRK contained in the bonding data securely, the application will call SecLib_ExportA2BBlobSecure with keyType gSecLtkElkeBlob_c for the LTK, and SecLib_ExportA2BBlobSecure with keyType gSecPlainText_c for the IRK. The E2E blobs obtained are sent along with the rest of the bonding data to the peer anchor device.
After the bonding data is trasfered the E2E key is no longer needed and ECDH_P256_FreeE2EKeyData is called with the key object obtained at step 2 when ECDH_P256_ComputeA2BKeySecure was called.