Connectivity framework CHANGELOG#
7.3.3 mcux SDK 26.06.00#
New supported platform : kw43, mcxw70 (EAR: Engineering drop only)
Minor Changes#
[kw43_mcxw70][NVM] Added flash ECC option support for KW43 platforms.
[kw45_k32w1_mcxw71][kw47_mcxw72] Removed use of SIRCCSR SDK definitions for wakeup by UART0.
[platform] Added platform abstraction macros
PLATFORM_GET_IPSR,PLATFORM_SET_INT_MASK, andPLATFORM_CLEAR_INT_MASKto allow platform-specific customization of IPSR read and interrupt mask functions while maintaining backward compatibility.
Bug Fixes#
[kw43_mcxw70] Enabled
gPlatformUseHwParameter_dto prevent generation of a new Bluetooth device address at each reset.[kw43_mcxw70] Added
gPlatformHasNbu_dcompile flag to KW43 platform configuration to declare NBU domain presence.
7.3.2 mcux SDK 26.06.00 pvw2#
Major Changes#
[NVM] Enhanced robustness of NVM MIT (Meta Information Tag) operations with improved validation and error handling. Added checksum validation feature controlled by
gNvmMetaCheckSum_dcompilation switch. Systematically validates MIT fields before use and triggers page switch if corruption detected. FixedmNvTableSizeInFlashtracking when table entries are modified. RefactoredNvWriteRecord()and addedNvModuleSwitchPage()for better ECC fault handling. AddedNvSetChecksumEnable()API to control feature at runtime. Feature disabled by default.
Minor Changes#
[wireless_mcu][ble] Refactored
PLATFORM_SetBleMaxTxPower()API moved from platform file to fwk_platform_ble.c for Zephyr compatibility.[wireless_mcu] Modified
PLATFORM_GetBDAddr()to return consistent address across calls whengPlatformUseHwParameter_dis disabled.[platform] Added FRDMKW43 to supported platform families.
[Common] Enhanced external flash API with C++ compatibility by adding extern “C” guards.
[kw43_mcxw70] Relocated
PLATFORM_TM_CLK_SELECTmacro to fwk_platform_definitions.h for platform-specific configuration.[kw43_mcxw70][sensors] Adapted temperature measurement to use FIFO0 instead of FIFO1 as only single FIFO available on this platform.
[kw43_mcxw70] Updated framework component selections in configuration files.
[wireless_nbu] Replaced
FPGA_TARGETguard withFWK_KW43_MCXW70_NBU_FAMILIESfor CPU clock configuration to better reflect target family.[kw43_mcxw70] Updated RF switch control and debug signal configurations for bringup support.
[kw43_mcxw70] Hardware parameters placement switched to IFR mode. Compilation macro
gHwParamsProdDataPlacement_cchanged fromgHwParamsProdDataMainFlash2IfrMode_ctogHwParamsProdDataIfrMode_c.[kw43_mcxw70_nbu] Enabled NBU Deep Sleep support. Removed
PLATFORM_RemoteActiveReq()andPLATFORM_RemoteActiveRel()implementations as they are not required for this platform.[kw43_mcxw70] Enabled TRNG support on kw43_mcxw70 platform.
[SecLib_RNG] Renamed
TRNG_ISRtoRNG_TrngIrqHandler()and mapped IRQ handler for platforms using TRNG to this implementation.
Bug Fixes#
[NVM] Fixed initialization procedure in
InitNVMConfig()to validate start address and partition_size.[wireless_nbu] Fixed resource access issue by reverting TSTMR read restriction on NBU as underlying issue has been resolved.
[wireless_mcu][wireless_nbu] Fixed timestamp initialization to ensure defined value when tstmrId is out of range.
[SecLib_RNG] Corrected copyright header in seclib.c.
[MISRA] Various MISRA and CERT-C compliance fixes in NVM module.
7.3.1 mcux SDK 26.06.00 pvw1#
Major Changes#
[SecLib_RNG] Refactored SecLib mutex declaration and made Lock/Unlock functions public. Changed return type from
osa_status_ttosecResultType_tfor SecLib mutex functions and moved mutex Lock/Unlock function declarations to SecLib.h.[SecLib_RNG][PSA] Activated PSA opaque execution with s200 and its secure key storage. Switched from PSA transparent mode to opaque mode for all functions except
CMAC_LsbFirstInput()which is currently not supported in opaque version. Optimized SecLib_psa_config to fully accelerate all PSA_WANT_KEY_TYPE_ECC_KEY_PAIR functions.
Minor Changes#
[RW61X] Added new API
PLATFORM_BlePriorityRemap()with HCI vendor command HCI_CMD_NXP_REMAP_BLE_PRIORITY 0x2A1 to configure BLE ADV and Connection Priority relative to Wi-Fi/OT.[DBG] Disabled DTEST signals and GPIO debug for debug target to prevent significant low power current consumption degradation.
Bug Fixes#
[OTA][Coverity] Sanitized pImageOffset parameter in OTA functions to avoid possible overflow.
[SecLib] Fixed multiplication buffer pointer initialization for segmented ECDH operations. Fixed EC P256 multistep operations using SW legacy library. Fixed
ECDH_P256_ComputeDhKeySeg()andECDH_P256_GenerateKeysSeg()argument checking across SecLib variants. FixedSecLib_AES_CMAC_PRF_128()behavior for SecLib sss variant that tolerated VK length to be 0. Removed unreachable code fromSecLib_HMAC_SHA256_Finish().[Platform] Fixed TSTMR timestamp 64 bit read compilation failure when
gPlatformTstmr32Bit_dis undefined.
7.2.3 mcux SDK 26.03.00 RFP#
Major Changes#
[SecLib] Refactored SecLib functions with improved error handling and naming conventions. Added return status codes for better testing, added
SecLib_prefix for all functions with backward compatibility maintained via#definestubs. Added parameter checks on all functions and improved test coverage for all SecLib flavors.[SecLib] Updated CryptoLibSW APIs by removing unused
pMultiplicationBufferargument fromEcdh_ComputeDhKeyUltraFast(),ECP256_GeneratePublicKeyUltraFast(), andECP256_GenerateKeyPairUltraFast(). RenamedECP256_GeneratePublicKey()toECP256_GeneratePublicKeySeg()in legacy implementation. Added newECP256_GeneratePublicKey()API for SPAKE2+ ComputeL procedure.
Minor Changes#
[FunctionLib] Enhanced
FLib_StrLen()to return error value when string size exceeds maximum limit (4096 bytes), adopting strnlen behavior.[Common] Cleaned deprecated mbedtls2x Kconfig configurations.
[wireless_mcu][lcl] Updated FEM API to send configuration to NBU for proper XCVR timing adaptation during Channel Sounding activity. XCVR register backup and restore uses current mechanism with config sent through
PLATFORM_NbuApiReq().[Kconfig] Fixed KCONFIG dependency loop related to
MCUX_COMPONENT_component.wifi_bt_module.configby switchingMCUX_COMPONENT_driver.conn_fwloaderfrom select to depends on.[SecLib_RNG] Removed support for deprecated devices including FSL_FEATURE_SOC_SIM_COUNT RNG and QN908x platform.
[FactoryDataProvider] Removed deprecated FactoryDataProvider service as it is no longer used following mbedtls2.x deprecation.
Bug Fixes#
[wireless_mcu] Fixed FRO6M calibration failure in OEM closed lifecycle by replacing inaccessible DWT cycle counter with SysTick timer. The implementation saves/restores SysTick state to maintain FreeRTOS compatibility.
[wireless_mcu][ble] Removed redundant assert in
PLATFORM_SendHciVendorEvent()as invalid parameters are already sanitized with error returned to caller.[SecLib] Fixed CMakeLists.txt lib_crypto variant dependency.
[MISRA] Various MISRA compliance fixes in OTA, flash related files, FSCI, NVM, platform files, and ICS modules. Fixed potential flash blank check issue with unaligned pointers, split
OTA_PostWriteToFlash()to match HIS_LEVEL constraint, prevented infinite loop inFLib_StrLen(), and ensured union has consistent non-zero size across compilers.
7.2.2 mcux SDK 26.03.00 pvw2#
Major Changes#
[wireless_mcu][ble] Refactored BLE platform into separate core HCI and utilities modules for improved modularity and Zephyr compatibility. Core HCI transport functions remain in fwk_platform_ble.c while utility functions (BD address generation, security, TX power, timestamps) moved to new fwk_platform_ble_utils.c module. This enables minimal HCI-only builds without hardware parameter, RNG, or controller API dependencies.
[wireless_mcu][ble] Aligned HCI platform APIs with Zephyr driver requirements.
PLATFORM_SetHciRxCallback()now returns int instead of void, added newPLATFORM_StartHci()API, and enhancedPLATFORM_InitBle()with initialization guard to prevent multiple initialization attempts.[wireless_mcu][ble] Made optional initialization steps configurable in
PLATFORM_InitBle()with new flagsgPlatformSetBleMaxTxPowerAtInit_d,gPlatformSetSfcConfigAtInit_d, andgPlatformSetWakeUpDelayAtInit_dto enable cleaner integration with Zephyr and minimal configurations.[wireless_mcu][wireless_nbu] Added new APIs:
PLATFORM_TSTMR_GetBase(),PLATFORM_TSTMR_Enable(), and modifiedPLATFORM_TSTMR_ReadTimeStamp()to use TSTMR instance ID rather than pointer. Removed dependencies on MCUX component tstmr.[SecLib_RNG] Removed legacy SecLib and RNG mbedtls framework implementations now replaced by PSA. Removed deprecated SecLib AES-MMO implementation.
[RNG] Introduced
gRngEnableAutoReseed_dfeature flag to control automatic reseeding via WorkQ. Defaults to enabled for platforms with NBU, disabled otherwise. This allows single-core platforms to use RNG without WorkQ dependency when handling reseeding manually.
Minor Changes#
[wireless_mcu][ot] Conditionally exclude MCUXpresso-specific dependencies (board_platform.h, pin_mux.h, SecLib.h, RNG_Interface.h, HWParameter.h) when building for Zephyr, with stubbed IEEE 802.15.4 address generation functions.
[wireless_mcu] Made TRDC driver dependency optional based on
gPlatformNbuDebugGpioDAccessEnabled_dusage, changing from mandatory (select) to optional (imply) in Kconfig.[wireless_nbu] Added new NBU APIs
PLATFORM_GetSharedMemConfig()andPLATFORM_GetDMemConfig()to retrieve size of SMU/DMEM.[NVM] Added
Nv_GetPartitionAddressAndSize()API to retrieve NVM partition characteristics.[DBG] Added warning ID tracking support with enhanced
NBUDBG_StateCheck()to monitor NBU warnings. AddedPLATFORM_IsNbuWarningSet()API with callback support for proactive warning monitoring.[DBG] Added HCI vendor event transmission support with
NBUDBG_ConfigureHciVendorEvent()API to enable/disable debug structure transmission over HCI.[DBG] Added coredump support on fault handler with
gFaultHandlerCoredumpEnabled_dconditional compilation.[DBG] Initialized .debugbuf from flash into sqram_debug_region for GCC builds with
INIT_BLE_DEBUG_DAT.[Sensors] Added initialization guard to prevent redundant sensor initialization calls with
PLATFORM_InitSensors().[Platform] Added missing localization dependency to XCVR in Kconfig.
[Platform] Fixed missing Kconfig dependencies for KW47 core1 variants (KW47B42ZB2, KW47B42ZB3, KW47B42ZB6, KW47B42Z96, KW47B42Z97).
[MCXW23] Enabled
gSecLibUseDspExtension_dto leverage CM33 DSP extensions for ultra-fast cryptographic library.[MCXW23] Changed temperature dummy value for sensors to support application enablement.
[OTA] Improved OTA coverage by allowing static functions to be invoked from unit tests.
[FSCI] Added UUID retrieval via
PLATFORM_GetMCUUid()abstraction inFSCI_ReadNbuVer()API.[Common] Made services CMakeLists optional to allow integration of only required services into Zephyr’s hal_nxp.
[Platform] Made timer manager optional with configuration flag.
[wireless_mcu][lcl] Corrected FEM & COEX API functions with proper NBU wake-up handling and RF_GPO pin conflict checks.
[wireless_mcu] Consolidated KB() and MB() macro definitions by using fwk_hal_macros.h instead of platform-specific definitions to prevent conflicts and ensure Zephyr compatibility.
[Common] Added Zephyr RTOS compatibility to fwk_hal_macros.h by including <zephyr/sys/util.h> when
__ZEPHYR__is defined and guarding _DO_CONCAT and CONTAINER_OF macros to prevent redefinition conflicts.
Bug Fixes#
[SecLib_RNG][PSA] Fixed RNG and PSA context release in
RNG_Deinit()by invokingmbedtls_psa_crypto_free()and resetting rng_ctx.mRngInitialized to ensure proper reinitialization inRNG_ReInit().[NVM] Fixed
GetFlashTableVersion()function to prevent recursion[NVM] Treated missing error case in
NvCopyRecord()if failed to find record.[NVS] Fixed blank check procedure to return false (non-blank) when checking a 0 length area and corrected internal flash blank check of unaligned flash data.
[SecLib] Initialized CMAC context before using it to prevent usage of uninitialized memory.
[WorkQ] Increased workqueue stack size when coverage is enabled.
[wireless_mcu] Fixed build issue when ICS WorkQ is disabled.
[MISRA] Various MISRA and CERT-C compliance fixes in NVM, HWParameter, DBG (including platform dbg), LowPower, SecLib, Platform modules (platform_ics, platform_sensors), FSCI, FunctionLib, wireless_mcu, and Common modules.
7.2.1 mcux SDK 26.03.00 pvw1#
Major Changes#
[wireless_mcu][ot] Removed
gPlatformUseOuiFromIfrconfiguration flag. OUI will now be read from IFR by default on mcxw72 platform, with a fallback to the static OUI if no value is found in IFR.[wireless_mcu][ble] Enabled
gPlatformUseUniqueDeviceIdForBdAddr_d = 2on kw47/mcxw72 platforms to read the complete BD address from IFR. If no address is found in IFR, the system will fall back to generating one using the RNG method.[SecLib] Removed unused cryptographic implementations (SHA1, AES-EAX, AES-OFB) and obsolete
FSL_FEATURE_SOC_AES_HWoption to reduce code size and complexity.
Minor Changes#
[wireless_mcu][ble] Added callback registration for HCI log. Users can register a callback to log the HCI commands sent/received on the platform using new wrapper API.
[wireless_nbu][CS][COEX] Added Channel Sounding (CS) coexistence enablement support.
Bug fixes#
[wireless_nbu][lowpower] Fixed NBU low-power timing issue by forcing LPO delay to 0 during active NBU window. The delay is restored to the default parameter right before re-entering low-power mode to guarantee accurate Link Layer timing calculations.
[platform] Removed
PLATFORM_GetClockFreq()API which contained MISRA violations, was unused, and duplicatedPLATFORM_GetNbuFreq()functionality.[MISRA] Various MISRA compliance fixes in SFC, SecLib, Platform (including platform_ics and platform low power), FSCI, and PDUM modules.
7.1.3 mcux SDK 25.12.00 RFP#
Major Changes#
[wireless_mcu][wireless_nbu] Replaced interrupt masking macros with static inline functions
PLATFORM_SetInterruptMask()andPLATFORM_ClearInterruptMask()to ensure consistent BASEPRI value handling across all compilers. This addresses compiler-dependent behavior issues with the previous macro implementation.[wireless_mcu] Added BASEPRI-based interrupt masking in
PLATFORM_RemoteActiveRel()to allow high-priority IRQs while ensuring only IMU0 or thread context can call this function.[wireless_mcu] Introduced
gPlatformUseHwParameter_dcompile flag to allow builds without HWParameter section. When undefined or set to 0, crystal trimming functions conditionally access HWParameters only when required.
Minor Changes#
[kw47_mcxw72] Introduced platform-specific library for KW47/MCXW72 platforms.
[kw47_mcxw72] Support for additional KW47 phantoms including ZB2/ZB3/ZB6/ZB7 and Z83/Z96/Z97.
[kw47_mcxw72] Removed SH_MEM_TOTAL_SIZE override as it is now automatically calculated to match rpmsg-lite configuration.
[wireless_mcu] Set RL_BUFFER_PAYLOAD_SIZE to word-aligned value as expected by rpmsg-lite.
[wireless_mcu] Added system-generated HCI vendor events capability for debug and diagnostic purposes.
[DBG] Added debug structure transmission over HCI vendor events with
NBUDBG_ConfigureHciVendorEvent()API to enable/disable the feature.[DBG] Added debug structure versioning and logging buffer address/size information to debug structure.
[DBG] Removed 15.4 region from debug structure as not supported on KW47.
[DBG] Added stack overflow detection for armv8_m_mainline architecture.
[Platform] Simplified enablement of reset features via pin detection
Automatically selects
gUseResetByLvdForce_cwhengAppForceLvdResetOnResetPinDet_dis enabled.Automatically select
gUseResetByDeepPowerDown_cwhengAppForceDeepPowerDownResetOnResetPinDet_dis enabled.
[RNG] Replaced
gRngHasSecLibDependency_dcompilation switch withgRngUseSecLib_d.[mcxw23] Defined
gRngIsrPrio_con the preprocessor to make it global and avoid redefinition warnings.[mcxw23] Implemented
PLATFORM_ResetCrypto()API called by RNG_reinit/SecLib_reinit.[mcxw23] Added support of Timer Manager timestamp with OSTIMER.
Bug fixes#
[wireless_mcu] Fixed race condition in
PLATFORM_RemoteActiveRel()by adding verification loop to confirm NBU core execution before releasing power domain.[wireless_mcu] Added instruction synchronization barrier (__ISB()) after interrupt re-enable in
PLATFORM_RemoteActiveRel()to ensure pending interrupts execute between critical sections.[wireless_mcu] Fixed external IO voltage isolation issue during low-power initialization - isolation is now cleared at init to ensure proper behavior.
[wireless_mcu] Replaced spin-wait loops with event-based synchronization in NBU communication APIs. Added mutex protection to
PLATFORM_NbuApiReq()andPLATFORM_GetNbuInfo()to prevent race conditions and deadlocks when multiple tasks call these APIs concurrently.[wireless_mcu] Fixed OSA bare metal event race condition in ICS where auto-clear event feature could cause tasks to become permanently stuck. Disabled auto-clear feature in bare metal builds and manually clear event flags after
OSA_EventWait()returns successfully.[NVM] Fixed
NvIdle()to prevent looping for more operations than the queue size.[NVS] Fixed blank check procedure to return false (non-blank) when checking a 0 length area.
[NVS] Made external and internal flash ports consistent.
[DBG] Fixed debug structure size and callback access issues - corrected memory placement overlap between reg_info and assert_info.
[MISRA] Various MISRA compliance fixes in NVM, HWParameter, LowPower, SecLib, Platform modules and IFR offset definitions.
7.1.2 mcux SDK 25.12.00 pvw2#
Major Changes#
[wireless_mcu] Reduced RPMSG buffer payload size from 496 to 270 bytes on KW43/KW47 platforms, saving 226 bytes per buffer (1808 bytes total with 4 buffers on each core). This optimization is possible as rpmsg-lite no longer requires buffer sizes to be powers of two.
[configs] Introduced
RL_ALLOW_CUSTOM_SHMEM_CONFIGflag in rpmsg_config.h to enable connectivity applications to useplatform_set_static_shmem_config()andplatform_get_custom_shmem_config().
Minor Changes#
[wireless_mcu] Updated radio power management configuration with PLATFORM_InitRadio() API on kw47/mcxw72 platforms
[DBG] Added NBU assert indication support to host with line/file info using debug structure.
[DBG] Enhanced NBU debug framework with warning detection and notification capabilities. Extended
NBUDBG_StateCheck()to monitor NBU warnings viaPLATFORM_IsNbuWarningSet()with callback support for proactive warning monitoring.[Sensors] Added periodic temperature measurement support allowing app/host to request periodic temperature measurement.
[Sensors] Added markdown documentation explaining periodic measurement functionality upon NBU requests.
[SecLib_RNG] Added documentation for asynchronous seed handling using
RNG_NotifyReseedNeeded()and SecLib implementation flavors (Software, EdgeLock, PSA Crypto, MbedTLS).[PSA] Simplified PSA configuration files and reduced imports/definitions for wireless MCU platforms.
[mcxw23] Changed temperature dummy value for sensors to progress on application enablement.
[NVS] Enhanced debug capabilities by adding
CONFIG_NVS_LOG_LEVELand improved LOG macros to adapt to PRINTF limitations.
Bug fixes#
[wireless_mcu] Fixed FRO32K as 32 kHz clock source with deferred OSC32K switching to improve initialization performance after warm reset.
[wireless_mcu] Added wait loop for NBU power domain readiness in
PLATFORM_InitNbu()to prevent race conditions when accessing NBU power domain in applications without NBU images.[wireless_mcu] Fixed external flash blank check procedure for LSPI external NOR Flash by correcting
PLATFORM_ExternalFlashAreaIsBlank()to read from RAM buffer and perform erase pattern comparison in RAM with optimized 4-byte step loops.[NVS] Removed mflash dependency from NVS external flash port and fixed internal flash blank check of unaligned flash data.
[mcxw23] Ensured TX power does not exceed 6dBm maximum limit.
7.1.1 mcux SDK 25.12.00 pvw1#
Minor Changes#
[wireless_mcu][wireless_nbu] Migrated TSTMR implementation to use SDK fsl_tstmr driver for better maintainability and consistency. This migration replaces custom TSTMR register definitions with official SDK driver APIs while maintaining existing
PLATFORM_*API compatibility.
Bug fixes#
[SecLib_RNG][mbedtls] Enhanced ECDH context preservation across low-power transitions on KW45_MCXW71 and KW47_MCXW72 platforms using export/import APIs to ensure cryptographic context is retained when hardware accelerator loses internal memory during power-down mode.
[wireless_nbu] Fixed incorrect FRODIV values that were causing reduced peripheral clocks by updating
PLATFORM_FroDiv[]mapping array to prevent over-division of flash APB and RF_CMC clocks.[rw61x/rt1060/rt1170] Added missing common files for external and OTA support on rw61x/rt1060/rt1170 platforms.
7.0.3 RFP mcux SDK 25.09.00#
Major Changes#
[wireless_mcu] Replaced ICS RX linked list with message queue to eliminate memory allocation in ISR context and enable user callbacks to run in thread context where memory allocation is permitted.
[wireless_mcu] Added HCI RX workqueue processing support to reduce ISR execution time and system impact. Feature controlled by
gPlatformHciUseWorkqueueRxProcessing_dconfiguration option (enabled by default on kw45_k32w1_mcxw71 and kw47_mcxw72 platforms in freertos applications). When enabled, HCI transport processes received data in system workqueue thread, allowing user callbacks to run in thread context.[wireless_nbu] Introduced
PLATFORM_ConfigureSmuDmemMapping()API to configure SMU and DMEM sharing on NBU for kw47_mcxw72 platform, using linker file symbols for correct configuration.[mcxw23] Implemented HCI interface using PLATFORM API as preliminary requirement for Zephyr enablement, introducing
PLATFORM_SendHciMessageAlt()alternative API.[wireless_mcu][wireless_nbu] Added NBU2Host event manager for status indications to host (Information, Warning, Error) sent over RPMSG.
[wireless_mcu] Added a call to
PLATFORM_IcsRxWorkHandler()withinPLATFORM_NbuApiReq()for baremetal applications to prevent potential deadlocks.
Minor Changes#
[wireless_mcu] Fixed variable underflow issue in
PLATFORM_RemoteActiveRel().[SecLib_RNG] Fixed escaping local HashKeyBuffer address issue and added missing cast in
RNG_GetTrueRandomNumber()function.[Common] Fixed heap memory manager return values and added missing include to fwk_freertos_utils.h.
[rw61x] Prevented array out of bounds in
PLATFORM_RegisterRtcHandle().[FSCI] Fixed memory leak in FSCI module.
[NVM] Enhanced debug facilitation by restricting variable scope, assigning return statuses to variables, and fixing display format in
NV_ShowFlashTable().[wireless_mcu] Added new chip revision A2.1 support in
PLATFORM_SendChipRevision()API.[kw47_mcxw72] Implemented BLE BD address retrieval from IFR memory with fallback to OUI + RNG.
[DBG] Added ThreadX support to fault handlers and reworked fault handler structure with dedicated RTOS files.
[DBG][Common] Added NBU debug support on host side to detect faults and system errors, with debug info extraction capability (limited to MCXW72/KW47).
[Common] Platform CMake rework and Kconfig renaming, removing unneeded checks and renaming PRJSEG platform Kconfigs to COMPONENT.
[mcxw23] Added experimental SecLib PSA support with additional configuration for MBEDTLS_ECP_C and MBEDTLS_BIGNUM_C.
[wireless_mcu] Cleaned CMakeLists.txt to avoid wrong inclusions of files and folders from incorrect platforms.
[wireless_mcu][wireless_nbu] Added NBU2Host warning when 32MHz crystal is unready on low power exit.
[wireless_mcu][ot] Introduced
gPlatformUseOuiFromIfrto use OUI from IFR for the extended address (disabled by default). When enabled and IFR is not blank, copies first three bytes to OUI field of extended address, otherwise uses static OUI as fallback.[General] Removed useless warning about TSTMR_CLOCK_FREQUENCY_MHZ definition.
[General] Updated framework license and SBOM for 25.09 RFP release.
[wireless_mcu] Fixed unused variable warning when
gPlatformIcsUseWorkqueueRxProcessing_dandgPlatformHciUseWorkqueueRxProcessing_dare disable
7.0.3 revB mcux SDK 25.09.00#
Major Changes#
[wireless_mcu] Adjusted default value of
BOARD_RADIO_DOMAIN_WAKE_UP_DELAYfrom 0x16 to 0x10 to address stability issues observed with the previous setting. This change enhances system reliability but will reduce low-power performance.
Minor Changes (bug fixes)#
[Common] Added MDK compatibility for the errno framework header.
[mcxw23] Implemented missing
PLATFORM_OtaClearBootInterface()API.[mcxw23] Refactored fwk_platform.c to separate BLE-specific logic into fwk_platform_ble.c.
[OTA] Corrected definition of
gEepromParams_WriteAlignment_cflag for mcxw23[OTA] Enabled calling
OTA_GetImgState()prior toOTA_Initialize().[wireless_mcu] Fixed
PLATFORM_IsExternalFlashSectorBlank()to check the entire sector instead of just one page.[mcxw23] Added support for OTA using external flash.
[mcxw23] Introduced
PLATFORM_GetRadioIdleDuration32K()to estimate time until next radio event.[OTA] Removed
gUseInternalStorageLink_dlinker flag definition when external OTA storage is used.[mcxw23] Extended
CopyAndReboot()to support external flash OTA.[wireless_mcu] Resolved counter wrap issue in
PLATFORM_GetDeltaTimeStamp().[kw43_mcxw70] Defined LPTMR frequency constants in fwk_platform_definitions.h.
[kw47_mcxw72] Updated shared memory allocation for RPMsg adapter.
[mcxw23] Implement
PLATFORM_IsExternalFlashBusy()API.[kw45_mcxw71][kw47_mcxw72] Moved RAM bank definitions from the connectivity framework to device-specific definitions.
7.0.3 revA mcux SDK 25.09.00#
Major Changes#
[wireless_nbu] Enhanced XTAL32M trimming handling: updates are applied when requested by the application core and the NBU enters low-power mode, ensuring no interference from ongoing radio activity. Introduced new APIs to lock (
PLATFORM_LockXtal32MTrim()) and unlock XTAL32M (PLATFORM_UnlockXtal32MTrim()) trimming updates using a counter-based mechanism. Also added a reset API (PLATFORM_ResetContext()) for platform-specific variables (currently limited to the trimming lock).[wireless_mcu] Introduced a new API,
PLATFORM_SetLdoCoreNormalDriveVoltage(), to enable support for NBU clock frequency at 64 MHz, as required by BLE channel sounding applications.[wireless_mcu][wireless_nbu] Increased delayLpoCycle default from 2 to 3 to address link layer instabilities in low-power NBU use cases. Adjusted
BOARD_RADIO_DOMAIN_WAKE_UP_DELAYfrom 0x10 to 0x16 to balance power consumption and stability. ⚠️ NBU may malfunction if delayLpoCycle (orBOARD_LL_32MHz_WAKEUP_ADVANCE_HSLOT) is set to 2 whileBOARD_RADIO_DOMAIN_WAKE_UP_DELAYis 0x16.
Minor Changes (bug fixes)#
[WorkQ] Increased stack size when RNG use mbedtls port and coverage is enabled.
[FSCI] Resolved an issue where messages remained unprocessed in the queue by ensuring
OSA_EventSet()is triggered when pending messages are detected.[OTA] Fixed a bug in in
OTA_PullImageChunk()that prevented retrieval of data previously received viaOTA_PushImageChunk()when still buffered in RAM during posted operations.[OTA] Various MISRA and coverity fixes.
[mcxw23] Fixed an unused variable warning in
PLATFORM_RegisterNbuTemperatureRequestEventCb()API.[SFC] Remove obsolete flag
gNbuJtagCapability.[wireless_mcu] Introduced new API
PLATFORM_GetRadioIdleDuration32K(). DeprecatedPLATFORM_CheckNextBleConnectivityActivity()API.[mcxw23] Aligned platform-specific implementations with the corresponding prototypes defined in wireless_mcu.
[DBG] Cleaned up fwk_fault_handler.c.
7.0.2 RFP mcux SDK 25.06.00#
Major Changes#
[wireless_mcu][wireless_nbu] Introduced
PLATFORM_Get32KTimeStamp()API, available on platforms that support it.[RNG] Switched to using a workqueue for scheduling seed generation tasks.
[Sensors] Integrated workqueue to trigger temperature readings on periodic timer expirations.
[wireless_nbu] Removed outdated configuration files from
wireless_nbu/configs.[SecLib_RNG][PSA] Added a PSA-compliant implementation for SecLib_RNG. ⚠️ This is an experimental feature and should be used with caution.
[wireless_mcu][wireless_nbu] Implemented
PLATFORM_SendNBUXtal32MTrim()API to transmit XTAL32M trimming values to the NBU.
Minor Changes (bug fixes)#
[MWS] Migrated the Mobile Wireless Standard (MWS) service to the public repository. This service manages coexistence between connectivity protocols such as BLE, 802.15.4, and GenFSK.
[HWParameter][NVM][SecLib_RNG][Sensors] Addressed various MISRA compliance issues across multiple modules.
[Sensors] Applied a filtering mechanism to temperature data measured by the application core before forwarding it to the NBU, improving data reliability.
[Common] Relocated the
GetPowerOfTwoShift()function to a shared module for broader accessibility across components.[RNG] Resolved inconsistencies in RNG behavior when using the fsl_adapter_rng HAL by aligning it with other API implementations.
[SecLib] Updated the AES CMAC block counter in
AES_128_CMAC()andAES_128_CMAC_LsbFirstInput()to support data segments larger than 4KB.[SecLib] Utilized
sss_sscp_key_object_free()withkSSS_keyObjFree_KeysStoreDefragmentto avoid key allocation failures.[MCXW23] Removed redundant
NVIC_SetPriority()call for the ctimer IRQ in the platform file, as it’s already handled by the driver.[WorkQ] Increased workqueue stack size to accommodate RNG usage with mbedtls.
[wireless_mcu][ot] Suppressed chip revision transmission when operating with nbu_15_4.
[platform][mflash] Ensured proper address alignment for external flash reads in
PLATFORM_ReadExternalFlash()when required by platform constraints.[RNG] Corrected reseed flag behavior in
RNG_GetPseudoRandomData()after reachinggRngMaxRequests_dthreshold.[platform][mflash] Fixed uninitialized variable issue in
PLATFORM_ReadExternalFlash().[platform][wireless_nbu] Fixed an issue on KW47 where PLATFORM_InitFro192M incorrectly reads IFR1 from a hardcoded flash address (0x48000), leading to unstable FRO192M trimming. The function is now conditionally compiled for KW45 only.
7.0.2 revB mcux SDK 25.06.00#
Major Changes#
[RNG][wireless_mcu][wireless_nbu] Rework RNG seeding on NBU request
[wireless_mcu] [LowPower] Add
gPlatformEnableFro6MCalLowpower_dmacro to enable FRO6M frequency verification on exit of Low Poweradd
PLATFORM_StartFro6MCalibration()andPLATFORM_EndFro6MCalibration()new function for FRO6M calibration (6MHz or 2Mhz) on wake-up from low power mode.Enabled by default in fwk_config.h
[wireless_nbu][LowPower] Clear pending interrupt status of the systick before going in lowpower - Reduce NBU active time
[wireless_nbu] Fix impossibility to go to WFI in combo mode (15.4/BLE)
[wireless_mcu] Implement XTAL32M temperature compensation mechanism. 2 new APIs:
PLATFORM_RegisterXtal32MTempCompLut(): register the temperature compensation table for XTAL32M.PLATFORM_CalibrateXtal32M(): apply XTAL32M temperature compensation depending on current temperature.
[Sensors][wireless_mcu] Add support for periodic temperature measurement. new API:
SENSORS_TriggerTemperatureMeasurementUnsafe(): to be called from Interrupt masked critical section, from ISR or when scheduler is stopped
[SFC] Change default maximal ppm target of the SFC algorithm from 200 to 360ppm. Impact the SFC algorith of kw45 and mcxw71 platforms, 360ppm was already the default setting for kw47 and mcxw72 platforms
Minor Changes (bug fixes)#
[DBG] Fix FWK_DBG_PERF_DWT_CYCLE_CNT_STOP macro
[wireless_nbu] Add
gPlatformIsNbu_dcompile Macro set to 1[wireless_nbu][ics] gFwkSrvHostChipRevision_c can be processed in the system workqueue
[kw45_mcxw71][kw47_mcxw72]
Remove LTC dependency from platform in kconfig
gPlatformShutdownEccRamInLowPowermoved from fwk_platform_definition.h to fwk_confg.h as this is a configuration flag.
[wireless_mcu][sensors] Rework and remove unnecessary ADC APIs
[wireless_nbu] Add
PLATFORM_GetMCUUid()function from Chip UID[SecLib] Change
AES_MMO_BlockUpdate()function from private to public for zigbee.
7.0.2 revA mcux SDK 25.06.00#
Supported platforms:
Same as 25.03.00 release
Major Changes#
[KW45/MCXW71] HW parameters placement now located in IFR section. Flash storage is not longer used:
Compilation: Macro
gHwParamsProdDataPlacement_cchanged fromgHwParamsProdDataMainFlash2IfrMode_ctogHwParamsProdDataIfrMode_c
[KW47] NBU: Add new fwk_platform_dcdc.[ch] files to allow DCDC stepping by using SPC high power mode. This requires new API in board_dcdc.c files. Please refer to new compilation MACROs
gBoardDcdcRampTrim_candgBoardDcdcEnableHighPowerModeOnNbu_din board_platform.h files located in kw47evk, kw47loc, frdmmcxw72 board folders.[KW45/MCXW71/KW47/MCXW72] Trigger an interrupt each time App core calls
PLATFORM_RemoteActiveReq()to access NBU power domain in order to restart NBU core for domain low power process
Minor Changes (bug fixes)#
Services#
[SecLib_RNG]
Rename
mSecLibMutexIdmutex tomSecLibSssMutexIdin SecLib_sss.cRemove
MEM_TRACKINGflag from RNG.cImplement port to fsl_adapter_rng.h API using
gRngUseRngAdapter_ccompil Macro from RNG.cAdd support for BLE debug Keys in SecLi and SecLin_sss.c with
gSecLibUseBleDebugKeys_d- for Debug only
[FSCI] Add queue mechanism to prevent corruption of FSCI global variableAllow the application to override the trig sample number parameter when
gFsciOverRpmsg_cis set to 1[DBG][btsnoop] Add a mechanism to dump raw HCI data via UART using
SBTSNOOP_MODE_RAW[OTA]
OtaInternalFlash.c: Take into account chunks smaller than a flash phrase worth
fwk_platform_ot.c: dependencies and include files to gpio, port, pin_mux removed
Platform specific#
[kw45_mcxw71][kw47_mcxw72]
fwk_platform_reset.h : add compil Macro
gUseResetByLvdForce_candgUseResetByDeepPowerDown_cto avoid compile the code if not supported on some platformsNew compile Flag
gPlatformHasNbu_dRework FRO32K notification service for MISRA fix
7.0.1 RFP mcux SDK 25.03.00#
Supported platforms:
KW45x, KW47x, MCXW71, MCXW72, K32W1x
RW61x
RT595, RT1060, RT1170
MCXW23
Minor Changes (bug fixes)#
[General] Various MISRA/Coverity fixes in framework: NVM, RNG, LowPower, SecLib and platform files
Services#
[SecLib_RNG] fix return status from
RNG_GetTrueRandomNumber()function: return correctlygRngSuccess_dwhenRNG_entropy_func()function is successful[SFC] Allow the application to override the trig sample number parameter
[Settings] Re-define the framework settings API name to avoid double definition when
gSettingsRedefineApiName_cflag is defined
Platform specific#
[wireless_mcu] fwk_platform_sensors update :
Enable temperature measurement over ADC ISR
Enable temperature handling requested by NBU
[wireless_mcu] fwk_platform_lcl coex config update for KW45
[kw47_mcxw72] Change the default ppm_target of SFC algorithm from 200 to 360ppm
7.0.1 revB mcux SDK 25.03.00#
Supported platforms:
KW45x, KW47x, MCXW71, MCXW72, K32W1x
RW61x
RT595, RT1060, RT1170
MCXW23
Minor Changes (bug fixes)#
General#
[General] Various MISRA/Coverity fixes in framework: NVM, RNG, LowPower, FunctionLib and platform files
Services#
[SecLib_RNG] AES-CBC evolution:
added
AES_CBC_Decrypt()API for sw, SSS and mbedtls variants.Made AES-CBC SW implementation reentrant avoiding use of static storage of AES block.
fixed SSS version to update Initialization Vector within SecLib, simplifying caller’s implementation.
modified
AES_128_CBC_Encrypt_And_Pad()so as to avoid the constraint mandating that 16 byte headroom be available at end of input buffer.
[SecLib_RNG] RNG modifications:
RNG_GetPseudoRandomData()could return 0 in some error cases where caller expected a negative status.Explicited RNG error codes
Added argument checks for all APIs and return
gRngBadArguments_d(-2) when wrongadded checks of RNG initalization and return
gRngNotInitialized_d(-3) when not donefixed correcteness of
RNG_GetPrngFunc()andRNG_GetPrngContext()relative to API description.Added
RNG_DeInit()function mostly for test and coverage purposes.Improved RNG description in README.md
Unified the APIs behaviour between mbedtls and non mbedtls variants.
RNG/mbedtls : Prevent
RNG_Init()from corrupting RNG entropy context if called more than once.RNG/mbedtls: fixed
RNG_GetTrueRandomNumber()to return a propermbedtls_entropy_func()result.Use defragmetation option when freeing key object in SecLib_sss to avoid leak in S200 memory
Add new API ECP256_IsKeyValid() to check whether a public key is valid
[OtaSupport] Update return status to OTA_Flash_Success when success at the end of InternalFlash_WriteData() and InternalFlash_FlushWriteBuffer() APIs
[WorQ] Implementing a simple workqueue service to the framework
[SFC] Keep using immediate measurement for some measurement before switching to configuration trig to confirm the calibration made
[DBG] Adding modules to framework DBG :
sbtsnoop
SWO
[Common] Fix HAL_CTZ and HAL_RBIT IAR versions
[LowPower] Fix wrong tick error calculation in case of infinite timeout
[Settings] Add new macro gSettingsRedefineApiName_c to avoid multiple definition of settings API when using connectivity framework repo
Platform specific#
[KW47/MCXW72] Change xtal cload default value from 4 to 8 in order to increase the precision of the link layer timebase in NBU
[wireless_mcu] [wireless_nbu] Use new WorkQ service to process framework intercore messages
[rw61x] Fix HCI message sending failure in some corner case by releasing controller wakes up after that the host has send its HCI message
[MCXW23] Adding the initial support of MCXW23 into the framework
7.0.0 mcux SDK 24.12.00#
Supported platforms:
KW45x, KW47x, MCXW71, MCXW72, K32W1x
RW61x
RT595, RT1060, RT1170
Minor Changes (bug fixes)#
Platform specific#
[RW61X]
Add MCUX_COMPONENT_middleware.wireless.framework.platform.rng to the platform to fix a warning at generation
Retrieve IEEE 64 bits address from OTP memory
[KW45x, MCXW71x, KW47x, MCXW72x]
Ignore the secure bit from RAM addresses when comparing used ram bank in bank retention mechanism
Add
gPlatformNbuDebugGpioDAccessEnabled_dCompile Macro (enabled by default). Can be used to disable the NBU debug capability using IOs in case Trustzone is enabled (``PLATFORM_InitNbu()` code executed from unsecure world).Fix in NBU firmware when sending ICS messages gFwkSrvNbuApiRequest_c (from controller_api.h API functions)
Services#
[OTA]
Add choice name to OtaSupport flash selection in Kconfig
[NVM]
Add gNvmErasePartitionWhenFlashing_c feature support to gcc toolchain
[SecLib_RNG]
Misra fixes
7.0.0 revB mcux SDK 24.12.00#
Supported platforms: KW45x, KW47x, MCXW71, MCXW72, K32W1x, RW61x, RT595, RT1060, RT1170
Major Changes (User Applications may be impacted)#
mcux github support with cmake/Kconfig from sdk3 user shall now use CmakeLists.txt and Kconfig files from root folder. Compilation should be done using west build command. In order to see the Framework Kconfig, use command >west build -t guiconfig
Board files and linker scripts moved to examples repository
Bugfixes#
[platform lowpower]
Entering Deep down power mode will no longer call
PLATFORM_EnterPowerDown(). This API is now called only when going to Power down mode
Platform specific#
[KW47/MCXW72]: Early access release only
Deep sleep power mode not fully tested. User can experiment deep sleep and deep down modes using low power reference design applications
XTAL32K-less support using FRO32K not tested
[KW45/MCXW71/K32W148]
Deep sleep mode is supported. Power down mode is supported in low power reference design applications as experimental only
XTAL32K-less support using FRO32K is experimental - FRO32K notifications callback is debug only and should not be used for mass production firmware builds
Minor Changes (no impact on application)#
Overall folder restructuring for SDK3
[Platform]:
Rename platform_family from connected_mcu/nbu to wireless_mcu/nbu
platform family have now a dedicated fwk_config.h, rpmsg_config.h and SecLib_mbedtls_config.h
[Services]
Move all framework services in a common directory “services/”
7.0.0 revA: KW45/KW47/MCX W71/MCX W72/K32W148#
Experimental Features only#
Power down on application power domain: Some tests have shown some failure. Power consumption higher than Deep Sleep. => This feature is not fully supported in this release
XTAL32K less board with FRO32K support: Some additional stress tests are under progress.
FRO32K notifications callback is for debug only and shall not be used for production. User shall not execute long processing (such as PRINTF) as it is executed in ISR context.
Main Changes#
Cmake/Kconfig support for SDK3.0
[Sensors] API renaming:
SENSORS_InitAdc()renamed toSENSORS_Init()SENSORS_DeinitAdc()remamed toSENSORS_Deinit()
[HWparams]
Repair PROD_DATA sector in case of ECC error (implies loss of previous contents of sector)
[NVM] Linker script modification for armgcc whenever gNvTableKeptInRam_d option is used:
placement of NVM_TABLE_RW in data initialized section, providing start and end address symbols. For details see NVM_Interface.h comments.
[OtaSupport]
OTA_Initialize(): now transitions the image state from RunCandidate to Permanent if not done by the application. OTA module shall always be initialized on a Permanent image, this change ensures it is the case.OTA_MakeHeadRoomForNextBlock(): now erases the OTA partition up to the image total size (rounded to the sector) if known.
Minor changes#
[Platform]
Updated macro values: -kw47: BOARD_32MHZ_XTAL_CDAC_VALUE from 12U to 16U, BOARD_32MHZ_XTAL_ISEL_VALUE from 7U to 11U, BOARD_32KHZ_XTAL_CLOAD_DEFAULT from 8U to 4U, BOARD_32KHZ_XTAL_COARSE_ADJ_DEFAULT from 1U to 3U
MCX W72 (low-power reference design applications only): BOARD_32MHZ_XTAL_CDAC_VALUE from 12U to 10U, BOARD_32MHZ_XTAL_ISEL_VALUE from 7U to 11U, BOARD_32KHZ_XTAL_CLOAD_DEFAULT from 8U to 4U, BOARD_32KHZ_XTAL_COARSE_ADJ_DEFAULT from 1U to 3U
New
PLATFORM_RegisterNbuTemperatureRequestEventCb()API: register a function callback when NBU request new temperature measurement. API provides the interval request for the temperature measurementUpdate
PLATFORM_IsNbuStarted()API to return true only if the NBU firmware has been started.
[platform lowpower]
Move RAM layout values in fwk_platform_definition.h and update RAM retention API for KW47/MCXW72
Bugfixes#
[OtaSupport]
OTA_MakeHeadRoomForNextBlock(): fixed a case where the function could try to erase outside the OTA partition range.
6.2.4: KW45/K32W1x/MCXW71/RX61x SDK 2.16.100#
This release does not contain the changes from 6.2.3 release.
This release contains changes from 6.2.2 release.
Main Change#
armgcc support for Cmake sdk2 support and VS code integration
Minor changes#
[NBU]
Optimize some critical sections on nbu firmware
[Platform]
Optimize
PLATFORM_RemoteActiveReq()execution time.
6.2.3: KW47 EAR1.0#
Initial Connectivity Framework enablement for KW47 EAR1.0 support.
New features#
OpenNBU feature : nbu_ble project is available for modification and building
Supported features#
Deep sleep mode
Unsuported features#
Power down mode
FRO32K support (XTAL32K less boards)
Main changes#
[NBU]
LPTMR2 available and TimerManager initialization with Compile Macro:
gPlatformUseLptmr_dNBU can now have access to GPIOD
SW RNG and SW SecLib ported to NBU (Software implementation only)
[RNG]
Obsoleted API removed :
FWK_RNG_DEPRECATED_APIRNG can be built without SecLib for NBU, using
gRngUseSecLib_din fwk_config.hSome API updates:
RNG_IsReseedneeded()renamed toRNG_IsReseedNeeded,RNG_TriggerReseed()renamed toRNG_NotifyReseedNeeded(),RNG_SetSeed()andRNG_SetExternalSeed()return status code.
Optimized Linear Congruential modulus computation to reduce cycle count.
Minor changes#
[NVM]
Optimize
NvIsRecordErased()procedure for faster garbage collectionMISRA fix : Remove externs and weaks from NVM module - Make RNG and timer manager dependencies conditional
[Platform]
Allow the debugger to wakeup the KW47/MCXW72 target
6.2.2: KW45/K32W1 MR6 SDK 2.16.000#
Experimental Features only:
Power down on application power domain : Some tests have shown some failure. Power consumption higher than Deep Sleep. => This feature is not fully supported in this release
XTAL32K less board with FRO32K support : Some additional stress tests are under progress.
FRO32K notifications callback is for debug only and shall not be used for production. User shall not execute long processing (such as PRINTF) as it is executed in ISR context.
Changes#
[Board] Support for freedom board FRDM-MCX W7X
[HWparams]
Support for location of HWParameters and Application Factory Data IFR in IFR1
Default is still to use HWparams in Flash to keep backward compatibility
[RNG]: API updates:
New APIS RNG_IsReseedneeded(), RNG_SetSeed() to provide See to PRNG on NBU/App core - See BluetoothLEHost_ProcessIdleTask() in app_conn.c
New APIs RNG_SetExternalSeed() : User can provide external seed. Typically used on NBU firmrware for App core to set a seed to RNG. RNG_TriggerReseed() : Not required on App core. Used on NBU only.
[NVS] Wear statistics counters added - Fix nvs_file_stat() function
[NVM] fix Nv_Shutdown() API
[SecLib] New feature AES MMO supported for Zigbee
6.2.2: RW61x RFP4 SDK 2.16.000#
[Platform] Support Zigbee stack
[OTA] Add support for RW61x OTA with remap feature.
Required modifications to prevent direct access to flash logical addresses when remap is active.
Image trailers expected at different offset with remap enabled (see gPlatformMcuBootUseRemap_d in fwk_config.h)
fixed image state assessment procedure when in RunCandidate.
[NVS] Wear statistics counters added
[SecLib] New feature AES MMO supported for Zigbee
[Misra] various fixes
6.2.1: KW45/K32W1 MR5 SDK 2.15.000#
Experimental Features only:
Power down on application power domain : Some tests have shown some failure. This feature is not fully supported in this release
XTAL32K less board with FRO32K support : Some additional stress tests are under progress. Timing variation of the timebase are being analyzed
Major changes#
[RNG]: API updates
New compile flag to keep deprecated API: FWK_RNG_DEPRECATED_API
change return error code to int type for RNG_Init(), RNG_ReInit()
New APIs RNG_GetTrueRandomNumber(), RNG_GetPseudoRandomData()
[Platform]
fwk_platform_sensors
Change default temperature value from -1 to 999999 when unknown
fwk_platform_genfsk
rename from platform_genfsk.c/h to fwk_platform_genfsk.c/h
platform family
Rename the framework platform folder from kw45_k32w1 to connected_mcu to support other platform from the same family
fwk_platform_intflash
Moved from fwk_platform files to the new fwk_platform_intflash files the internal flash dependant API
[NBU]
BOARD_LL_32MHz_WAKEUP_ADVANCE_HSLOT changed from 2 to 3 by default
BOARD_RADIO_DOMAIN_WAKE_UP_DELAY changed from 0x10 to 0x0F
[gcc linker]
Exclude k32w1_nbu_ble_15_4_dyn.bin from .data section
Minor Changes#
[Platform]
PLATFORM_GetTimeStamp(0 has an important fix for reading the Timestamp in TSTMR0
New API PLATFORM_TerminateCrypto(), PLATFORM_ResetCrypto() called from SecLib for lowpower exit
Fix when enable fro debug callback on nbu
[DBG]
SWO
Add new files fwk_debug_swo.c/h to use SWO for debug purpose
Two new flags has been added:
BOARD_DBG_SWO_CORE_FUNNEL to chose on which core you want to use SWO
BOARD_DBG_SWO_PIN_ENABLE to enable SWO on a pin
[NVS]
Add support of NVS and Settings in framework
[NBU]
Fix power down issues and reduce critical section on NBU side:
new API PLATFORM_RemoteActiveReqWithoutDelay() called from NBU functions where waiting delay is not required
Increase delay needed in power down for OEM part to request the SOC to be active
Remove unnecessary code to PLATFORM_RemoteActiveReqWithoutDelay() from PLATFORM_HciRpmsgRxCallback()
Improve nbu memory allocation failure debug messages
[SDK]
Multicore: remove critical section in HAL_RpmsgSendTimeout() (only required in FPGA HDI mode)
Flash drivers: update for ECC detection
[Platform]
fwk_platform_sensors
Fix temperature reporting to NBU
fwk_platform_extflash
Align .c and .h prototype of PLATFORM_ExternalFlashAreaIsBlank() function
[NVM]
Keep Mutex in NvModuleDeInit(). In Bare metal OS, Mutex can not be destroyed
New API NvRegisterEccFaultNotificationCb() to register Notification callback when Ecc error happens in FileSystem
[MISRA] fixes
SecLib_sss.c: ECDH_P256_ComputeDhKey()
fwk_platform_extflash.c: PLATFORM_IsExternalFlashPageBlank()
fwk_fs_abstraction.c: Various fixes
[HWparams]
Fix on if condition when gHwParamsProdDataPlacementLegacy2IfrMode_c mode is selected
[OTA]
Enable gOtaCheckEccFaults_d by default to avoid bus in case of ECC error during OTA
Fix OTA partition overflow during OTA stop and resume transfer
[BOARD]
Place code button or led specific under correct defines in board_comp.c/h
Bring back MACROs BOARD_INITRFSWITCHCONTROLPINS in pin_mux header file of the loc board
[SecLib]
Add some undefinition in SecLib_mbedtls_config as new dependency has been added in mbedtls repo:
MBEDTLS_SSL_CBC_RECORD_SPLITTING, MBEDTLS_SSL_PROTO_TLS1, MBEDTLS_SSL_PROTO_TLS1_1
[FRO32K]
FRO32K notification callback PLATFORM_FroDebugCallback_t() has new parameter to report he fro_trim value
maxCalibrationIntervalMs value can be provided to NBU using PLATFORM_FwkSrvSetRfSfcConfig()
[Sensors]
fix: PLATFORM_GetTemperatureValue() shall have NBU started to send temperature to NBU
6.2.1: RW61x RFP3#
[NVS]
Add support of NVS and Settings in framework
[MISRA] fixes
board_lp.c BOARD_UninitDebugConsole() and BOARD_ReinitDebugConsole()
fwk_platform_ble.c: Various fixes
[OTA]
Fix OTA partition overflow during OTA stop and resume transfer
6.2.0: RT1060/RT1170 SDK2.15 Major#
6.1.8: KW45/K32W1 MR4#
[BOARD PLATFORM]
Move gBoardUseFro32k_d to board_platform.h file
Offer the possibility to change the source clock accuracy to gain in power consumption
[BOARD LP]
Move PLATFORM_SetRamBanksRetained() at end of BOARD_EnterLowPowerCb() in case a memory allocation is done previously in this function
fix low power, increase BOARD_RADIO_DOMAIN_WAKE_UP_DELAY from 0 to 0x10 - Skip this delay when App requesting NBU wakeup
[PLATFORM]
fwk_platform_ble.c/h: New timestamp API that returns the difference between the current value of the LL clock and the argument of the function
fwk_platform.c/h:
New PLATFORM_EnableEccFaultsAPI_d compile flag: Enable APIs for interception of ECC Fault in bus fault handler
New gInterceptEccBusFaults_d compile flag: Provide FaultRecovery() demo code for bus fault handler to Intercept bus fault from Flash Ecc error
[LOC]
Incorrect behavior for set_dtest_page (DqTEST11 overridden)
Fix SW1 button wake able on Localization board
Fix yellow led not properly initialized
Format localization pin_mux.c/h files
[Inter Core]
Affect values to enumeration giving the inter core service message ids
Shared memory settings shared between both cores
Add callback to register when NBU has unrecoverable Radio issue
[NVM]
Add NV_STORAGE_MAX_SECTORS, NV_STORAGE_SIZE as linker symbol for alignment with other toolchain
ECC detection and recovery. New gNvSalvageFromEccFault_d and gNvVerifyReadBackAfterProgram_d compile flags. Please refer to ECC Fault detection section in README.md file located in NVM folder
[OTA]
Prevent bus fault in case of ECC error when reading back OTA_CFR update status (disable by default)
[SecLib]
Shared mutex for RNG and SecLib as they share same hardware resource
[Key storage]
Fix to ignore the garbage at the end of buffers
Detect when buffers are too small in KS_AddKey() functions
[FileCache]
Fix deadlock in Filecache FC_Process()
[SDK]
Applications: remove definition of stack location and use default from linker script, fix warmboot stack in freertos at 0x20004000
Memory Manager Light:
fix Null pointer harfault when MEM_STATISTICS_INTERNAL enable
Fix MemReinitBank() on wakeup from lowpower when Ecc banks are turned off
6.1.7: KW45/K32W1 MR3#
[OTA]
New API OTA_SetNewImageFlagWithOffset()
Fix StorageBitmapSize calculation
OTA clean up: Removed OTA_ValidateImage()
[Low Power]
New linker Symbol m_lowpower_flag_start in linker file.
Flag is used to indicate NBU that Application domain goes to power down mode. Keep this flag to 0 if only Deep sleep is supported
This flag will be set to 1 if Application domain goes to power down mode
Re-introduce PWR_AllowDeviceToSleep()/PWR_DisallowDeviceToSleep(), PWR_IsDeviceAllowedToSleep() API
Implement tick compensation mechanism for idle hook in a dedicated freertos utils file fwk_freertos_utils.[ch], new functions: FWK_PreIdleHookTickCompensation() and FWK_PostIdleHookTickCompensation
Rework timestamping on K4W1
PLATFORM_GetMaxTimeStamp() based on TSTMR
Rename PLATFORM_GetTimestamp() to PLATFORM_GetTimeStamp()
Update PLATFORM_Delay(): Rework to use TSTMR instead of LPTMR for platform_delay
Update PLATFORM_WaitTimeout(): Fixed a bug in PLATFORM_WaitTimeout() related to timer wrap
Add PLATFORM_IsTimeoutExpired() API
Fix race condition in PWR_EnterLowPower(), masking interrupts in case not done at upper layer
Low power timer split in new files fwk_platform_lowpower_timer.[ch]
New PWR_systicks_bm.c file for bare metal usage: implement SysTick suspend/resume functionality, New weak PWR_SysTicksLowPowerInit()
[FRO32K]
Improve FRO32K calibration in NBU
create PLATFORM_InitFro32K() to initialize FRO32K instead of XTAL32K (to be called from hardware_init())
update FRO32K README.md file in SFC module
Debug:
Add Notification callback feature for SFC module FRO32K
Linker script update to support m_sfc_log_start in SMU2
[SecLib]
Remove gSecLibSssUseEncryptedKeys_d compile option, split Secure/Unsecure APIs
RNG update to use same mutex than SecLib
Fix AES_128_CBC_Encrypt_And_Pad length
Implement RNG_ReInit() for lowpower
Fix issue in ECDH_P256_GenerateKeys() when waking up from power down
Call CRYPTO_ELEMU_reset() from SecLib_reInit() for power down support
[BOARD]
Create new board_platform.h file for all Board characteristics settings (32Mhz XTAL, 32KHZ XTAL, etc..)
TM_EnterLowpower() TM_EnterLowpower() to be called from LP callbacks
Support Localization boards, Only BUTTON0 supported
New compile flag BOARD_LOCALIZATION_REVISION_SUPPORT
New pin_mux.[ch] files
Offer the possibility to override CDAC and ISEL 32MHz settings before the initialization of the crystal in board_platform.h
new BOARD_32MHZ_XTAL_CDAC_VALUE, BOARD_32MHZ_XTAL_ISEL_VALUE
BOARD_32MHZ_XTAL_TRIM_DEFAULT obsoleted
[NVM file system]
Look ahead in pending save queue - Avoid consuming space to save outdated record
Fix NVM gNvDualImageSupport feature in NvIsRecordCopied
[Inter Core]
Change PLATFORM_NbuApiReq() API return parameters granularity from uint32 to uint8
MAX_VARIANT_SZ change from 20 to 25
Set lp wakeup delay to 0 to reduce time of execution on host side, NBU waits XTAL to be ready before starting execution
Update inter core config rpmsg_config.h
Add timeout to while loops that relies on hardware in RemoteActiveReq(), Application can register Callbacks when timeout
Return non-0 status when calling PLATFORM_FwkSrvSendPacket when NBU non started
Let PLATFORM_GetNbuInfo return -10 if response not received on timeout - Doxygen platform_ics APIs
[HW params]
New compile Macro for HW params placement in IFR - Save 8K in FLash: gHwParamsProdDataPlacement_c . 3 modes:
Legacy placement, move from legacy to IFR, IFR only placement
New compile Macro for Application data to be stored with HW params (in shared flash sector): gHwParamsAppFactoryDataExtension_d, New APIs:
Nv_WriteAppFactoryData(), Nv_GetAppFactoryData()
See HWParameter.h
[Platform]
Implement PLATFORM_GetIeee802_15_4Addr() API in fwk_platform_ot.c - New gPlatformUseUniqueDeviceIdFor15_4Addr_d compile Macro
Wakeup NBU domain when reading RADIO_CTRL UID_LSB register in PLATFORM_GenerateNewBDAddr()
[Reset]
New reset Implementations using Deep power down mode or LVD:
new files fwk_platform_reset.[ch]
new APIs: PLATFORM_ForceDeepPowerDownReset(), PLATFORM_ForceLvdReset() + reset on ext pins
new compile flags: gAppForceDeepPowerDownResetOnResetPinDet_d and gAppForceLvdResetOnResetPinDet_d to reset on external pins
[FSCI]
fix when gFsciRxAck_c enabled
integrate new reset APIs
6.1.4: RW610/RW612 RFP1#
[Low Power]
Added support of low power for OpenThread stack.
Added PWR_AllowDeviceToSleep/PWR_DisallowDeviceToSleep/PWR_IsDeviceAllowedToSleep APIs.
[platform]
Added PLATFORM_GetMaxTimeStamp API.
Fixed high impact Coverity.
[FreeRTOS]
Created a new utilities module for FreeRTOS: fwk_freertos_utils.c/h.
Implemented a tick compensation mechanism to be used in FreeRTOS idle hook, likely around flash operations. This mechanism aims to estimate the number of ticks missed by FreeRTOS in case the interrupts are masked for a long time.
6.1.4: KW45/K32W1 MR2#
[Low power]
Powerdown mode tested and enabled on Low Power Reference Design applications
XTAL32K removal functionality using FRO32K, supported from NBU firmwares - limitation: Application domain supports Deep Sleep only (not power down)
NBU low power improvement: low power entry sequence improvement and system clock reduction to 16Mhz during WFI
Wake up time from cold boot, reset, power switch greatly improved. Device starts on FRO32K, switch to XTAL32K when ready if gBoardUseFro32k_d not set
Bug fixes:
Move PWR LowPower callback to PLATFORM layers
Fix wrong compensation of SysTicks
Reinit system clocks when exiting power down mode: BOARD_ExitPowerDownCb(), restore 96MHz clock is set before going to low power
Call Timermanager lowpower entry exit callbacks from PLATFORM_EnterLowPower()
Update PLATFORM_ShutdownRadio() function to force NBU for Deep power down mode
K32W1:
Support lowpower mode for 15.4 stacks
[NVM]
New Compilation MACRO gNvDualImageSupport to support multiple firmware image with different register dataset
Change default configuration gNvStorageIncluded_d to 1, gNvFragmentation_Enabled_d to 1, gUnmirroredFeatureSet_d to TRUE
Some MISRA issues for this new configuration.
Remove deprecated functionality gNvUseFlexNVM_d
[SecLib]
New NXP Ultrafast ecp256 security library:
New optimized API for ecdh DhKey/ecp256 key pair computation: Ecdh_ComputeDhKeyUltraFast(), ECP256_GenerateKeyPairUltraFast().
New macro gSecLibUseDspExtension_d.
Improved software version of Seclib with Ultrafast library for ECP256_LePointValid()
Bug fixes:
Share same mutex between Seclib and RNG to prevent concurrent access to S200
Optimized S200 re-initialization, restore ecdh key pair after power down
Fixed race condition when power down low power entry is aborted
Endianness function updates and clean up
[OTA]
OTASupport improvements:
New API OTA_GetImgState(), OTA_UpdateImgState()
OTASupport and fwk_platform_extflash API updates for external flash: OTA_SelectExternalStoragePartition(), PLATFORM_IsExternalFlashSectorBlank(), PLATFORM_IsExternalFlashPageBlank(), PLATFORM_OtaGetOtaPartitionConfig()
Updated OtaExternalFlash.c, 2 new APIs in fwk_platform_extflash.c
Removed unused FLASH_op_type and FLASH_TransactionOpNode_t definitions from public API
Removed unused InternalFlash_EraseBlock() from OtaInternalFlash.c
[NBU firmware]
Mechanism to set frequency constraint to controller from the host PLATFORM_SetNbuConstraintFrequency()
NbuInfo has one more digit in versionBuildNo field
[Board]
Support Extflash low power mode, add BOARD_UninitExternalFlash(), PLATFORM_UninitExternalFlash(), PLATFORM_ReinitExternalFlash()
Support XTAL32K removal functionatity, use FRO32K instead by setting gBoardUseFro32k_d to 1 in board.h file
Support localization boards KW45B41Z-LOC Rev C
Low power improvement: New BOARD_InitPins() and BOARD_InitPinButtonBootConfig() called from hardware_init.c
Removed KW45_A0_SUPPORT support (dcdc)
Bug fixes:
Fixed glitches on the serial manager RX when exiting from power down
Fixed ADC not deinitialized in clock gated modes in BOARD_EnterLowPowerCb()
Fixed UART output flush when going to low power: BOARD_UninitAppConsole()
[platform]
PLATFORM_InitBle(), PLATFORM_SendHci() can now block with timeout if NBU does not answer. Application can register callback function to be notified when it occurs: PLATFORM_RegisterBleErrorCallback()
Added API to set and get 32Khz XTAL capacitance values: PLATFORM_GetOscCap32KValue() and PLATFORM_SetOscCap32KValue()
Added new Service FWK call gFwkSrvNbuMemFullIndication_c to get NBU mem full indication, register with PLATFORM_RegisterNbuMemErrorCallback()
Added support negative value in platform intercore service
[linker script]
Realigned gcc linker script with IAR linker script.
Added possibility to redefine cstack_start position
Added Possibility to change gNvmSectors in gcc linker script
Added dedicated reserved Section in shared memory for LL debugging
[FreeRTOSConfig.h]
Removed unused MACRO configFRTOS_MEMORY_SCHEME and configTOTAL_HEAP_SIZE
[HW Param]
Added xtalCap32K field to store XTAL32K triming value
[fwk_hal_macros.h]
Added MACRO for KB, MB and set, clear bits in bit fields
[Debug]
Added MACROs for performance measurement using DWT: DBG_PERF_MEAS
6.1.3 KW45 MR1 QP1#
[Initialization] Delay the switch to XTAL32K source clock until the BLE host stack is initialized
[lowpower] NBU wakeup from lowpower: configuration can now be programmed with BOARD_NBU_WAKEUP_DELAY_LPO_CYCLE, BOARD_RADIO_DOMAIN_WAKE_UP_DELAY in board.h file
[NBU firmware] Major fix for NBU system clock accuracy
[clock_config]
Update SRAM margin and flash config when switching system frequency
Trim FIRC in HSRUN case
[XTAL 32K trim] XTAL 32K configuration can be tuned in board.h file with BOARD_32MHZ_XTAL_TRIM_DEFAULT, BOARD_32KHZ_XTAL_CLOAD_DEFAULT, BOARD_32KHZ_XTAL_COARSE_ADJ_DEFAULT
[MAC address] Add OUI field in PLATFORM_GenerateNewBDAddr() when using Unique Device Id
6.1.2: RW610/RW612 PRC1#
[Low Power]
Updates after SDK Power Manager files renaming.
Moved PWR LowPower callback to PLATFORM layers.
Bug fixes:
Fixed wrong compensation of SysTicks during tickless idle.
Reinit RTC bus clock after exit from PM3 (power down).
[OTA]
Initial support for OTA using the external flash.
[platform]
Implemented platform specific time stamp APIs over OSTIMER.
Implemented platform specific APIs for OTA and external flash support.
Removed PLATFORM_GetLowpowerMode API.
Added support of CPU2 wake up over Spinel for OpenThread stack.
Bug fixes:
Fixed issues related to handling CPU2 power state.
[board]
Updated flash_config to support 64MB range.
[linker script]
Fixed wrong assert.
6.1.1: KW45/K32W1 MR1#
[platform] Use new FLib_MemSet32Aligned() to write in ECC RAM bank to force ECC calculation in the MEM_ReinitRamBank() function
[FunctionLib] Implement new API to set a word aligned
[platform] Set coarse amplifier gain of the oscilattor 32k to 3
[platform] Switch back to RNG for MAC Adress generation
[SecLib] Get rid of the lowpower constraint of deep sleep in ECDH API
[DCDC] Set DCDC output voltage to 1.35V in case LDO core is set to 1.1V to ensure a drop of 250mV between them
[NVM] NvIdle() is now returning the number of operations that has been executed
[documentation] Add markdown of each framework module by default on all package
[LowPower] Add a delay advised by hardware team on exit of lowpower for SPC
[SecLib] Rework of SecLib_mbedTLS ECDH functions
[OTA] Make OTA_IsTransactionPending() public API
[FunctionLib] Change prototype of FLib_MemCpyWord(), pDst is now a void* to permit more flexibility
[NVM] Add an API to know if there is a pending operation in the queue
[FSCI] Fix wrong error case handling in FSCI_Monitor()
6.1.0: KW45/K32W1 RFP#
[LowPower] Do not call PLATFORM_StopWakeUpTimer() in PWR_EnterLowPower() if PLATFORM_StartWakeUpTimer() was not previously called
[boards] Add the possibility to wakeup on UART 0 even if it is not the default UART
[boards] Add support for Hardware flow control for UART0, Enable with gBoardUseUart0HwFlowControl, Pin mux update with two additional API for RTS, CTS pins
[Sensors] Improve ADC wakeup time from deep sleep state: use save and restore API for ADC context before/after deep sleep state.
[linker script] update SMU2 shared memory region layout with NBU: increase sqram_btblebuf_size to support 24 connections. Shared memory region moved to the end
[SecLib] SecLib_DeriveBluetoothSKD() API update to support if EdgeLock key shall be regenerated