MCUXpresso SDK Documentation

Hardware setup

Hardware setup#

The examples described in this document use a KW45B41Z-EVK, KW45B41Z-LOC, MCX-W71-EVK, FRDM-MCXW71, KW47-EVK, KW47-LOC, MCX-W72-EVK, FRDM-MCXW72 or FRDM-KW43 as the development platform, as shown in the figures below.

  • The default interface selected in the IAR Embedded Workbench for Arm projects included in this release is below:

    • CMSIS-DAP for kw45b41zevk, kw45b41zloc, mcxw71evk, frdmmcxw71, frdm-kw43 platforms.

    • JLink for kw47evk, kw47loc, mcxw72evk, frdmmcxw72 and frdm-kw43 platforms.

  • Use jumpers to configure the boards in one of the available power configurations (refer to the specific board documentation).

  • On all boards, the OpenSDA USB port is connected to a Windows PC. The OpenSDA chip on the board requires flashing with appropriate firmware with debugging and virtual serial COM port capabilities.

KW45B41Z-EVK board KW45B41Z-EVK board

KW45B41Z-LOC board KW45B41Z-LOC board

MCX-W71-EVK board MCX-W71-EVK board

FRDM-MCXW71 board FRDM-MCXW71 board

KW47-EVK board KW47-EVK board

KW47-LOC board KW47-LOC board

MCX-W72-EVK board MCX-W72-EVK board

FRDM-MCXW72 board FRDM-MCXW72 board

FRDM-KW43 board FRDM-KW43 board