MCUXpresso SDK Documentation

Introduction

Contents

Introduction#

NXP hardware platforms provide the features to deploy and operate Bluetooth Low Energy localization applications implementing the Channel Sounding functionality. This document provides an overview of the features and steps to run these applications on the supported NXP hardware platforms. It also describes the sample applications included in the SDK release package.

Audience#

This document is a ready reference for firmware and system developers who create Bluetooth Low Energy localization enabled products. The document also provides a high-level description of Bluetooth Low Energy localization application scenarios that can be deployed on NXP development boards.

Parent topic:Introduction