MCUXpresso SDK Documentation

NCP Localization Reader

NCP Localization Reader#

This section describes the functionality of the NCP Localization Reader demo application.

Description#

The BLE NCP Localization Reader application is a simple demonstration program for core 1 based on the MCUXpresso SDK. This application implements a BLE device that performs distance measurement using Channel Sounding.

The application is made to be used together with the corresponding loc_reader_host application on core 0.

The device handles all BLE related operations (connection, channel sounding, service discovery) and sends the local and remote Channel Sounding data to the Core 0 application for processing.

Parent topic:NCP Localization Reader

Supported platforms#

The following platforms support the NCP Localization Reader application:

  • MCX-W72-EVK

  • FRDM-MCXW72

Parent topic:NCP Localization Reader

Parent topic:Bluetooth LE stack and demo applications