Prerequisites#
The Bluetooth Low Energy Connection Handover feature can be integrated in an application that fulfills the following requirements:
Supported platforms: KW45, KW47 and FRDM-KW43.
Bluetooth Low Energy application that is using the lib_ble_OPT_host_cm33_iar.a host library.
Communication channel between the Source and Target devices involved in the Connection Handover procedure.