MCUXpresso SDK Documentation

Demo functionality overview

Demo functionality overview#

The two demo applications provided showcase the following Digital Key R3 features:

  • Owner Pairing between a Device and a Car Anchor

  • Passive Entry

  • Synchronizing bonding data between Car Anchors

  • Connection between a Car Anchor and a non-CCC key fob

The demo applications also showcase the NXP proprietary Connection Handover and Anchor Monitoring features, as well as the A2B feature (secured synchronization of bonding data).