Advanced Secure Mode#
This section describes the advanced security capabilities of the Bluetooth LE Host Stack which are available on the KW45/KW47/MCXW72/FRDM-KW43 platform via the EdgeLock Secure Enclave (ELKE).
The security capabilities are enabled at application, Host and Controller level by setting Advanced Secure Mode to active. To do this, the user must set the gAppSecureMode_d macro to 1 in the project’s app_preinclude.h file. This macro is defined by default as 0 in app_preinclude_common.h:
#if (gAppSecureMode_d == 1U)
#define gHostSecureMode_d (1U)
#else
#define gHostSecureMode_d (0U)
#endif
At application level, when Advanced Secure Mode is enabled, the security mode and level for pairing is automatically enforced as Mode 1 Level 4, ensuring LE Secure Connections pairing. Legacy pairing is not supported in this mode.
When enabled, the main benefit of Advanced Secure Mode is the secured storage and handling of Bluetooth LE security keys. The EdgeLock Secure Enclave is capable of generating, importing, and exporting security keys as plain text or as encrypted blobs. All encrypted blobs are created by the EdgeLock Secure Enclave using a die unique key, which makes them impossible to decrypt by devices other than the one that created them. The Bluetooth LE security keys are managed in Advanced Secure Mode as follows:
IRK
The peer IRKs received after pairing and bonding are no longer stored into NVM as plaintext, but as encrypted blobs 40 bytes in length (or ELKE blobs). They can still be retrieved and converted to plaintext.
The local IRK is no longer generated using the default method of hashing over the board’s UID at every startup. It is instead generated once using the EdgeLock Secure Enclave and stored into a new NVM dataset as an ELKE blob.
Local and peer IRKs are no longer transmitted through HCI in plaintext but as EIRK (Encrypted IRK) blobs, 16 bytes in length, which can be decrypted by the Controller.
LTK
The LTK is no longer stored into NVM as plaintext, but as an ELKE blob. Furthermore, the plaintext of the LTK is never available to the Host/application. Generating the LTK via the ECDH process and generating the Session Key for individual connections is done by the Host via the EdgeLock Secure Enclave and custom vendor HCI messages which are transparent to the application.
CSRK
The local CSRK is no longer generated using the default method of hashing over the board’s UID at every startup. It is instead generated once using the EdgeLock Secure Enclave and stored into a new NVM dataset as an ELKE blob.
At startup, Advanced Secure Mode for the Controller is enabled dynamically by calling:
#if (defined(gAppSecureMode_d) && (gAppSecureMode_d > 0U))
(void) PLATFORM_EnableBleSecureKeyManagement();
#endif
This call can be found in BluetoothLEHost_Init, as part of the initialization sequence.
Additional considerations#
The Gap_LoadKeys API will return the IRK in plaintext, having converted it from the ELKE blob which is stored in the NVM. However, it cannot convert the LTK to plaintext - it will thus return the LTK in ELKE blob form.
As mentioned in the section above, the plaintext LTK is never available. Generating the Session Key for individual connections is done via the EdgeLock Secure Enclave by the Host, using the LTK in ELKE blob form. The Session Key is passed to the Controller via a custom vendor HCI message. Be aware that the content of the HCI_LE_Long_Term_Key_Request_Reply command is not the actual LTK and cannot be used for debugging.
The Host works with IRKs in ELKE blob form, therefore APIs such as Gap_EnableHostPrivacy and Gap_CreateRandomAddress take ELKE blobs as arguments. The Controller works with IRKs in EIRK blob form, therefore the Gap_EnableControllerPrivacy takes an EIRK blob as argument. This management is done in ble_conn_manager.c when Advanced Secure Mode is enabled.
Parent topic:Application Structure