MCUXpresso SDK Documentation

Acronyms

Acronyms#

The following acronyms are used in this document.

Acronym

Description

CS

Channel Sounding

PDE

Phase-based Distance Estimation

RTP

Round-Trip Phase

RTT

Rount-Trip Time

ToF

Time of Flight

MD

Measuring Device

RD

Reflector Device

EDLC

Early Detect Late Commit

SFD

Start-of-Frame Delimiter

T_FCS

The RF circuitry locks to the measurement channel (f_i). Devices can also use this time for additional internal calibrations, if necessary. The initiator may start to ramp up its output signal toward the end of this step.

T_FM

Time for Frequency Measurement

T_SY

Time for Synchronization sequence (CS packet)

T_IP1

Interlude Period 1 - transition from TX to RX and the other way around when transmitting in mode 1 (Tn-Tn)

T_IP2

Interlude Period 2 - transition from TX to RX and the other way around when transmitting in mode 2 (Tn-Tn)

T_GD

Transition time between packet and tone

T_RD

Ramp-Down time for transmission

T_PM

Single-antenna Phase Measurement period

N_AP

Number of Antenna Paths

T_SW

Antenna-Switching period

AGC

Automatic Gain Control

ADC

Analog-to-Digital Conversion

CDE

Complex Distance Estimation

IFFT

Inverse Fast Fourier Transform