Hardware product and feature information#
These query functions can be used to identify the product and its key features and to get VGLite driver information.
Enumerations for product and feature queries#
This section describes enumerations used for product and feature queries.
vg_lite_feature_t enumeration#
The following feature values may be queried for availability in compatible hardware. (expanded March 2023 to support additional hardware for driver V4)
Used in information function: vg_lite_query_feature.
|
Description |
|---|---|
gcFEATURE_BIT_VG_16PIXELS_ALIGN |
Require 16 pixels aligned for the input pixel buffer |
gcFEATURE_BIT_VG_24BIT |
RGB888 or RGBA5658 formats support |
gcFEATURE_BIT_VG_24BIT_PLANAR |
24-bit planar format support |
gcFEATURE_BIT_VG_AYUV_INPUT |
AYUV input format support |
gcFEATURE_BIT_VG_BORDER_CULLING |
Border culling support |
gcFEATURE_BIT_VG_COLOR_KEY |
Color key support. |
gcFEATURE_BIT_VG_COLOR_TRANSFORMATION |
Color transform support. |
gcFEATURE_BIT_VG_DEC_COMPRESS |
DEC compression format output support |
gcFEATURE_BIT_VG_DITHER |
Dither support |
gcFEATURE_BIT_VG_DOUBLE_IMAGE |
Support two image source inputs |
gcFEATURE_BIT_VG_FLEXA |
FLEXA interface support |
gcFEATURE_BIT_VG_GAMMA |
Gamma support |
gcFEATURE_BIT_VG_GAUSSIAN_BLUR |
Gaussian blur sampling support |
gcFEATURE_BIT_VG_GLOBAL_ALPHA |
Global alpha support |
gcFEATURE_BIT_VG_HW_PREMULTIPLY |
HW supports alpha premultiply for image |
gcFEATURE_BIT_VG_IM_DEC_INPUT |
DEC compressed format input support |
gcFEATURE_BIT_VG_IM_FASTCLEAR |
Fast Clear support |
gcFEATURE_BIT_VG_IM_INDEX_FORMAT |
Index format support for image |
gcFEATURE_BIT_VG_IM_INPUT |
Blit and draw API support |
gcFEATURE_BIT_VG_IM_REPEAT_REFLECT |
Image repeat reflect mode support |
gcFEATURE_BIT_VG_INDEX_ENDIAN |
Index format endian support |
gcFEATURE_BIT_VG_LINEAR_GRADIENT_EXT |
Support for extended linear gradient capabilities |
gcFEATURE_BIT_VG_LVGL_SUPPORT |
LVGL blend mode support |
gcFEATURE_BIT_VG_MASK |
Mask support |
gcFEATURE_BIT_VG_MIRROR |
Mirror support |
gcFEATURE_BIT_VG_NEW_BLEND_MODE |
New blend mode DARKEN/LIGHTEN support |
gcFEATURE_BIT_VG_NEW_IMAGE_INDEX |
New CLUT image index support |
gcFEATURE_BIT_VG_PARALLEL_PATHS |
New parallel path HW support |
gcFEATURE_BIT_VG_PE_CLEAR |
Pixel engine clear support |
gcFEATURE_BIT_VG_PIXEL_MATRIX |
Pixel matrix support |
gcFEATURE_BIT_VG_QUALITY_8X |
8x anti-aliasing path support |
gcFEATURE_BIT_VG_RADIAL_GRADIENT |
Radial gradient support |
gcFEATURE_BIT_VG_RECTANGLE_TILED_OUT |
Rectangle tiled output support |
gcFEATURE_BIT_VG_RGBA2_FORMAT |
RGBA2222 format support |
gcFEATURE_BIT_VG_RGBA8_ETC2_EAC |
ETC2/EAC compressed image format support |
gcFEATURE_BIT_VG_SCISSOR |
Scissor support |
gcFEATURE_BIT_VG_SRC_PREMULTIPLIED |
Source image alpha premultiplied |
gcFEATURE_BIT_VG_STENCIL |
Stencil image mode support |
gcFEATURE_BIT_VG_STRIPE_MODE |
Stripe mode support |
gcFEATURE_BIT_VG_TESSELLATION_TILED_OUT |
Tessellation tiled output support |
gcFEATURE_BIT_VG_USE_DST |
Read destination pixel support |
gcFEATURE_BIT_VG_YUV_INPUT |
YUV input format support |
gcFEATURE_BIT_VG_YUV_OUTPUT |
YUV format output support |
gcFEATURE_BIT_VG_YUV_TILED_INPUT |
YUV tiled input format support |
gcFEATURE_BIT_VG_YUY2_INPUT |
YUY2 input format support |
Parent topic:Enumerations for product and feature queries
Parent topic:Hardware product and feature information
Structures for product and feature queries#
This section describes structures used for product and feature queries.
vg_lite_info_t structure#
This structure is used to query VGLite driver information.
Used in function: vg_lite_get_info_t.
vg_lite_info_t member |
Type |
Description |
|---|---|---|
api_version |
vg_lite_uint32_t |
VGLite API version |
header_version |
vg_lite_uint32_t |
VGLite header version |
release_version |
vg_lite_uint32_t |
VGLite driver release version |
reserved |
vg_lite_uint32_t |
Reserved for future use |
Parent topic:Structures for product and feature queries
Parent topic:Hardware product and feature information
Functions for product and feature queries#
This section describes functions used for product and feature queries.
vg_lite_get_product_info#
Description:
This function is used to identify the VGLite-compatible product.
Syntax:
uint32_t vg_lite_get_product_info (
char *name,
uint32_t *chip_id,
uint32_t *chip_rev
);
Parameters:
Name |
Description |
|---|---|
|
A character array to store the name of the chip. |
|
Stores an ID number for the chip. |
|
Stores a revision number for the chip. |
Parent topic:Functions for product and feature queries
vg_lite_get_info#
Description:
This function is used to query the VGLite driver information.
Syntax:
vg_lite_error_t vg_lite_get_info (
vg_lite_info_t *info
);
Parameters:
Name |
Description |
|---|---|
|
Points to the VGLite driver information structure, which includes the API version, header version, and release version |
Parent topic:Functions for product and feature queries
vg_lite_get_register#
Description:
This function can be used to read a GPU AHB register value given the AHB byte address of a register. Refer to the appropriate Vivante GPU AHB register specification documents for register descriptions. The value range of AHB accessible addresses for VGLite cores is usually 0x0 to 0x1FF and 0xA00 to 0xA7F.
Syntax:
vg_lite_error_t vg_lite_get_register (
vg_lite_uint32_t address,
vg_lite_uint32_t *result
);
Parameters:
Name |
Description |
|---|---|
|
Byte Address of the register which value you want. |
|
The registers value. |
Parent topic:Functions for product and feature queries
vg_lite_query_feature#
Description:
This function is used to query if a specific feature is available.
Syntax:
vg_lite_uint32_t vg_lite_query_feature (
vg_lite_feature_t feature
);
Parameters:
Name |
Description |
|---|---|
|
Feature to be queried, as detailed in enum vg_lite_feature_t |
Returns:
The feature is either not supported (0) or supported (1).
Parent topic:Functions for product and feature queries
vg_lite_get_mem_size#
Description:
This function queries whether there is any remaining allocated contiguous video memory. (available from June 2020)
Syntax:
vg_lite_error_t vg_lite_get_mem_size(
vg_lite_uint32_t *size
);
Parameters:
Name |
Description |
|---|---|
|
Pointer to the remaining allocated contiguous video memory. |
Returns:
Returns VG_LITE_SUCCESS if the query is successful and memory is available. Returns VG_LITE_NO_CONTEXT if the driver is not initialized or there is no available memory.
Parent topic:Functions for product and feature queries
Parent topic:Hardware product and feature information