USB host FatFs throughput#
The following test is based on usb_host_msd_fatfs, bm, IAR, release target.
Test device - Sandisk extreme USB3.0 64G SDCZ80 - 64G |
|
|---|---|
Controller |
Write speed |
RT1050 EHCI |
~32163 KB/s |
K28FA KHCI |
~913 KB/s |
LPCXpresso54628 IP3516 |
~22034 KB/s |
LPCXpresso54628 OHCI |
~860 KB/s |