MCUXpresso SDK Documentation

MCUXpresso IDE

MCUXpresso IDE#

  1. Rearrange source files

    1. For RT1170, import dev_msc_disk_bm_cm7 and dev_hid_mouse_bm_cm4 example. For RT1180, import dev_msc_disk_bm_cm33 and dev_hid_mouse_bm_cm4 example.

    2. Open the directory of the two examples in the file explorer.

    3. For RT1170, compare the whole project directory and add the folders that are in the cm7 project but not cm4 to the cm4 project. For RT1180, compare the whole project directory and add the folders that are in the cm33 project but not cm7 to the cm7 project.

    4. Compare the two folders. For RT1170, delete the files that are in the cm4 project but not cm7 and add the files that are in the cm7 project but not cm4 to the cm4 project. For RT1180, delete the files that are in the cm7 project but not cm33 and add the files that are in the cm33 project but not cm7 to the cm7 project. In the RT1170 case,

    • For the board, source, and usb folders, replace them in the cm4 project with the ones in the cm7 directory.

      |

|

-   For the `component` folder, delete the `timer` folder in the `cm4` directory.

    |![](../images/image26.png)

|

-   For the `drivers` folder, delete `fsl_pit` source files in the `cm4` project and add `fsl_usdhc` source files to the `cm4` directory.

    |![](../images/image27.png)

|

-   For the `sdmmc` folder, copy it to the `cm4` project.

    |![](../images/image28.png)

|

  1. Rearrange project files

    After the source files are updated, the project files are loaded to the cm4 project of RT1170 or the cm7 project of RT1180 automatically. No manual updates to the project files are required.

    Due to the deletion in the first step, for the board, source and usb folders, an option must be deleted in the properties. Right click board -> properties -> C/C++build and uncheck Exclude resource from build. Perform the same operation in the source and usb folders. Take RT1170 as an example:

    |

|

  1. Adjust project settings

    Note: The following steps are described for RT1170. However, these steps are also applicable for RT1180.

    1. Compare the macro in the project settings, by clicking Properties -> C/C++ Build -> Setting -> MCU C Compiler -> Preprocessor. Add the macro that is in the cm7 project but not in cm4 to the cm4 project.

      In this case, the macro is SD_ENABLED.

      |

|

2.  Change the include paths in the project settings, by clicking **Properties** -\> **C/C++ Build** -\> **Setting** -\> **MCU C Compiler** -\> **Includes**, according to the changes of project files.

    In this case, delete the paths framed in the red box and add the paths in the green box.

    |![](../images/image31.png)

|

  1. Change project name

    1. Right-click project name > rename, change the filename dev_hid_mouse_bm_cm4 to dev_msc_disk_bm_cm4, and then click OK.

      |

|

With all above steps done, the RT1170 M7 project successfully changes to an M4 project and the M4 example USB project is available for downloading and debugging. The RT1180 M33 project successfully changes to an M7 project and the M7 example USB project is downloading and debugging.