Version 1.6.0#
New major features#
MCUboot updated to v1.9.0.
Mbed TLS updated to v3.1.0 (Support all required PSA Crypto APIs).
Enabled Secure Function (SFN) Model Partition compliance in IPC backend.
Interrupt support (both SLIH/FLIH) for the SFN backend.
MM-IOVEC Support for the SFN backend.
The following Secure Partitions are converted to SFN model:
Protected Storage
Internal Trusted Storage
Initial Attestation
FF-M v1.1 SFN Model supported in Profile Small.
HAL Separation of Library Model and IPC/SFN backend.
FP support for Armv8.1-M Mainline for IPC backend.
Simplified build output message and configurable output.
Halting instead of rebooting on panic in debug build type.
- 1PSA Unified Driver spec
Automated testing of MCUboot BL2.
A new driver interface for the CC-312 runtime library as specified in the PSA Unified Driver spec 1PSA Unified Driver spec.
Added reference bootloader stage 1 (BL1) bootloader for certain platforms.
A new CC312 ROM library for the BL1.
Updated documentation structure.
New security advisories#
New platforms supported#
Deprecated platforms#
None
Tested platforms#
The following platforms are successfully tested in this release.
AN519
AN521
AN547
B-U585I-IOT02A
Corstone-1000
Corstone-Polaris
LPCXpresso55S69
Musca-B1
Musca-S1
nrf9160
nrf5340
NUCLEO-L552ZE-Q
PSoC 64
STM32L562E-DK
Known issues#
Some open issues are not fixed in this release.
Descriptions |
Issue links |
PSA Arch framework test suite has several known failures.
|
3PSA Arch framework test failuresPSA Arch framework test failures 3PSA Arch framework test failures |
Issues closed since v1.5.0#
The following issues in v1.5.0 known issues list are closed.
Descriptions |
Issue links |
2Arm Compiler 6.18 release note:
Arm Compiler [SDCOMP-59788]. See the Arm Compiler 6.18 release note 2Arm Compiler 6.18 release note: For details.
|
Reference#
Copyright (c) 2022-2023, Arm Limited. All rights reserved.