MCUXpresso SDK Documentation

Version 1.1#

New Features#

  • Upgraded MCUBoot to v1.6.0., default is now the upstream MCUBoot instead of the TF-M fork.

  • TF-Fuzz tool for fuzz testing PSA APIs.

  • Updated Source code folder structure.

  • IAR compiler support.

  • LPCXpresso55S69-EVK board support.

  • Add Profile Small.

  • Enable Ninja CMake Generator.

  • FVP_SSE300_MPS2 platform support.

  • Rename SST(Secure STorage) to PS(Protected Storage) and partition moved from PSA Root of Trust to Application Root of Trust.

  • NUCLEO-L552ZE-Q and DISCO-L562QE platform support.

  • Restructure documentation to make it more user-friendly.

  • Enable Attestation service to use symmetric key algorithm.

  • Use CMSIS for testing from tf-m-tests repository. This removes dependency on the external CMSIS_5 repo.

New Platforms supported#

New Platforms limitations#

  • LPCXpresso55S69-EVK doesn’t support BL2.

  • LPCXpresso55S69-EVK doesn’t support ARMCLANG and IARARM toolchain. Patch with support for IARARM is available at review.trustedfirmware.org #4023

  • FVP_SSE300_MPS2 doesn’t support GNUARM and IARARM toolchain. Patch with support for IARARM is available at review.trustedfirmware.org #4574

Known issues#

Some open issues exist and will not be fixed in this release.

All the supported GNUARM toolchain versions generate corrupt veneer
code for Armv8-M baseline architecture, when the -Os optimization flag
is used. This affects the AN519 and AN539 platforms built with GNUARM
toolchain and Minsizerel build type.

Issue: https://gcc.gnu.org/bugzilla/show_bug.cgi?id=95646

PSA Arch Crypto tests have several known failures.

See this link for detailed analysis of the failures : ARM-software/psa-arch-tests

AN521 FVP soft reset via AIRCR does not reset MPC / PPC / MPU and will
cause boot failure. This is known issue for AN521 FVP. This will cause
the system to not boot after a warm reset during PSA Arch FF testing.

Issue: https://developer.trustedfirmware.org/T692

There are 2 additional failures for PSA-Arch Crypto tests with CC-312
other than the known failures. This is due to limitation of CC-312
implementation as it does not support MD_NONE hashing mode causing the
additional failures.

Issue: https://developer.trustedfirmware.org/T691

Boot up fails if there is unexpected data in flash on Musca-A. The boot
is successful and the tests pass if all the associated (PS/ITS/NV
Counter) flash areas are erased.

Issue: https://developer.trustedfirmware.org/T694

When PS/ITS are using Flash on Musca-B1, PSA Arch FF test fails due to
known warm reset limitation in the platform. There is an issue with
Musca-B1 QSPI flash that causes this failure. The fix is under
investigation.

Issue: https://developer.trustedfirmware.org/T696

Issues fixed since 1.0#

The eflash driver on Musca-B1 can return random failures hence
triggering random failures during PSA Arch ITS and PSA Arch PS tests.
This happens when ITS/SST is configured to use flash.

Issue: https://developer.trustedfirmware.org/T697

Release build of PSA Arch Crypto tests have a different number of tests
when built for AN521 FVP. This is an issue in the PSA Arch Crypto
tests.

Issue for PSA Arch Tests project : ARM-software/psa-arch-tests#169


Copyright (c) 2020, Arm Limited. All rights reserved.