STM32H5#
TF-M is supported on STM32H5 family
https://www.st.com/en/microcontrollers-microprocessors/stm32h5-series.html
Directory content#
- stm/common/stm32h5xx/stm32h5xx_hal:
Content from STMicroelectronics/stm32h5xx_hal_driver
- stm/common/stm32h5xx/Device:
Content from STMicroelectronics/cmsis_device_h5
- stm/common/stm32h5xx/bl2:
stm32h5xx bl2 code specific from STMicroelectronics/STM32CubeH5.git (Projects/STM32H573I_DK/Applications/TFM)
- stm/common/stm32h5xx/secure:
stm32h5xx Secure porting adaptation from STMicroelectronics/STM32CubeH5.git (Projects/STM32H573I_DK/Applications/TFM)
- stm/common/stm32h5xx/boards:
Adaptation and tools specific to stm32 board using stm32h5xx soc from STMicroelectronics/STM32CubeH5.git (Projects/STM32H573I_DK/Applications/TFM)
- stm/common/stm32h5xx/CMSIS_Driver:
Flash and uart driver for stm32h5xx platform
- stm/common/stm32h5xx/Native_Driver:
Random generator and tickless implementation
Specific Software Requirements#
STM32_Programmer_CLI is required.(see https://www.st.com/en/development-tools/stm32cubeprog.html)
Limitations to Consider When Using the Platform#
MPU and ICACHE disabled in bl2 boot stage
Write software on target#
In build folder:
postbuild.sh: Updates regression.sh and TFM_UPDATE.sh scripts according to flash_layout.h
regression.sh: Sets platform option bytes config and erase platform
TFM_UPDATE.sh: Writes bl2, secure, and non secure image in target
Connect board to USB and Execute the 3 scripts in following order to update platform: postbuild.sh, regression.sh, TFM_UPDATE.sh
The virtual com port from STLINK is used for TFM log and serial port configuration should be:
Baud rate = 115200
Data = 8 bits
Parity = none
Stop = 1 bit
Flow control = none
Copyright (c) 2023 STMicroelectronics. All rights reserved. SPDX-License-Identifier: BSD-3-Clause