LPCXpresso55S69#
1. Building TF-M#
Prepare the tf-m-tests repository inside the TF-M base folder.
cd <TF-M base folder>
git clone https://git.trustedfirmware.org/TF-M/tf-m-tests.git
There are two options for the TF-M build - with or without secondary bootloader (BL2).
1.1 Building TF-M demo without BL2#
To build S and NS application image without a BL2, run the following commands:
cd <TF-M base folder>/tf-m-test/tests_reg
cmake -S spe -B build_spe -DTFM_PLATFORM=nxp/lpcxpresso55s69 -DCONFIG_TFM_SOURCE_PATH=<TF-M base folder>/trusted-firmware-m -G"Unix Makefiles" -DBL2=OFF
cmake --build build_spe -- install
cmake -S . -B build_test -G"Unix Makefiles" -DCONFIG_SPE_PATH=<TF-M base folder>/tf-m-tests/tests_reg/build_spe/api_ns
cmake --build build_test
1.2 Building TF-M demo with BL2#
To build S and NS application along with a BL2, run the following commands:
cd <TF-M base folder>/tf-m-test/tests_reg
cmake -S spe -B build_spe -DTFM_PLATFORM=nxp/lpcxpresso55s69 -DCONFIG_TFM_SOURCE_PATH=<TF-M base folder>/trusted-firmware-m -G"Unix Makefiles" -DBL2=ON
cmake --build build_spe -- install
cmake -S . -B build_test -G"Unix Makefiles" -DCONFIG_SPE_PATH=<TF-M base folder>/tf-m-tests/tests_reg/build_spe/api_ns
cmake --build build_test
1.3 Building TF-M regression tests#
To buld the S and NS regression tests without BL2, run the following commands:
cd <TF-M base folder>/tf-m-test/tests_reg
cmake -S spe -B build_spe -DTFM_PLATFORM=nxp/lpcxpresso55s69 -DCONFIG_TFM_SOURCE_PATH=<TF-M base folder>/trusted-firmware-m -G"Unix Makefiles" -DTEST_S=ON -DTEST_NS=ON -DBL2=OFF
cmake --build build_spe -- install
cmake -S . -B build_test -G"Unix Makefiles" -DCONFIG_SPE_PATH=<TF-M base folder>/tf-m-tests/tests_reg/build_spe/api_ns
cmake --build build_test
2. Flashing TF-M with PyOCD#
PyOCD is an open source Python package for programming and debugging Arm Cortex-M microcontrollers using multiple supported types of USB debug probes. See: PyOCD <https://pypi.org/project/pyocd/>
If you built TF-M with the BL2 secondary bootloader, use the following commands:
pyocd erase --mass -t LPC55S69
pyocd flash build_spe/bin/bl2.hex -t LPC55S69
pyocd flash build_test/tfm_s_ns_signed.bin --base-address 0x8000 -t LPC55S69
When BL2 is disabled, flash the generated hex secure and non-secure images:
pyocd erase --mass -t LPC55S69
pyocd flash build_spe/bin/tfm_s.hex build_test/bin/tfm_ns.hex -t LPC55S69
Note
There is sometimes a stability issue with the pyocd flash erasing, it is needed to rerun the pyocd erase command again.
Copyright (c) 2020, Linaro. All rights reserved. Copyright (c) 2020-2021, Arm Limited. All rights reserved. Copyright 2020-2024 NXP. All rights reserved. *SPDX-License-Identifier: BSD-3-Clause