NuMaker-PFM-M2354#
Building TF-M#
Build TF-M regression test with M2354 by following commands:
$ cd tf-m-test/tests_reg
$ cmake -S spe -B build_spe \
-G"Unix Makefiles" \
-DTFM_PLATFORM=nuvoton/m2354 \
-DTFM_TOOLCHAIN_FILE=[tf-m path]/toolchain_GNUARM.cmake \
-DCMAKE_BUILD_TYPE=Release \
-DTEST_S=ON -DTEST_NS=ON
$ cmake --build build --parallel -- install
$ cmake -S . -B build_test \
-G"Unix Makefiles" \
-DCONFIG_SPE_PATH=[tf-m-tests path]/tests_reg/build_spe/api_ns \
-DTFM_TOOLCHAIN_FILE=cmake/toolchain_ns_GNUARM.cmake \
-DCMAKE_BUILD_TYPE=Release \
$ cmake --build build_test --parallel -- install
Define TEST_NS=ON or TEST_S=ON for non-secure or secure regression test. CMAKE_BUILD_TYPE could be “Release”, “RelWithDebInfo” or “Minsizerel” Other cmake parameters should not be changed.
Flashing Image with Nuvoton NuLink Tool#
NuMaker-PFM-M2354 board supports on board ICE called NuLink. Connect NuLink to PC with USB cable and using NuLink Command Tool to flashing the image.
The commands are as follows:
> NuLink_M2354 -C
> NuLink_M2354 -E ALL
> NuLink_M2354 -W NSCBA 0x80000 0
> NuLink_M2354 -S
> NuLink_M2354 -C
> NuLink_M2354 -W APROM .\build_spe\bin\bl2.bin 0
> NuLink_M2354 -W APROM .\build_spe\bin\tfm_s_signed.bin 0 0x20000 0
> NuLink_M2354 -W APROMNS .\build_test\bin\tfm_ns_signed.bin 0
Copyright (c) 2021-2023, Nuvoton Technology Corp. All rights reserved.