Adding Secure Partition#
Terms and abbreviations#
This document uses the following terms and abbreviations.
Term |
Meaning |
|---|---|
FF-M |
Firmware Framework for M |
ID |
Identifier |
IPC |
Interprocess communication |
IPC model |
The secure IPC framework |
irqs |
Interrupt requests |
MMIO |
Memory Mapped I/O |
PSA |
Platform Security Architecture |
RoT |
Root of Trust |
SFN |
Secure Function |
SFN model |
Secure Function model |
SID |
RoT Service ID |
SP |
Secure Partition |
SPM |
Secure Partition Manager |
TF-M |
Trusted firmware M |
Introduction#
Secure Partition is an execution environment that provides the following functions to Root of Trust (RoT) Services:
Access to resources, protection of its own code and data.
Mechanisms to interact with other components in the system.
Each Secure Partition is a single thread of execution and the smallest unit of isolation.
This document mainly describes how to add a secure partition in TF-M and focuses on the configuration, manifest, implement rules. The actual source-level implementation is not included in this document.
Note
If not otherwise specified, the steps are identical for IPC and SFN model.
The IPC and SFN model conforms to the PSA Firmware Framework for M (FF-M) v 1.1 changes. Refer to PSA Firmware Framework specification and Firmware Framework for M 1.1 Extensions for details.
Process#
The main steps to add a secure partition are as follows:
Add source folder#
Add a source folder under <TF-M base folder>/secure_fw/partitions for the
new secure partition (Let’s take example as the folder name):
This folder should include those parts:
Manifest file
CMake configuration files
Source code files
Add manifest#
Each Secure Partition must have resource requirements declared in a manifest file. The Secure Partition Manager (SPM) uses the manifest file to assemble and allocate resources within the SPE. The manifest includes the following:
A Secure Partition name.
A list of implemented RoT Services.
Access to other RoT Services.
Memory requirements.
Scheduling hints.
Peripheral memory-mapped I/O regions and interrupts.
Note
The current manifest format in TF-M is “yaml” which is different from the requirement of PSA FF.
Note
The users can use LOW, NORMAL and HIGH to determine the priority of the Secure Partition in manifest. They are replaced by 01, 02 and 03 auotmatically when parsing manifest lists for section naming.
Here is a manifest reference example for the IPC model:
Note
To use SFN model, the user needs to replace "model": "IPC" to
"model": "SFN". The user also needs to remove the attribute
"entry_point", and optionally replace it with "entry_init".
{
"psa_framework_version": 1.1,
"name": "TFM_SP_EXAMPLE",
"type": "APPLICATION-ROT",
"priority": "NORMAL",
"model": "IPC",
"entry_point": "tfm_example_main",
"stack_size": "0x0200",
"services" : [
{
"name": "ROT_A",
"sid": "0x000000E0",
"non_secure_clients": true,
"connection_based": true,
"version": 1,
"version_policy": "STRICT"
"mm_iovec": "disable"
}
],
"mmio_regions": [
{
"name": "TFM_PERIPHERAL_A",
"permission": "READ-WRITE"
}
],
"irqs": [
{
"source": "TFM_A_IRQ",
"name": "A_IRQ",
"handling": "SLIH"
}
]
"dependencies": [
"TFM_CRYPTO",
"TFM_INTERNAL_TRUSTED_STORAGE_SERVICE"
]
}
Update manifest list#
The <TF-M base folder>/tools/tfm_manifest_list.yaml is used to collect
necessary information of secure partition.
The manifest tool tools/tfm_parse_manifest_list.py processes it and
generates necessary files while building.
Please refer to the Manifest List for the format of manifest lists.
Reference configuration example:
{
"description": "TFM Example Partition",
"manifest": "secure_fw/partitions/example/tfm_example_partition.yaml",
"conditional": "@TFM_PARTITION_EXAMPLE@",
"output_path": "partitions/example",
"version_major": 0,
"version_minor": 1,
"pid": 290,
"linker_pattern": {
"library_list": [
"*tfm_*partition_example*"
]
}
}
TF-M also supports out-of-tree Secure Partition build where you can have your own manifest lists. Please refer to Out-of-tree Secure Partition build for details.
Secure Partition ID Distribution#
Every Secure Partition has an identifier (ID). TF-M will generate a header file
that includes definitions of the Secure Partition IDs. The header file is
<TF-M build folder>generated/interface/include/psa_manifest/pid.h. Each
definition uses the name attribute in the manifest as its name and the
value is allocated by SPM.
The Partition ID can be set to a fixed value or omitted to be auto allocated.
#define name id-value
Secure Partitions |
PID Range |
|---|---|
TF-M Internal Partitions |
0 - 255 |
PSA and user Partitions |
256 - 2999 |
TF-M test Partitions |
3000 - 4999 |
Firmware Framework test Partitions |
5000 - 5999 |
Reserved |
6000 - |
Please refer to <TF-M base folder>/tools/tfm_manifest_list.yaml,
<TF-M test repo>/test/secure_fw/tfm_test_manifest_list.yaml and
<TF-M base folder>/tools/tfm_psa_ff_test_manifest_list.yaml for the detailed
PID allocations.
About where to add the definition, please refer to the chapter Update manifest list.
RoT Service ID (SID) Distribution#
An RoT Service is identified by its RoT Service ID (SID). A SID is a 32-bit number that is associated with a symbolic name in the Secure Partition manifest. The bits [31:12] uniquely identify the vendor of the RoT Service. The remaining bits [11:0] can be used at the discretion of the vendor.
Here is the RoT Service ID table used in TF-M.
Partitions |
Vendor ID(20 bits) |
Function ID(12 bits) |
|---|---|---|
initial_attestation |
0x00000 |
0x020-0x03F |
platform |
0x00000 |
0x040-0x05F |
protected_storage |
0x00000 |
0x060-0x06F |
internal_trusted_storage |
0x00000 |
0x070-0x07F |
crypto |
0x00000 |
0x080-0x09F |
firmware_update |
0x00000 |
0x0A0-0x0BF |
tfm_secure_client |
0x0000F |
0x000-0x01F |
tfm_ipc_client |
0x0000F |
0x060-0x07F |
tfm_ipc_service |
0x0000F |
0x080-0x09F |
tfm_slih_test_service |
0x0000F |
0x0A0-0x0AF |
tfm_flih_test_service |
0x0000F |
0x0B0-0x0BF |
tfm_ps_test_service |
0x0000F |
0x0C0-0x0DF |
tfm_secure_client_2 |
0x0000F |
0x0E0-0x0FF |
tfm_sfn_test_service_1 |
0x0000F |
0x100-0x11F |
tfm_sfn_test_service_2 |
0x0000F |
0x120-0x13F |
tfm_attest_test_service |
0x0000F |
0x140-0x15F |
RoT Service Stateless Handle Distribution#
A Secure partition may include stateless services. They are distinguished and
referenced by stateless handles. In manifest, a stateless_handle attribute
is set for indexing stateless services. It must be either "auto" or a
number in the range [1, 32] in current implementation and may extend. Also the
connection-based attribute must be set to false for stateless services.
The indexes of stateless handles are divided into two ranges for different
usages.
Indexes [1, 16] are assigned to TF-M Secure Partitions.
The rest indexes [17, 32] are reserved for any other Secure Partitions, for
example Secure Partitions in tf-m-tests and tf-m-extras.
The following table summaries the stateless handle allocation for the TF-M Secure Partitions.
Partition name |
Stateless Handle |
|---|---|
TFM_SP_CRYPTO |
1 |
TFM_SP_PS |
2 |
TFM_SP_ITS |
3 |
TFM_SP_INITIAL_ATTESTATION |
4 |
TFM_SP_FWU |
5 |
TFM_SP_PLATFORM |
6 |
For the indexes of other Secure Partitions, please refer to their manifests or documentations.
stack_size#
The stack_size is required to indicate the stack memory usage of the Secure
Partition.
The value of this attribute must be a decimal or hexadecimal value in bytes.
It can also be a build configurable with default value defined in
config_base.cmake.
The value of the configuration can be overridden to fit different use cases.
heap_size#
This attribute is optional. The default value is 0.
It indicates the heap memory usage of the Secure Partition.
The allowed values are the same as the stack_size.
mmio_regions#
This attribute is a list of MMIO region objects which the Secure Partition
needs access to. TF-M only supports the named_region current. Please refer
to PSA FF for more details about it. The user needs to provide a name macro to
indicate the variable of the memory region.
TF-M uses the below structure to indicate a peripheral memory.
struct platform_data_t {
uint32_t periph_start;
uint32_t periph_limit;
int16_t periph_ppc_bank;
int16_t periph_ppc_loc;
};
Note
This structure is not expected by TF-M, it’s only that the current implementations are using. Other peripherals that need different information to create isolation need to define a different structure with the same name.
Here is an example for it:
struct platform_data_t tfm_peripheral_A;
#define TFM_PERIPHERAL_A (&tfm_peripheral_A)
mm_iovec#
Memory-mapped iovecs (MM-IOVEC) provides direct mapping of client input and output vectors into the
Secure Partition.
When this attribute is set to enable, it enables Secure Partitions to use the MM-IOVEC APIs if
the framework supports MM-IOVEC.
Using MM-IOVEC provides a memory and runtime optimization for larger buffers, but reduces mitigation for common security vulnerabilities. Please refer to Firmware Framework for M 1.1 Extensions for more details. Whether to use MM-IOVEC depends on the requirements of memory and runtime optimization and security.
Update the Build System#
The following changes to the build system are required for the newly added secure partition.
Add a CMakeLists.txt file#
Each Secure Partition must have a corresponding CMakeLists.txt, in this case,
<TF-M base folder>/secure_fw/partitions/example/CMakeLists.txt, which is the compilation
configuration for this Secure Partition.
Here is a reference example for CMakeLists.txt
The CMake file should include the following contents
Add library
tfm_app_rot_partition_exampleand associated source files.add_library(tfm_app_rot_partition_example STATIC) target_sources(tfm_app_rot_partition_example PRIVATE tfm_example_partition.c )
Note
The secure partition must be built as a standalone static library, and the name of the library must follow this pattern, as it affects how the linker script will lay the partition in memory:
tfm_psa_rot_partition*in case of a PSA RoT partitiontfm_app_rot_partition*in case of an Application RoT partition
Add source files generated by the manifest tool.
# The intermedia file defines the partition stack. target_sources(tfm_app_rot_partition_example PRIVATE ${CMAKE_BINARY_DIR}/generated/example_partition/auto_generated/intermedia_tfm_example_partition.c ) # The load info file includes the static data of the partition. target_sources(tfm_partitions INTERFACE ${CMAKE_BINARY_DIR}/generated/example_partition/auto_generated/load_info_tfm_example_partition.c )
Add dependency with manifest tool.
To make sure the above generated files are up-to-date when the Secure Partition library is built, dependencies between the library and the manifest tool target should be set up.
add_dependencies(tfm_app_rot_partition_example manifest_tool)
Link
tfm_sprtfor the PSA API interfaces.target_link_libraries(tfm_app_rot_partition_example PRIVATE tfm_sprt )
Link the Secure Partition library to
tfm_partitionsso that it can be included in the final image.target_link_libraries(tfm_partitions INTERFACE tfm_app_rot_partition_example )
Finally, the build of this Secure Partition should be added to
<TF-M base folder>/secure_fw/partitions/CMakeLists.txt.
add_subdirectory(example)
Update the Config System#
If the Secure Partition has the build config to enable or disable it, the config option should be added to config systems.
CMake Config#
The default value of the config option should be added to the
<TF-M base folder>/config/config_base.cmake.
set(TFM_PARTITION_EXAMPLE OFF CACHE BOOL "Enable the example partition")
Kconfig#
A menuconfig should be added to <TF-M base folder>/secure_fw/partitions/example/Kconfig.
menuconfig TFM_PARTITION_EXAMPLE bool "Enable the Example Partition" default n
And add it to <TF-M base folder>/secure_fw/partitions/Kconfig
rsource ``example/Kconfig``
Note
The Secure Partition building should be skipped if it is not enabled.
This should be done by adding the following code at the begining of its CMakeLists.txt
if (NOT TFM_PARTITION_EXAMPLE)
return()
endif()
Implement the RoT services#
To implement RoT services, the partition needs a source file which contains the
implementations of the services, as well as the partition entry point. The user
can create this source file under
<TF-M base folder>/secure_fw/partitions/example/tfm_example_partition.c.
As an example, the RoT service with SID ROT_A will be implemented.
Entry point for IPC Model Partitions#
This function must have a loop that repeatedly waits for input signals and then processes them, following the Secure Partition initialization.
#include "psa_manifest/tfm_example.h"
#include "psa/service.h"
void tfm_example_main(void)
{
psa_signal_t signals = 0;
/* Secure Partition initialization */
example_init();
/*
* Continually wait for one or more of the partition's RoT Service or
* interrupt signals to be asserted and then handle the asserted
* signal(s).
*/
while (1) {
signals = psa_wait(PSA_WAIT_ANY, PSA_BLOCK);
if (signals & ROT_A_SIGNAL) {
rot_A();
} else {
/* Should not come here */
psa_panic();
}
}
}
Entry init for SFN Model Partitions#
In the SFN model, the Secure Partition consists of one optional initialization
function, which is declared as the entry_init symbol as mentioned in
section Add manifest. After initialization, the entry_init function
returns the following values:
Return
PSA_SUCCESSif initialization succeeds.Return
PSA_SUCCESSif initialization is partially successful, and you want some SFNs to receive messages. RoT Services that are non-operational must respond to connection requests withPSA_ERROR_CONNECTION_REFUSED.Return an error status if the initialization failed, and no SFNs within the Secure Partition must be called.
Service implementation for IPC Model#
The service is implemented by the rot_A() function, which is called upon an
incoming signal. This implementation is up to the user, however an example
service has been included for reference. The following example sends a message
“Hello World” when called.
#include "psa_manifest/tfm_example.h"
#include "psa/service.h"
/* Some other type of services. */
#define SOME_ROT_A_SERVICE_TYPE (1)
static void rot_A(void)
{
const int BUFFER_LEN = 32;
psa_msg_t msg;
int i;
uint8_t rec_buf[BUFFER_LEN];
uint8_t send_buf[BUFFER_LEN] = "Hello World";
psa_get(ROT_A_SIGNAL, &msg);
switch (msg.type) {
case PSA_IPC_CONNECT:
case PSA_IPC_DISCONNECT:
/*
* This service does not require any setup or teardown on connect
* or disconnect, so just reply with success.
*/
psa_reply(msg.handle, PSA_SUCCESS);
break;
default:
/* Handling services requested by psa_call. */
if (msg.type == PSA_IPC_CALL) {
for (i = 0; i < PSA_MAX_IOVEC; i++) {
if (msg.in_size[i] != 0) {
psa_read(msg.handle, i, rec_buf, BUFFER_LEN);
}
if (msg.out_size[i] != 0) {
psa_write(msg.handle, i, send_buf, BUFFER_LEN);
}
}
psa_reply(msg.handle, PSA_SUCCESS);
} else if (msg.type == SOME_ROT_A_SERVICE_TYPE) {
/* Operations for SOME_ROT_A_SERVICE_TYPE */
} else {
/* Invalid type for this Secure Partition. */
return PSA_ERROR_PROGRAMMER_ERROR;
}
}
}
Service implementation for SFN Model#
SFN model consists of a set of Secure Functions (SFN), one for each RoT Service. The connection, disconnection and request messages do not cause a Secure Partition signal to be asserted for SFN Secure Partitions. Instead, the Secure Function (SFN) for the RoT Service is invoked by the framework, with the message details provided as a parameter to the SFN. To add a secure function (SFN) to process messages for each RoT Service, each SFN will have following prototype.
psa_status_t <<name>>_sfn(const psa_msg_t *msg);
A connection-based example service has been included for reference which sends a message “Hello World” when called.
#include "psa_manifest/tfm_example.h"
#include "psa/service.h"
/* Some other type of services. */
#define SOME_ROT_A_SERVICE_TYPE (1)
psa_status_t rot_a_sfn(const psa_msg_t *msg)
{
const int BUFFER_LEN = 32;
int i;
uint8_t rec_buf[BUFFER_LEN];
uint8_t send_buf[BUFFER_LEN] = "Hello World";
switch (msg->type) {
case PSA_IPC_CONNECT:
case PSA_IPC_DISCONNECT:
/*
* This service does not require any setup or teardown on connect
* or disconnect, so just reply with success.
*/
return PSA_SUCCESS;
default:
/* Handling services requested by psa_call. */
if (msg->type == PSA_IPC_CALL) {
for (i = 0; i < PSA_MAX_IOVEC; i++) {
if (msg->in_size[i] != 0) {
psa_read(msg->handle, i, rec_buf, BUFFER_LEN);
}
if (msg.->out_size[i] != 0) {
psa_write(msg->handle, i, send_buf, BUFFER_LEN);
}
}
return PSA_SUCCESS;
} else if (msg->type == SOME_ROT_A_SERVICE_TYPE) {
/* Operations for SOME_ROT_A_SERVICE_TYPE */
} else {
/* Invalid type for this Secure Partition. */
return PSA_ERROR_PROGRAMMER_ERROR;
}
}
}
Test suites and test partitions#
A regression test suite can be added to verify whether the new secure partition works as expected. Refer to Adding TF-M Regression Test Suite for the details of adding a regression test suite.
Some regression tests require a dedicated RoT service. The implementations of the RoT service for test are similar to secure partition addition. Refer to Adding partitions for regression tests to get more information.
Out-of-tree Secure Partition build#
TF-M supports out-of-tree Secure Partition build, whose source code folders
are maintained outside TF-M repo. Developers can configure
TFM_EXTRA_MANIFEST_LIST_FILES and TFM_EXTRA_PARTITION_PATHS in build
command line to include out-of-tree Secure Partitions.
TFM_EXTRA_MANIFEST_LIST_FILESA list of the absolute path(s) of the manifest list(s) provided by out-of-tree Secure Partition(s). Use semicolons
;to separate multiple manifest lists. Wrap the multiple manifest lists with double quotes.TFM_EXTRA_PARTITION_PATHSA list of the absolute directories of the out-of-tree Secure Partition source code folder(s). TF-M build system searches
CMakeLists.txtof partitions in the source code folder(s). Use semicolons;to separate multiple out-of-tree Secure Partition directories. Wrap the multiple directories with double quotes.
A single out-of-tree Secure Partition folder can be organized as the figure below.
secure partition folder
├── CMakeLists.txt
├── manifest_list.yaml
├── out_of_tree_partition_manifest.yaml
└── source code
In the example above, TFM_EXTRA_MANIFEST_LIST_FILES and
TFM_EXTRA_PARTITION_PATHS in the build command can be configured as listed
below.
-DTFM_EXTRA_MANIFEST_LIST_FILES=<Absolute-path-sp-folder/manifest_list.yaml>
-DTFM_EXTRA_PARTITION_PATHS=<Absolute-path-sp-folder>
Multiple out-of-tree Secure Partitions can be organized in diverse structures. For example, multiple Secure Partitions can be maintained under the same directory as shown below.
top-level folder
├── Partition 1
│ ├── CMakeLists.txt
│ ├── partition_1_manifest.yaml
│ └── source code
├── Partition 2
│ └── ...
├── Partition 3
│ └── ...
├── manifest_list.yaml
└── Root CMakeLists.txt
In the example above, a root CMakeLists.txt includes all the partitions’
CMakLists.txt, for example via add_subdirectory(). The manifest_list.yaml
lists all partitions’ manifest files.
TFM_EXTRA_MANIFEST_LIST_FILES and TFM_EXTRA_PARTITION_PATHS in build
command line can be configured as listed below.
-DTFM_EXTRA_MANIFEST_LIST_FILES=<Absolute-path-top-level-folder/manifest_list.yaml>
-DTFM_EXTRA_PARTITION_PATHS=<Absolute-path-top-level-folder>
Alternatively, out-of-tree Secure Partitions can be separated in different folders.
partition 1 folder partition 2 folder
├── CMakeLists.txt ├── CMakeLists.txt
├── manifest_list.yaml ├── manifest_list.yaml
├── partition_1_manifest.yaml ├── partition_2_manifest.yaml
└── source code └── source code
In the example above, each Secure Partition manages its own manifest files and
CMakeLists.txt. TFM_EXTRA_MANIFEST_LIST_FILES and
TFM_EXTRA_PARTITION_PATHS in build command line can be configured as listed
below. Please note those input shall be wrapped with double quotes.
-DTFM_EXTRA_MANIFEST_LIST_FILES="<Absolute-path-part-1-folder/manifest_list.yaml>;<Absolute-path-part-2-folder/manifest_list.yaml>"
-DTFM_EXTRA_PARTITION_PATHS="<Absolute-path-part-1-folder>;<Absolute-path-part-2-folder>"
Note
Manifest list paths in TFM_EXTRA_MANIFEST_LIST_FILES do NOT have to be
one-to-one mapping to Secure Partition directories in
TFM_EXTRA_PARTITION_PATHS. The orders don’t matter either.
TFM_EXTRA_MANIFEST_LIST_FILES and TFM_EXTRA_PARTITION_PATHS can be
configurated in multiple extra sources. It is recommended to use CMake list
APPEND method to avoid unexpected override.
Further Notes#
In the IPC model, Use PSA FF proposed memory accessing mechanism. SPM provides APIs and checking between isolation boundaries, a free accessing of memory can cause program panic.
In the IPC model, the memory checking inside partition runtime is unnecessary. SPM handles the checking while memory accessing APIs are called.
In the IPC model, the client ID had been included in the message structure and secure partition can get it when calling psa_get() function. The secure partition does not need to call
tfm_core_get_caller_client_id()to get the caller client ID anymore.In the IPC model, SPM will check the security policy and partition dependence between client and service. So the service does not need to validate the secure caller anymore.
Reference#
Copyright (c) 2019-2022, Arm Limited. All rights reserved. Copyright (c) 2022 Cypress Semiconductor Corporation (an Infineon company) or an affiliate of Cypress Semiconductor Corporation. All rights reserved.