MCUXpresso SDK Documentation

Non-secure Client Extension Integration Guide#

This document introduces TF-M Non-secure Client Extension (NSCE) and how to integrate it with Non-secure Processing Environment (NSPE) RTOS.

What is NSCE for#

Besides the secure services provided via PSA APIs, there are two interactions between TF-M and NSPE RTOS.

  • Non-secure context management in TF-M

    When a NS task calls a secure service, a context is maintained in TF-M. If TF-M supports multiple secure service calls, the context needs to be loaded and saved with the corresponding NS task when the RTOS kernel (the kernel) does scheduling.

  • Non-secure client ID (NSID) management

    As per PSA Firmware Framework specification, NSID is required for a secure service call from the NSPE. The NSID can be managed by either SPM (the same NSID must be used for all connections) or the NSPE RTOS. For the latter case, the NSPE RTOS must provide the NSID for each connection.

NSCE is implemented to support the interactions above.

  • Provide the interface to NSPE RTOS for managing the context in TF-M.

  • Provide a mechanism to NSPE RTOS for providing the NSID for each connection.

NSCE component diagram#

../../../../../_images/nsce-integ.svg

Non-secure Client Extension Component Diagram#

This diagram shows the components of NSCE.

  • NSCE interface: The NSCE API interface to NSPE RTOS.

  • NS Client Context Manager: It is the internal component of SPM that is used to manage the NS client context. It is not accessible to NSPE.

Group-based context management#

NSCE introduces a group-based context management for NS clients. The purpose is to support diverse use scenarios in the IoT world.

For rich-resource devices, TF-M could assign separate contexts for each connection. For resource-constrained devices, TF-M may support very limited context slots. Multiple NS connections could share the same context provided they have mutual exclusion access to the secure services.

To support this flexibility, a group ID (gid) and a thread ID (tid) are specified for the connection of the NS client. NSCE allocates only one context for a given group. Threads in the same group share the context.

The gid and tid are specified by NSPE RTOS via NSCE interface.

NSCE interface#

NSCE defines a set of APIs as the interface for NSPE RTOS to manage the context in TF-M. NSID is provided as an input parameter of tfm_nsce_load_ctx().

NSCE APIs are typically called by the kernel and must be called from the non-secure handler mode.

uint32_t tfm_nsce_init(uint32_t ctx_requested)

This function should be called before any other NSCE APIs below to do non-secure context initialization in NSCE for the calling NS entity. ctx_requested is the number of the contexts requested by the NS entity. The number of assigned context will be returned. It may be equal to or smaller than the requested context number based on the current available resource in TF-M. If ctx_requested is 0, then the maximum available context number will be assigned and returned. If the initialization is failed, 0 should be returned.

Note

As TF-M only supports one context for now, so the return value is always 1 if no error. Currently, it is safe to skip calling tfm_nsce_init(). But, for future compatibility, it is recommended to do so.

uint32_t tfm_nsce_acquire_ctx(uint8_t group_id, uint8_t thread_id)

This function allocates a context for the NS client connection. The gid and tid are the input paramemters. A token will be returned to the NSPE if TF-M has an available context slot. Otherwise, TFM_NS_CLIENT_INVALID_TOKEN is returned. It is the responsibility of NSPE RTOS to assign gid and tid for each NS client.

uint32_t tfm_nsce_release_ctx(uint32_t token)

This function tries to release the context which was retrieved by tfm_nsce_acquire_ctx(). As the context may be shared with other threads within the same group, the context is only freed and back to the available context pool after all threads in the same group release the context.

uint32_t tfm_nsce_load_ctx(uint32_t token, int32_t nsid)

This function should be called when NSPE RTOS schedules in a NS client. token is returned by tfm_nsce_acquire_ctx(). nsid is the non-secure client ID used for the following PSA service calls.

The assignment of NSID is managed by the NSPE RTOS. It is not required to use the same NSID for a NS client when calling this function each time. This allows the NS client changing its NSID in the lifecycle. For example, the provisioning task may need to switch NSID to provision the keys for different NS clients created afterwards.

uint32_t tfm_nsce_save_ctx(uint32_t token)

This function should be called when NSPE RTOS schedules out a NS client. The input parameter token is returned by tfm_nsce_acquire_ctx(). After the context is saved, no secure service call can be made from NSPE until a context is loaded via tfm_nsce_load_ctx().

NSCE integration guide#

Enable NSCE in TF-M#

To enable NSCE in TF-M, set the build flag TFM_NS_MANAGE_NSID to ON (default OFF).

Support NSCE in an RTOS#

For supporting NSCE in an RTOS, the integrator needs to do the following major work:

  • Integrate the NSCE API calls into the NS task lifecycle. For example, creating/scheduling/destroying a NS task.

  • Manage the assignment for gid, tid and NSID.

The typical steps are listed below:

  • Before programming, the integrator should plan the group assignment for the NS tasks that need to call secure services. If the number of tasks is less than or equal to TF-M non-secure context slots, then different gid can be assigned to each task for taking dedicated context in TF-M. Otherwise, the integrator need to think about grouping the tasks to share the context.

  • In the kernel initialization stage, it calls tfm_nsce_init() with requested context number to initialize the non-secure context in TF-M. The actual allocated context number will be returned. 0 means initialization failed. The kernel could use different group assignment sets according to the context number allocated to it. TF-M only supports one context for now.

  • The kernel calls tfm_nsce_acquire_ctx() when creating a new task. This should be done before the new task calls any secure service. A valid token returned should be saved as part of the task context in NSPE RTOS.

  • When the kernel schedules in a task with a valid token associated, tfm_nsce_load_ctx() should be called before resuming the execution of that task. The NSID is specified by the kernel through the nsid parameter. The mapping between NSID and task is managed by the kernel. tfm_nsce_load_ctx() can be called multiple times without calling tfm_nsce_save_ctx() for switching the NSID for the same task (same tid and gid).

  • tfm_nsce_save_ctx() should be called if the current task has a valid token before being switched to another task. Calling tfm_nsce_load_ctx() for another task before saving the current context may result in NS context lost in TF-M for the running task.

  • When the task is terminated, destroyed or crashed, the kernel should call tfm_nsce_release_ctx to make sure the associated resource is back to the pool in TF-M.

Integration example#

../../../../../_images/nsce-rtos-example.svg

RTOS/NSCE integration example#

This is the software module diagram of a typical RTOS/NSCE integration example.

  • Built-in Secure Context Manager: An RTOS may have an existing built-in secure context manager with a group of secure context management APIs defined. Let’s take RTX which uses Armv8-M TrustZone APIs as the example.

Note

RTOS may define the NS task context in the secure side as “secure context”. It is the same thing as the “non-secure context” (context for a secure service call from NS client) from TF-M’s point of view.

  • Shim Layer/Secure Context Manager: If the RTOS has a “Built-in Secure Context Manager”, then a shim layer should be provided to translate the built-in API calls into the NSCE API calls. A reference shim layer for RTX TrustZone APIs is here.

    If the RTOS has no existing one, then a “Secure Context Manager” should be implemented based on the NSCE APIs. You can refer to the shim layer example above for the implementation. The timing of calling NSCE APIs in the kernel is introduced in the Support NSCE in an RTOS section above.

  • NSID Manager: If NSPE RTOS manages the NSID, then this module is used by the secure context manager or shim layer to manage the NSID assignment for the NS tasks. The assignment is implementation defined. A task name based NSID manager is provided as a reference.

Integration notes#

  • gid: It is a uint8_t value (valid range is 0 - 255). So, maximum 256 groups (NSCE context slots) are supported by the NSCE interface. TF-M only supports single context for now. So, it is recommended to use single group ID at this stage.

  • tid: It is a uint8_t value (valid range is 0 - 255). Thread ID is used to identify a NS client within a given group. tid has no special meaning for TF-M. So, usually the kernel only needs to ensure a NS task has a unique tid within a group.

  • gid and tid management: It is the responsibility of NSPE RTOS to manage the assignment of gid and tid. Based on the explaination above, the gid could be assigned as a constant value. And, the tid can be increased globally when calling tfm_nsce_acquire_ctx() for a new task. Just notice tid may overflow.

  • NSID management: It is the responsibility of NSPE RTOS to manage the assignment of the NSID for each task. It is highly recommended that a NS client uses the same NSID following a reboot or update. The binding of a NS client to a specific NSID will ensure the correct access to the assets. For example, the data saved in the protected storage.

  • Integrate with the existing secure context management APIs of NSPE RTOS: The NSCE APIs are designed to be compatible with most known existing secure context management APIs. A shim layer is needed to translate the API calls. See the integration example above.

  • tfm_nsce_acquire_ctx() must be called before calling tfm_nsce_load_ctx(), tfm_nsce_save_ctx() or tfm_nsce_release_ctx().

  • tfm_nsce_release_ctx() can be called without calling tfm_nsce_save_ctx() ahead.


Copyright (c) 2021, Arm Limited. All rights reserved.