Code Review Guideline#
The purpose of this document is to clarify design items to be reviewed during the code review process.
Please contact maintainers or write an e-mail thread on the TF-M mailing list for any questions.
List of the guidelines#
The prerequisites before going to the review stage:
Read the Contributing Process to know basic concepts.
Read the Source Structure for structure related reference.
The review guidelines consist of these items:
Note
Each guideline item is assigned with a unique symbol in the format Rx.y,
while x and y are numeric symbols. These symbols are created for easy
referencing during the code review process.
Exceptions#
Files under listed folders are fully or partially imported from 3rd party projects, these files follow the original project defined guidelines and styles:
Important
R1.1
extand its subfolders.
Non-source items#
For all non-source files such as build system files or configuration files:
Important
R2.1 Follow the existing style while making changes.
Namespace#
TF-M assign the namespace to files and symbols for an easier code reading. The symbol here includes functions, variables, types and MACROs. The prerequisites:
Important
R3.1 Follow the documents or specifications if they propose namespaces (‘psa_’ for PSA defined items E.g.,). Ask the contributor to tell the documents or specifications if the reviewer is not sure about a namespace.
R3.2 Assign TF-M specific namespace ‘tfm_’ or ‘TFM_’ for symbols implementing TF-M specific features. Ask the contributor to clarify the purpose of the patch if the reviewer is not sure about the namespace.
For the sources out of the above prerequisites (R3.1 and R3.2):
Important
R3.3 Do not assign a namespace for source files.
R3.4 Assigning a namespace for interface symbols is recommended. The namespace needs to be expressed in one word to be followed by other words into a phrase can represent the functionalities implemented. One word naming is allowed if the namespace can represent the functionality perfectly.
R3.5 Assign a namespace for private symbols is NOT recommended.
R3.6 Do not assign characters out of alphabets as the leading character.
Examples:
/* R3.1 FILE: s/spm/core/psa_client.c */
/* R3.2 FILE: s/spm/core/tfm_secure_context.c */
/* R3.4 FILE: s/spm/core/spm.c, 'spm\_' as the namespace */
void spm_init(void);
/* R3.5 FILE: s/spm/core/main.c */
static void init_functions(void);
/* R3.6 Not permitted: */
/* static uint32_t __count; */
Assembler code#
Important
R4.1 Pure assembler sources or inline assembler code are required to be put under the platform-independent or architecture-independent folders. The logic folders should not contain any assembler code, referring to external MACRO wrapped assembler code is allowed. Here is one example of the logic folder:
‘secure_fw/spm’.
Examples:
/*
* R4.1 The following MACRO is allowed to be referenced under
* 'secure_fw/spm'
*/
#define SVC(code) __asm volatile("svc %0", ::"I"(code))
Include#
This chapter describes the placement of the headers and including. There are
two types of headers: The interface headers contain symbols to be shared
between modules and the private headers contain symbols only for internal
usage.
Important
R5.1 Put the
interface headerof one module in theincludefolder under the root of this module. Deeper sub-folders can not haveincludefolders, which means only oneincludeis allowed for one module.R5.2 Creating sub-folders under
includeto represent the more granular scope of the interfaces is allowed.R5.3
private headercan be put at the same place with the implementation sources for the private symbols contained in the header. It also can be put at the place where the sources need it. The latter is useful when some “private header” contains abstracted interfaces, but these interfaces are not public interfaces so it won’t be put under “include” folder.R5.4 Use <> when including public headers.
R5.5 Use “” when including private headers.
R5.6 The module’s
includefolder needs to be added into referencing module’s header searching path.R5.7 The module’s
includefolder and the root folder needs to be added into its own header searching path and apply a hierarchy including with folder name.R5.8 Path hierarchy including is allowed since there are sub-folders under
includefolder and the module folder.R5.9 The including statement group order: the beginning group contains toolchain headers, then follows the public headers group and finally the private headers group.
R5.10 The including statement order inside a group: Compare the include statement as strings and sort by the string comparison result.
R5.11 The header for the referenced symbol or definition must be included even this header is included inside one of the existing included headers. This improves portability in case the existing header implementation changed.
Examples:
/*
* The structure:
* module_a/include/func1.h
* module_a/include/func2/fmain.h
* module_a/func1.c
* module_a/func2/fmain.c
* module_b/include/funcx.h
* module_b/include/funcy/fmain.h
* module_b/funcx.c
* module_b/funcxi.h
* module_b/funcy/fmain.c
* module_b/funcy/fsub.c
* module_b/funcy/fsub.h
* Here takes module_b/funcx.c as example:
*/
#include <func1.h>
#include <func2/fmain.h>
#include <funcx.h>
#include "funcxi.h"
#include "funcy/fsub.h"
Auto-doc#
Auto document system such as doxygen is useful for describing interfaces. While it would be a development burden since the details are described in the design documents already. The guidelines for auto-doc:
Important
R6.1 Headers and sources under these folders need to apply auto-doc style comments:
*include.R6.2 Developers decide the comment style for sources out of listed folders.
Commit Message#
TF-M has the requirements on commit message:
Important
R7.1 Assign correct topic for a patch. Check the following table.
Topic |
Justification |
|---|---|
Boot |
bl2/* or bl1/* |
Build |
For build system related purpose. |
Docs |
All *.rst changes. |
Dualcpu |
Dual-cpu related changes. |
HAL |
Generic HAL interface/implementation changes. |
Interface |
Interface changes, either Non-source and secure. |
Pack |
For packing purpose. |
Platform |
Generic platform related changes under platform/*. |
Platform Name |
Specific platform changes. |
Partition |
Multiple partition related changes. |
Partition Name |
Specific partition related changes. |
Service |
Multiple service related changes. |
Service Name |
Specific service related changes. |
SPM |
secure_fw/spm/* |
SPRTL |
secure-fw/partitions/lib/runtime/* |
Tool |
tools folder or tf-m-tools repo |
Note
Ideally, one topic should cover one specific type of changes. For crossing topic changes, check the main part of the change and use the main part related topic as patch topic. If there is no suitable topics to cover the change, contact the community for an update.
Copyright (c) 2020-2022, Arm Limited. All rights reserved.