Trusted Firmware-M Profile Medium-ARoT-less#
Introduction#
TF-M Profile Medium-ARoT-less is a reference implementation to align with security requirements defined in PSA Certified ARoT-less Level 2 protection profile (PSA Certified ARoT-less) 1SESIP Profile for PSA Certified ARoT-less Level 2.
TF-M Profile Medium-ARoT-less is defined based on TF-M Profile Medium 2Trusted Firmware-M Profile Medium Design, which aligns with PSA Certified Level 2 Protection Profile 3SESIP Profile for PSA Certified Level 2.
Overall design#
TF-M Profile Medium-ARoT-less defines the following feature set:
Firmware Framework
4Arm Firmware Framework for M 1.1 Extensions
- 5Arm Platform Security Architecture Firmware Framework 1.0
Secure Function (SFN) model 4Arm Firmware Framework for M 1.1 Extensions
Isolation level 1 5Arm Platform Security Architecture Firmware Framework 1.0
Internal Trusted Storage (ITS)
Crypto
- 6Transport Layer Security (TLS) / Datagram Transport Layer Security (DTLS) Profiles for the Internet of Things7The Constrained Application Protocol (CoAP)
Support both symmetric cryptography and asymmetric cryptography
Asymmetric key based cipher suite suggested in TLS/DTLS profiles for IoT 6Transport Layer Security (TLS) / Datagram Transport Layer Security (DTLS) Profiles for the Internet of Things and CoAP 7The Constrained Application Protocol (CoAP), including
Authenticated Encryption with Associated Data (AEAD) algorithm
Asymmetric key algorithm based signature and verification
Public-key cryptography based key exchange
Hash function
HMAC for default Pseudorandom Function (PRF)
Asymmetric digital signature and verification for Initial Attestation Token (IAT)
Initial Attestation
Asymmetric key algorithm based Initial Attestation
Lightweight boot
Anti-rollback protection
Multiple image boot
Firmware Update (FWU) RoT Service
Design details#
Most of design in Profile Medium-ARoT-less is identical to that in Profile Medium. Refer to Profile Medium document [2] for details. Only the differences between Profile Medium-ARoT-less and Profile Medium are specified below.
Firmware framework#
PSA Certified ARoT-less [1] is only applicable to devices that don’t support Application RoT (ARoT) services. The platform only consists of PSA RoT domain(s) in SPE making it unnecessary to implement the isolation between ARoT and PSA RoT. Therefore, this profile selects isolation level 1 to simplify implementation and optimize memory footprint and performance.
Since only isolation level 1 is required, this profile enables SFN model rather than IPC mode for further simplification.
Protected Storage#
Protected Storage (PS) is implemented as an Application RoT service in TF-M by default. Therefore, PS is disabled by default in this profile.
FWU RoT Service#
As PSA Certified ARoT-less requests, FWU RoT Service is enabled by default to support secure update of platform if the platform supports FWU.
8Secure OTA Updates for Cortex-M Devices with FreeRTOSNote
Implementation note
The entire secure update sequence involves multiple agents and components, including bootloader, TF-M FWU RoT Service, image update application(s), remote server(s), etc.
The secure update sequence is implementation-defined. Here is a reference of TF-M integration with FreeRTOS OTA 8Secure OTA Updates for Cortex-M Devices with FreeRTOS.
Implementation#
The basic idea is to add dedicated profile CMake configuration files
config/profile/profile_medium_arotless for this profile default configuration.
This top-level config file collects all the fundamental configuration flags and set them to default values, to explicitly configured the features required in this profile, during TF-M build.
A platform/use case overwrite the default settings to configure this profile.
The behavior of the build flow (particularly the order of configuration loading and overriding) can be found at Build configuration.
The default configurations in config/profile/profile_medium_arotless are shown below.
Configs |
Default value |
Descriptions |
|---|---|---|
|
|
Select level 1 isolation |
|
|
Select SFN model |
|
|
Enable ITS SP |
|
|
ITS internal transient buffer size |
|
|
Enable Crypto service |
|
|
Enable Crypto asymmetric encryption operations |
|
|
Re-use Profile Medium configuration |
|
|
Re-use Profile Medium configuration |
|
|
Enable Initial Attestation service |
|
|
Enable Firmware Update service |
|
|
Disable PS service |
|
|
Enable TF-M Platform SP |
Note
Where a configuration is the same as the default in
config/config_default.cmake, it might be omitted from the profile configuration
file.
Note
Implementation note
If the platform doesn’t support secure update functionalities, FWU service will be disabled automatically. A warning will be thrown out during build.
Regression test configuration#
FWU regression tests and SFN regression tests are selected by default when regression tests are enabled. Other implementations are the same as those in Profile Medium.
Platform support#
To enable Profile Medium-ARoT-less on a platform, the platform specific CMake file should be added into the platform support list in top-level Profile Medium-ARoT-less CMake config file.
Building Profile Medium-ARoT-less#
To build Profile Medium-ARoT-less, argument TFM_PROFILE in build command line should be
set to profile_medium_arotless.
Take Musca-B1 as an example. The following commands build Profile Medium-ARoT-less without test cases on Musca-B1 with build type MinSizeRel, built by Armclang.
cd <TFM root dir>
mkdir build && cd build
cmake -DTFM_PLATFORM=musca-b1 \
-DTFM_TOOLCHAIN_FILE=../toolchain_ARMCLANG.cmake \
-DTFM_PROFILE=profile_medium_arotless \
-DCMAKE_BUILD_TYPE=MinSizeRel \
../
cmake --build ./ -- install
The following commands build Profile Medium-ARoT-less with regression test cases on Musca-B1 with build type MinSizeRel, built by Armclang.
cd <TFM root dir>
mkdir build && cd build
cmake -DTFM_PLATFORM=musca-b1 \
-DTFM_TOOLCHAIN_FILE=../toolchain_ARMCLANG.cmake \
-DTFM_PROFILE=profile_medium_arotless \
-DCMAKE_BUILD_TYPE=MinSizeRel \
-DTEST_S=ON -DTEST_NS=ON \
../
cmake --build ./ -- install
Note
For devices with more constrained memory and flash requirements, it is possible to build with either only TEST_S enabled or only TEST_NS enabled. This will decrease the size of the test images. Note that both test suites must still be run to ensure correct operation.
More details of building instructions and parameters can be found TF-M build instruction guide 9TF-M build instruction.
Reference#
Copyright (c) 2020-2023, Arm Limited. All rights reserved.