Trusted Firmware-M Profile Large Design#
Introduction#
As one of TF-M Profiles, Profile Large protects less resource-constrained Arm Cortex-M devices.
Compared to Profile Small 1Trusted Firmware-M Profile Small Design and Profile Medium 2Trusted Firmware-M Profile Medium Design, Profile Large aims to enable more secure features to support higher level of security required in more complex usage scenarios.
Isolation level 3 enables additional isolation between Application RoT (App RoT) services.
More crypto algorithms and cipher suites are selected to securely connect devices to remote services offered by various major Cloud Service Providers (CSP)
Basic software countermeasures against physical attacks can be enabled.
Profile Large can be aligned as a reference implementation with the requirements defined in PSA Certified Level 3 Lightweight Protection Profile 3PSA Certified Level 3 Lightweight Protection Profile.
Overall design#
TF-M Profile Large defines the following feature set:
Firmware Framework
4Arm Platform Security Architecture Firmware Framework 1.0
Inter-Process Communication (IPC) model 4Arm Platform Security Architecture Firmware Framework 1.0
Isolation level 3 [4]
Internal Trusted Storage (ITS)
Crypto
- 5The Transport Layer Security (TLS) Protocol Version 1.2
Support both symmetric ciphers and asymmetric ciphers
Asymmetric key based cipher suites defined in TLS 1.2 5The Transport Layer Security (TLS) Protocol Version 1.2 to support direct secure connection to major CSPs, including
Authenticated Encryption with Associated Data (AEAD) algorithm
Asymmetric key algorithm based signature and verification
Public-key cryptography based key exchange
Hash function
HMAC for default Pseudorandom Function (PRF)
Asymmetric digital signature and verification for Initial Attestation Token (IAT)
Asymmetric algorithms for firmware image signature verification
Key derivation
Initial Attestation
Asymmetric key algorithm based Initial Attestation
- Secure boot
Anti-rollback protection
Multiple image boot
Protected Storage (PS) if off-chip storage device is integrated
Data confidentiality
Data integrity
Rollback protection
Software countermeasures against physical attacks
Design details#
More details of TF-M Profile Large design are described in following sections.
Firmware framework#
Profile Large selects IPC model and isolation level 3 by default.
Isolation level 3 supports additional isolation between App RoT services, compared to isolation level 2. It can protect RoT services from each other when their vendors don’t trust each other.
Crypto service#
Profile Large supports direct connection to Cloud services via common protocols, such as TLS 1.2.
In some usage scenarios, PSA RoT can be managed by device manufacturer or other vendors and is out of control of application developers. Profile Large selects alternative crypto algorithms for each crypto function to support multiple common cipher suites required by various major CSPs. Therefore, application developers can support services for diverse CSPs on same devices with Profile Large, without relying on PSA RoT upgrades of crypto.
Devices meeting Profile Large should be in a position to offer at least two alternatives to every cryptographic primitive for symmetric, asymmetric and hash, and be able to use them for encryption, AEAD, signature and verification.
It will cost more resource in Profile Large to support more crypto algorithms and cipher suites, compared to Profile Medium [2].
Boot loader#
BL2 implementation can be device specific. Devices may implement diverse boot processes with different features and configurations. However, the boot loader must support anti-rollback protection. Boot loader must be able to prevent unauthorized rollback, to protect devices from being downgraded to earlier versions with known vulnerabilities.
MCUBoot in TF-M is configured as multiple image boot by default in Profile Large. In multiple image boot, secure and non-secure images can be signed independently with different keys and they can be updated separately. It can support multiple vendors scenarios, in which non-secure and secure images are generated and updated by different vendors. Multiple image boot may cost larger memory footprint compared with single image boot.
Boot loader can implement software countermeasures to mitigate physical attacks.
Protected Storage#
PS service is required if an off-chip storage device is integrated and used on the platform.
Anti-rollback protection in PS relies on non-volatile counter(s) provided by TF-M Platform Secure Partition (SP).
Software countermeasures against physical attacks#
TF-M Profile Large enables TF-M Fault Injection Hardening (FIH) library Profile Medium by default. It enables the following countermeasure techniques:
Control flow monitor
Failure loop hardening
Complex constants
Redundant variables and condition checks
Refer to TF-M physical attack mitigation design document 6Physical attack mitigation in Trusted Firmware-M for FIH library details.
Note
TF-M FIH library is still under development.
TF-M FIH library hardens TF-M critical execution steps to make physical attacks more difficult, together with device hardware countermeasures. It is not guaranteed that TF-M FIH library is able to mitigate all kinds of physical attacks.
Note
Implementation note
TF-M FIH library doesn’t cover platform specific critical configurations. Platforms shall implement software countermeasures against physical attacks to protect platform specific implementation.
Implementation#
Overview#
The basic idea is to add dedicated profile CMake configuration files under
folder config/profile for TF-M Profile Large default configuration, the
same as other TF-M Profiles do.
The top-level Profile Large config file collects all the necessary configuration flags and set them to default values, to explicitly enable the features required in Profile Large and disable the unnecessary ones, during TF-M build.
A platform/use case can provide a configuration extension file to overwrite
Profile Large default setting and append other configurations.
This configuration extension file can be added via parameter
TFM_EXTRA_CONFIG_PATH in build command line.
The behaviour of the Profile Large build flow (particularly the order of configuration loading and overriding) can be found at Build configuration
The details of configurations will be covered in each module in Implementation details.
Implementation details#
This section discusses the details of Profile Large implementation.
Top-level configuration files#
The firmware framework configurations in config/profile/profile_large are
shown below.
Configs |
Descriptions |
Default value |
|---|---|---|
|
Select level 3 isolation |
|
|
Enable ITS SP |
|
|
Enable Crypto service |
|
|
MbedTLS config file path |
|
|
MbedTLS PSA config file path |
|
|
Enable Initial Attestation service |
|
|
Enable PS service |
|
|
Enable TF-M Platform SP |
|
PS service is enabled by default. Platforms without off-chip storage
devices can turn off TFM_PARTITION_PROTECTED_STORAGE to disable PS
service. See Protected Storage Secure Partition for details.
Crypto service configurations#
Crypto Secure Partition#
TF-M Profile Large enables Crypto SP in top-level CMake config file and selects all the Crypto modules.
MbedTLS configurations#
TF-M Profile Large adds a dedicated MbedTLS config file
tfm_mbedcrypto_config_profile_large.h and MbedTLS PSA config file
crypto_config_profile_large.h under
/lib/ext/mbedcrypto/mbedcrypto_config folder, instead of the common one
tfm_mbedcrypto_config_default.h and crypto_config_default.h 7Crypto design.
Major MbedTLS configurations are set as listed below:
Enable SHA256, SHA384 and SHA512
Enable generic message digest wrappers
Enable AES
Enable CCM mode, GCM mode, CTR mode, CFB mode and CBC mode for symmetric ciphers
Disable other modes for symmetric ciphers
Enable ECDH
Enable ECDSA
Enable RSA
Select ECC curve
secp256r1andsecp384r1Enable HMAC-based key derivation function
Other configurations required by selected option above
A device/use case can append an extra config header to the Profile Large default
MbedTLS config file to override the default settings. This can be done by
setting the TFM_MBEDCRYPTO_PLATFORM_EXTRA_CONFIG_PATH cmake variable in the
platform config file platform/ext<TFM_PLATFORM>/config.cmake.
This cmake variable is a wrapper around the MBEDTLS_USER_CONFIG_FILE
options, but is preferred as it keeps all configuration in cmake.
Internal Trusted Storage configurations#
ITS service is enabled in top-level Profile Large CMake config file by default.
The internal transient buffer size ITS_BUF_SIZE 8ITS integration guide is set to 64 bytes by
default. A platform/use case can overwrite the buffer size in its specific
configuration extension according to its actual requirement of assets and Flash
attributes.
Profile Large CMake config file won’t touch the configurations of device specific Flash hardware attributes.
Protected Storage Secure Partition#
Data confidentiality, integrity and anti-rollback protection are enabled by default in PS.
If PS is selected, AES-CCM is used as AEAD algorithm by default. If platform hardware crypto accelerator supports the AEAD algorithm, the AEAD operations can be executed in hardware crypto accelerator.
If platforms don’t integrate any off-chip storage device, platforms can disable
PS in platform specific configuration extension file via
platform/ext<TFM_PLATFORM>/config.cmake.
BL2 setting#
Profile Large enables MCUBoot provided by TF-M by default. A platform can
overwrite this configuration by disabling MCUBoot in its configuration extension
file platform/ext<TFM_PLATFORM>/config.cmake.
If MCUBoot provided by TF-M is enabled, multiple image boot is selected by default.
If a device implements its own boot loader, the configurations are implementation defined.
Software countermeasure against physical attacks#
Profile Large selects TF-M FIH library Profile Medium by specifying
-DTFM_FIH_PROFILE=MEDIUM in top-level CMake config file.
System integrators shall implement software countermeasures in platform specific implementations.
Device configuration extension#
To change default configurations and add platform specific configurations,
a platform can add a platform configuration file at
platform/ext<TFM_PLATFORM>/config.cmake
Test configuration#
Some cryptography tests are disabled due to the reduced MbedTLS config.
Profile Large specific test configurations are also specified in Profile Large
top-level CMake config file config/profile/profile_large_test.cmake.
Configs |
Default value |
Descriptions |
|---|---|---|
|
|
Test CBC cryptography mode |
|
|
Test CCM cryptography mode |
|
|
Test CFB cryptography mode |
|
|
Test ECB cryptography mode |
|
|
Test CTR cryptography mode |
|
|
Test OFB cryptography mode |
|
|
Test GCM cryptography mode |
|
|
Test SHA-384 cryptography algorithm |
|
|
Test SHA-512 cryptography algorithm |
|
|
Test HMAC-based key derivation function |
|
|
Test ECDH key agreement algorithm |
|
|
Test ChaCha20 stream cipher |
|
|
Test ChaCha20-Poly1305 AEAD algorithm |
|
|
Test single-part operations in hash, MAC, AEAD and symmetric ciphers |
Platform support#
To enable Profile Large on a platform, the platform specific CMake file should be added into the platform support list in top-level Profile Large CMake config file.
Building Profile Large#
To build Profile Large, argument TFM_PROFILE in build command line should be
set to profile_large.
Take AN521 as an example:
The following commands build Profile Large without test cases on AN521 with build type MinSizeRel, built by Armclang.
cd <TFM root dir>
mkdir build && cd build
cmake -DTFM_PLATFORM=arm/mps2/an521 \
-DTFM_TOOLCHAIN_FILE=../toolchain_ARMCLANG.cmake \
-DTFM_PROFILE=profile_large \
-DCMAKE_BUILD_TYPE=MinSizeRel \
../
cmake --build ./ -- install
The following commands build Profile Large with regression test cases on AN521 with build type MinSizeRel, built by Armclang.
cd <TFM root dir>
mkdir build && cd build
cmake -DTFM_PLATFORM=arm/mps2/an521 \
-DTFM_TOOLCHAIN_FILE=../toolchain_ARMCLANG.cmake \
-DTFM_PROFILE=profile_large \
-DCMAKE_BUILD_TYPE=MinSizeRel \
-DTEST_S=ON -DTEST_NS=ON \
../
cmake --build ./ -- install
More details of building instructions and parameters can be found TF-M build instruction guide 9TF-M build instruction.
Reference#
Copyright (c) 2021-2022, Arm Limited. All rights reserved.