MCUXpresso SDK Documentation

Target requirements

Target requirements#

This release of the Flashloader supports the following platforms:

  • MIMXRT1010-EVKMIMXRT1020-EVKMIMXRT1015-EVKMIMXRT1064-EVKIMXRT1050-EVKBMIMXRT1060-EVKMIMXRT1024-EVK LPCXpresso54018 MIMXRT1170 EVKMIMXRT1160 EVK

  • LPCXpresso54S018

  • LPCXpresso54S018M

There are no specific requirements for the hardware other than what the board requires to operate.