TLS 1.3 support#
Overview#
Mbed TLS provides an implementation of the TLS 1.3 protocol. The TLS 1.3 support may be enabled using the MBEDTLS_SSL_PROTO_TLS1_3 configuration option.
Support description#
Overview
Mbed TLS implements both the client and the server side of the TLS 1.3 protocol.
Mbed TLS supports ECDHE key establishment.
Mbed TLS supports DHE key establishment.
Mbed TLS supports pre-shared keys for key establishment, pre-shared keys provisioned externally as well as provisioned via the ticket mechanism.
Mbed TLS supports session resumption via the ticket mechanism.
Mbed TLS supports sending and receiving early data (0-RTT data).
Supported cipher suites: depends on the library configuration. Potentially all of them: TLS_AES_128_GCM_SHA256, TLS_AES_256_GCM_SHA384, TLS_CHACHA20_POLY1305_SHA256, TLS_AES_128_CCM_SHA256 and TLS_AES_128_CCM_8_SHA256.
Supported ClientHello extensions:
Extension
Support
server_name
YES
max_fragment_length
no
status_request
no
supported_groups
YES
signature_algorithms
YES
use_srtp
no
heartbeat
no
alpn
YES
signed_certificate_timestamp
no
client_certificate_type
no
server_certificate_type
no
padding
no
key_share
YES
pre_shared_key
YES
psk_key_exchange_modes
YES
early_data
YES
cookie
no
supported_versions
YES
certificate_authorities
no
post_handshake_auth
no
signature_algorithms_cert
no
Supported groups: depends on the library configuration. Potentially all ECDHE groups: secp256r1, x25519, secp384r1, x448 and secp521r1.
Potentially all DHE groups: ffdhe2048, ffdhe3072, ffdhe4096, ffdhe6144 and ffdhe8192.
Supported signature algorithms (both for certificates and CertificateVerify): depends on the library configuration. Potentially: ecdsa_secp256r1_sha256, ecdsa_secp384r1_sha384, ecdsa_secp521r1_sha512, rsa_pkcs1_sha256, rsa_pkcs1_sha384, rsa_pkcs1_sha512, rsa_pss_rsae_sha256, rsa_pss_rsae_sha384 and rsa_pss_rsae_sha512.
Note that in absence of an application profile standard specifying otherwise rsa_pkcs1_sha256, rsa_pss_rsae_sha256 and ecdsa_secp256r1_sha256 are mandatory (see section 9.1 of the specification).
Supported versions:
TLS 1.2 and TLS 1.3 with version negotiation on client and server side.
TLS 1.2 and TLS 1.3 can be enabled in the build independently of each other.
Compatibility with existing SSL/TLS build options:
The TLS 1.3 implementation is compatible with nearly all TLS 1.2 configuration options in the sense that when enabling TLS 1.3 in the library there is rarely any need to modify the configuration from that used for TLS 1.2. There are two exceptions though: the TLS 1.3 implementation requires MBEDTLS_PSA_CRYPTO_C and MBEDTLS_SSL_KEEP_PEER_CERTIFICATE, so these options must be enabled.
Most of the Mbed TLS SSL/TLS related options are not supported or not applicable to the TLS 1.3 implementation:
Mbed TLS configuration option
Support
MBEDTLS_SSL_ALL_ALERT_MESSAGES
yes
MBEDTLS_SSL_ASYNC_PRIVATE
no
MBEDTLS_SSL_CONTEXT_SERIALIZATION
no
MBEDTLS_SSL_DEBUG_ALL
no
MBEDTLS_SSL_ENCRYPT_THEN_MAC
n/a
MBEDTLS_SSL_EXTENDED_MASTER_SECRET
n/a
MBEDTLS_SSL_KEEP_PEER_CERTIFICATE
no (1)
MBEDTLS_SSL_RENEGOTIATION
n/a
MBEDTLS_SSL_MAX_FRAGMENT_LENGTH
no
MBEDTLS_SSL_SESSION_TICKETS
yes
MBEDTLS_SSL_SERVER_NAME_INDICATION
yes
MBEDTLS_SSL_VARIABLE_BUFFER_LENGTH
no
MBEDTLS_ECP_RESTARTABLE
no
MBEDTLS_ECDH_VARIANT_EVEREST_ENABLED
no
MBEDTLS_KEY_EXCHANGE_PSK_ENABLED
n/a (2)
MBEDTLS_KEY_EXCHANGE_DHE_PSK_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_ECDHE_PSK_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_RSA_PSK_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_RSA_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_DHE_RSA_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_ECDHE_RSA_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_ECDHE_ECDSA_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_ECDH_ECDSA_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_ECDH_RSA_ENABLED
n/a
MBEDTLS_KEY_EXCHANGE_ECJPAKE_ENABLED
n/a
MBEDTLS_PSA_CRYPTO_C
no (1)
MBEDTLS_USE_PSA_CRYPTO
yes
(1) These options must remain in their default state of enabled. (2) See the TLS 1.3 specific build options section below.
TLS 1.3 specific build options:
MBEDTLS_SSL_TLS1_3_COMPATIBILITY_MODE enables the support for middlebox compatibility mode as defined in section D.4 of RFC 8446.
MBEDTLS_SSL_TLS1_3_KEY_EXCHANGE_MODE_PSK_ENABLED enables the support for the PSK key exchange mode as defined by RFC 8446. If it is the only key exchange mode enabled, the TLS 1.3 implementation does not contain any code related to key exchange protocols, certificates and signatures.
MBEDTLS_SSL_TLS1_3_KEY_EXCHANGE_MODE_EPHEMERAL_ENABLED enables the support for the ephemeral key exchange mode. If it is the only key exchange mode enabled, the TLS 1.3 implementation does not contain any code related to PSK based key exchange. The ephemeral key exchange mode requires at least one of the key exchange protocol allowed by the TLS 1.3 specification, the parsing and validation of x509 certificates and at least one signature algorithm allowed by the TLS 1.3 specification for signature computing and verification.
MBEDTLS_SSL_TLS1_3_KEY_EXCHANGE_MODE_PSK_EPHEMERAL_ENABLED enables the support for the PSK ephemeral key exchange mode. If it is the only key exchange mode enabled, the TLS 1.3 implementation does not contain any code related to certificates and signatures. The PSK ephemeral key exchange mode requires at least one of the key exchange protocol allowed by the TLS 1.3 specification.
Coding rules checklist for TLS 1.3#
The following coding rules are aimed to be a checklist for TLS 1.3 upstreaming work to reduce review rounds and the number of comments in each round. They come along (do NOT replace) the project coding rules (https://mbed-tls.readthedocs.io/en/latest/kb/development/mbedtls-coding-standards). They have been established and discussed following the review of #4882 that was the PR upstreaming the first part of TLS 1.3 ClientHello writing code.
TLS 1.3 specific coding rules:
TLS 1.3 specific C modules, headers, static functions names are prefixed with
ssl_tls13_. The same applies to structures and types that are internal to C modules.TLS 1.3 specific exported functions, structures and types are prefixed with
mbedtls_ssl_tls13_.Use TLS1_3 in TLS 1.3 specific macros.
The names of macros and variables related to a field or structure in the TLS 1.3 specification should contain as far as possible the field name as it is in the specification. If the field name is “too long” and we prefer to introduce some kind of abbreviation of it, use the same abbreviation everywhere in the code.
Example 1: #define CLIENT_HELLO_RANDOM_LEN 32, macro for the length of the
randomfield of the ClientHello message.Example 2 (consistent abbreviation):
mbedtls_ssl_tls13_write_sig_alg_ext()andMBEDTLS_TLS_EXT_SIG_ALG,sig_algstanding forsignature_algorithms.Regarding vectors that are represented by a length followed by their value in the data exchanged between servers and clients:
Use
<vector name>_lenfor the name of a variable used to compute the length in bytes of the vector, whereis the name of the vector as defined in the TLS 1.3 specification. Use
p_<vector_name>_lenfor the name of a variable intended to hold the address of the first byte of the vector length.Use
<vector_name>for the name of a variable intended to hold the address of the first byte of the vector value.Use
<vector_name>_endfor the name of a variable intended to hold the address of the first byte past the vector value.
Those idioms should lower the risk of mis-using one of the address in place of another one which could potentially lead to some nasty issues.
Example:
cipher_suitesvector of ClientHello inssl_tls13_write_client_hello_cipher_suites()size_t cipher_suites_len; unsigned char *p_cipher_suites_len; unsigned char *cipher_suites;
Where applicable, use:
the macros to extract a byte from a multi-byte integer MBEDTLS_BYTE_{0-8}.
the macros to write in memory in big-endian order a multi-byte integer MBEDTLS_PUT_UINT{8|16|32|64}_BE.
the macros to read from memory a multi-byte integer in big-endian order MBEDTLS_GET_UINT{8|16|32|64}_BE.
the macro to check for space when writing into an output buffer
MBEDTLS_SSL_CHK_BUF_PTR.the macro to check for data when reading from an input buffer
MBEDTLS_SSL_CHK_BUF_READ_PTR.
The three first types, MBEDTLS_BYTE_{0-8}, MBEDTLS_PUT_UINT{8|16|32|64}_BE and MBEDTLS_GET_UINT{8|16|32|64}_BE improve the readability of the code and reduce the risk of writing or reading bytes in the wrong order.
The two last types,
MBEDTLS_SSL_CHK_BUF_PTRandMBEDTLS_SSL_CHK_BUF_READ_PTR, improve the readability of the code and reduce the risk of error in the non-completely-trivial arithmetic to check that we do not write or read past the end of a data buffer. The usage of those macros combined with the following rule mitigate the risk to read/write past the end of a data buffer.Examples:
hs_hdr[1] = MBEDTLS_BYTE_2( total_hs_len ); MBEDTLS_PUT_UINT16_BE( MBEDTLS_TLS_EXT_SUPPORTED_VERSIONS, p, 0 ); MBEDTLS_SSL_CHK_BUF_PTR( p, end, 7 );
To mitigate what happened here (https://github.com/Mbed-TLS/mbedtls/pull/4882#discussion_r701704527) from happening again, use always a local variable named
pfor the reading pointer in functions parsing TLS 1.3 data, and for the writing pointer in functions writing data into an output buffer and only that variable. The namephas been chosen as it was already widely used in TLS code.When an TLS 1.3 structure is written or read by a function or as part of a function, provide as documentation the definition of the structure as it is in the TLS 1.3 specification.
General coding rules:
We prefer grouping “related statement lines” by not adding blank lines between them.
Example 1:
ret = ssl_tls13_write_client_hello_cipher_suites( ssl, buf, end, &output_len ); if( ret != 0 ) return( ret ); buf += output_len;
Example 2:
MBEDTLS_SSL_CHK_BUF_PTR( cipher_suites_iter, end, 2 ); MBEDTLS_PUT_UINT16_BE( cipher_suite, cipher_suites_iter, 0 ); cipher_suites_iter += 2;
Use macros for constants that are used in different functions, different places in the code. When a constant is used only locally in a function (like the length in bytes of the vector lengths in functions reading and writing TLS handshake message) there is no need to define a macro for it.
Example:
#define CLIENT_HELLO_RANDOM_LEN 32When declaring a pointer the dereferencing operator should be prepended to the pointer name not appended to the pointer type:
Example:
mbedtls_ssl_context *ssl;Maximum line length is 80 characters.
Exceptions:
string literals can extend beyond 80 characters as we do not want to split them to ease their search in the code base.
A line can be more than 80 characters by a few characters if just looking at the 80 first characters is enough to fully understand the line. For example it is generally fine if some closure characters like “;” or “)” are beyond the 80 characters limit.
If a line becomes too long due to a refactoring (for example renaming a function to a longer name, or indenting a block more), avoid rewrapping lines in the same commit: it makes the review harder. Make one commit with the longer lines and another commit with just the rewrapping.
When in successive lines, functions and macros parameters should be aligned vertically.
Example:
int mbedtls_ssl_start_handshake_msg( mbedtls_ssl_context *ssl, unsigned hs_type, unsigned char **buf, size_t *buf_len );
When a function’s parameters span several lines, group related parameters together if possible.
For example, prefer:
mbedtls_ssl_start_handshake_msg( ssl, hs_type, buf, buf_len );
over
mbedtls_ssl_start_handshake_msg( ssl, hs_type, buf, buf_len );
even if it fits.
Overview of handshake code organization#
The TLS 1.3 handshake protocol is implemented as a state machine. The
functions mbedtls_ssl_tls13_handshake_{client,server}_step are the top level
functions of that implementation. They are implemented as a switch over all the
possible states of the state machine.
Most of the states are either dedicated to the processing or writing of an handshake message.
The implementation does not go systematically through all states as this would result in too many checks of whether something needs to be done or not in a given state to be duplicated across several state handlers. For example, on client side, the states related to certificate parsing and validation are bypassed if the handshake is based on a pre-shared key and thus does not involve certificates.
On the contrary, the implementation goes systematically though some states
even if they could be bypassed if it helps in minimizing when and where inbound
and outbound keys are updated. The MBEDTLS_SSL_CLIENT_CERTIFICATE state on
client side is a example of that.
The names of the handlers processing/writing an handshake message are
prefixed with (mbedtls_)ssl_tls13_{process,write}. To ease the maintenance and
reduce the risk of bugs, the code of the message processing and writing
handlers is split into a sequence of stages.
The sending of data to the peer only occurs in mbedtls_ssl_handshake_step
between the calls to the handlers and as a consequence handlers do not have to
care about the MBEDTLS_ERR_SSL_WANT_WRITE error code. Furthermore, all pending
data are flushed before to call the next handler. That way, handlers do not
have to worry about pending data when changing outbound keys.
Message processing handlers#
For message processing handlers, the stages are:
coordination stage: check if the state should be bypassed. This stage is optional. The check is either purely based on the reading of the value of some fields of the SSL context or based on the reading of the type of the next message. The latter occurs when it is not known what the next handshake message will be, an example of that on client side being if we are going to receive a CertificateRequest message or not. The intent is, apart from the next record reading to not modify the SSL context as this stage may be repeated if the next handshake message has not been received yet.
fetching stage: at this stage we are sure of the type of the handshake message we must receive next and we try to fetch it. If we did not go through a coordination stage involving the next record type reading, the next handshake message may not have been received yet, the handler returns with
MBEDTLS_ERR_SSL_WANT_READwithout changing the current state and it will be called again later.pre-processing stage: prepare the SSL context for the message parsing. This stage is optional. Any processing that must be done before the parsing of the message or that can be done to simplify the parsing code. Some simple and partial parsing of the handshake message may append at that stage like in the ServerHello message pre-processing.
parsing stage: parse the message and restrict as much as possible any update of the SSL context. The idea of the pre-processing/parsing/post-processing organization is to concentrate solely on the parsing in the parsing function to reduce the size of its code and to simplify it.
post-processing stage: following the parsing, further update of the SSL context to prepare for the next incoming and outgoing messages. This stage is optional. For example, secret and key computations occur at this stage, as well as handshake messages checksum update.
state change: the state change is done in the main state handler to ease the navigation of the state machine transitions.
Message writing handlers#
For message writing handlers, the stages are:
coordination stage: check if the state should be bypassed. This stage is optional. The check is based on the value of some fields of the SSL context.
preparation stage: prepare for the message writing. This stage is optional. Any processing that must be done before the writing of the message or that can be done to simplify the writing code.
writing stage: write the message and restrict as much as possible any update of the SSL context. The idea of the preparation/writing/finalization organization is to concentrate solely on the writing in the writing function to reduce the size of its code and simplify it.
finalization stage: following the writing, further update of the SSL context to prepare for the next incoming and outgoing messages. This stage is optional. For example, handshake secret and key computation occur at that stage (ServerHello writing finalization), switching to handshake keys for outbound message on server side as well.
state change: the state change is done in the main state handler to ease the navigation of the state machine transitions.