MCUXpresso SDK Documentation

Mbed TLS invasive testing strategy#

Introduction#

In Mbed TLS, we use black-box testing as much as possible: test the documented behavior of the product, in a realistic environment. However this is not always sufficient.

The goal of this document is to identify areas where black-box testing is insufficient and to propose solutions.

This is a test strategy document, not a test plan. A description of exactly what is tested is out of scope.

This document is structured as follows:

TLS#

This document currently focuses on data structure manipulation and storage, which is what the crypto/keystore and X.509 parts of the library are about. More work is needed to fully take TLS into account.

Rules#

Always follow these rules unless you have a good reason not to. If you deviate, document the rationale somewhere.

See the section “Possible approaches” for a rationale.

Interface design for testing#

Do not add test-specific interfaces if there’s a practical way of doing it another way. All public interfaces should be useful in at least some configurations. Features with a significant impact on the code size or attack surface should have a compile-time guard.

Reliance on internal details#

In unit tests and in test programs, it’s ok to include internal header files from library/. Do not define non-public interfaces in public headers. In contrast, sample programs must not include header files from library/.

Sometimes it makes sense to have unit tests on functions that aren’t part of the public API. Declare such functions in library/*.h and include the corresponding header in the test code. If the function should be static for optimization but can’t be static for testing, declare it as MBEDTLS_STATIC_TESTABLE, and make the tests that use it depend on MBEDTLS_TEST_HOOKS (see “rules for compile-time options”).

If test code or test data depends on internal details of the library and not just on its documented behavior, add a comment in the code that explains the dependency. For example:

/* This test file is specific to the ITS implementation in PSA Crypto
 * on top of stdio. It expects to know what the stdio name of a file is
 * based on its keystore name.
 */
# This test assumes that PSA_MAX_KEY_BITS (currently 65536-8 bits = 8191 bytes
# and not expected to be raised any time soon) is less than the maximum
# output from HKDF-SHA512 (255*64 = 16320 bytes).

Rules for compile-time options#

If the most practical way to test something is to add code to the product that is only useful for testing, do so, but obey the following rules. For more information, see the rationale.

  • Only use test-specific code when necessary. Anything that can be tested through the documented API must be tested through the documented API.

  • Test-specific code must be guarded by #if defined(MBEDTLS_TEST_HOOKS). Do not create fine-grained guards for test-specific code.

  • Do not use MBEDTLS_TEST_HOOKS for security checks or assertions. Security checks belong in the product.

  • Merely defining MBEDTLS_TEST_HOOKS must not change the behavior. It may define extra functions. It may add fields to structures, but if so, make it very clear that these fields have no impact on non-test-specific fields.

  • Where tests must be able to change the behavior, do it by function substitution. See “rules for function substitution” for more details.

Rules for function substitution#

This section explains how to replace a library function mbedtls_foo() by alternative code for test purposes. That is, library code calls mbedtls_foo(), and there is a mechanism to arrange for these calls to invoke different code.

Often mbedtls_foo is a macro which is defined to be a system function (like mbedtls_calloc or mbedtls_fopen), which we replace to mock or wrap the system function. This is useful to simulate I/O failure, for example. Note that if the macro can be replaced at compile time to support alternative platforms, the test code should be compatible with this compile-time configuration so that it works on these alternative platforms as well.

Sometimes the substitutable function is a static inline function that does nothing (not a macro, to avoid accidentally skipping side effects in its parameters), to provide a hook for test code; such functions should have a name that starts with the prefix mbedtls_test_hook_. In such cases, the function should generally not modify its parameters, so any pointer argument should be const. The function should return void.

With MBEDTLS_TEST_HOOKS set, mbedtls_foo is a global variable of function pointer type. This global variable is initialized to the system function, or to a function that does nothing. The global variable is defined in a header in the library directory such as psa_crypto_invasive.h. This is similar to the platform function configuration mechanism with MBEDTLS_PLATFORM_xxx_ALT.

In unit test code that needs to modify the internal behavior:

  • The test function (or the whole test file) must depend on MBEDTLS_TEST_HOOKS.

  • At the beginning of the test function, set the global function pointers to the desired value.

  • In the test function’s cleanup code, restore the global function pointers to their default value.

Requirements#

General goals#

We need to balance the following goals, which are sometimes contradictory.

  • Coverage: we need to test behaviors which are not easy to trigger by using the API or which cannot be triggered deterministically, for example I/O failures.

  • Correctness: we want to test the actual product, not a modified version, since conclusions drawn from a test of a modified product may not apply to the real product.

  • Effacement: the product should not include features that are solely present for test purposes, since these increase the attack surface and the code size.

  • Portability: tests should work on every platform. Skipping tests on certain platforms may hide errors that are only apparent on such platforms.

  • Maintainability: tests should only enforce the documented behavior of the product, to avoid extra work when the product’s internal or implementation-specific behavior changes. We should also not give the impression that whatever the tests check is guaranteed behavior of the product which cannot change in future versions.

Where those goals conflict, we should at least mitigate the goals that cannot be fulfilled, and document the architectural choices and their rationale.

Problem areas#

Allocation#

Resource allocation can fail, but rarely does so in a typical test environment. How does the product cope if some allocations fail?

Resources include:

  • Memory.

  • Files in storage (PSA API only — in the Mbed TLS API, black-box unit tests are sufficient).

  • Key slots (PSA API only).

  • Key slots in a secure element (PSA SE HAL).

  • Communication handles (PSA crypto service only).

Storage#

Storage can fail, either due to hardware errors or to active attacks on trusted storage. How does the code cope if some storage accesses fail?

We also need to test resilience: if the system is reset during an operation, does it restart in a correct state?

Cleanup#

When code should clean up resources, how do we know that they have truly been cleaned up?

  • Zeroization of confidential data after use.

  • Freeing memory.

  • Freeing key slots.

  • Freeing key slots in a secure element.

  • Deleting files in storage (PSA API only).

Internal data#

Sometimes it is useful to peek or poke internal data.

  • Check consistency of internal data (e.g. output of key generation).

  • Check the format of files (which matters so that the product can still read old files after an upgrade).

  • Inject faults and test corruption checks inside the product.

Possible approaches#

Key to requirement tables:

  • ++ requirement is fully met

  • + requirement is mostly met

  • ~ requirement is partially met but there are limitations

  • ! requirement is somewhat problematic

  • !! requirement is very problematic

Fine-grained public interfaces#

We can include all the features we want to test in the public interface. Then the tests can be truly black-box. The limitation of this approach is that this requires adding a lot of interfaces that are not useful in production. These interfaces have costs: they increase the code size, the attack surface, and the testing burden (exponentially, because we need to test all these interfaces in combination).

As a rule, we do not add public interfaces solely for testing purposes. We only add public interfaces if they are also useful in production, at least sometimes. For example, the main purpose of mbedtls_psa_crypto_free is to clean up all resources in tests, but this is also useful in production in some applications that only want to use PSA Crypto during part of their lifetime.

Mbed TLS traditionally has very fine-grained public interfaces, with many platform functions that can be substituted (MBEDTLS_PLATFORM_xxx macros). PSA Crypto has more opacity and less platform substitution macros.

Requirement

Analysis

Coverage

~ Many useful tests are not reasonably achievable

Correctness

++ Ideal

Effacement

!! Requires adding many otherwise-useless interfaces

Portability

++ Ideal; the additional interfaces may be useful for portability beyond testing

Maintainability

!! Combinatorial explosion on the testing burden

! Public interfaces must remain for backward compatibility even if the test architecture changes

Fine-grained undocumented interfaces#

We can include all the features we want to test in undocumented interfaces. Undocumented interfaces are described in public headers for the sake of the C compiler, but are described as “do not use” in comments (or not described at all) and are not included in Doxygen-rendered documentation. This mitigates some of the downsides of fine-grained public interfaces, but not all. In particular, the extra interfaces do increase the code size, the attack surface and the test surface.

Mbed TLS traditionally has a few internal interfaces, mostly intended for cross-module abstraction leakage rather than for testing. For the PSA API, we favor internal interfaces.

Requirement

Analysis

Coverage

~ Many useful tests are not reasonably achievable

Correctness

++ Ideal

Effacement

!! Requires adding many otherwise-useless interfaces

Portability

++ Ideal; the additional interfaces may be useful for portability beyond testing

Maintainability

! Combinatorial explosion on the testing burden

Internal interfaces#

We can write tests that call internal functions that are not exposed in the public interfaces. This is nice when it works, because it lets us test the unchanged product without compromising the design of the public interface.

A limitation is that these interfaces must exist in the first place. If they don’t, this has mostly the same downside as public interfaces: the extra interfaces increase the code size and the attack surface for no direct benefit to the product.

Another limitation is that internal interfaces need to be used correctly. We may accidentally rely on internal details in the tests that are not necessarily always true (for example that are platform-specific). We may accidentally use these internal interfaces in ways that don’t correspond to the actual product.

This approach is mostly portable since it only relies on C interfaces. A limitation is that the test-only interfaces must not be hidden at link time (but link-time hiding is not something we currently do). Another limitation is that this approach does not work for users who patch the library by replacing some modules; this is a secondary concern since we do not officially offer this as a feature.

Requirement

Analysis

Coverage

~ Many useful tests require additional internal interfaces

Correctness

+ Does not require a product change

~ The tests may call internal functions in a way that does not reflect actual usage inside the product

Effacement

++ Fine as long as the internal interfaces aren’t added solely for test purposes

Portability

+ Fine as long as we control how the tests are linked

~ Doesn’t work if the users rewrite an internal module

Maintainability

+ Tests interfaces that are documented; dependencies in the tests are easily noticed when changing these interfaces

Static analysis#

If we guarantee certain properties through static analysis, we don’t need to test them. This puts some constraints on the properties:

  • We need to have confidence in the specification (but we can gain this confidence by evaluating the specification on test data).

  • This does not work for platform-dependent properties unless we have a formal model of the platform.

Requirement

Analysis

Coverage

~ Good for platform-independent properties, if we can guarantee them statically

Correctness

+ Good as long as we have confidence in the specification

Effacement

++ Zero impact on the code

Portability

++ Zero runtime burden

Maintainability

~ Static analysis is hard, but it’s also helpful

Compile-time options#

If there’s code that we want to have in the product for testing, but not in production, we can add a compile-time option to enable it. This is very powerful and usually easy to use, but comes with a major downside: we aren’t testing the same code anymore.

Requirement

Analysis

Coverage

++ Most things can be tested that way

Correctness

! Difficult to ensure that what we test is what we run

Effacement

++ No impact on the product when built normally or on the documentation, if done right

! Risk of getting “no impact” wrong

Portability

++ It’s just C code so it works everywhere

~ Doesn’t work if the users rewrite an internal module

Maintainability

+ Test interfaces impact the product source code, but at least they’re clearly marked as such in the code

Guidelines for compile-time options#

  • Minimize the number of compile-time options.
    Either we’re testing or we’re not. Fine-grained options for testing would require more test builds, especially if combinatorics enters the play.

  • Merely enabling the compile-time option should not change the behavior.
    When building in test mode, the code should have exactly the same behavior. Changing the behavior should require some action at runtime (calling a function or changing a variable).

  • Minimize the impact on code.
    We should not have test-specific conditional compilation littered through the code, as that makes the code hard to read.

Runtime instrumentation#

Some properties can be tested through runtime instrumentation: have the compiler or a similar tool inject something into the binary.

  • Sanitizers check for certain bad usage patterns (ASan, MSan, UBSan, Valgrind).

  • We can inject external libraries at link time. This can be a way to make system functions fail.

Requirement

Analysis

Coverage

! Limited scope

Correctness

+ Instrumentation generally does not affect the program’s functional behavior

Effacement

++ Zero impact on the code

Portability

~ Depends on the method

Maintainability

~ Depending on the instrumentation, this may require additional builds and scripts

+ Many properties come for free, but some require effort (e.g. the test code itself must be leak-free to avoid false positives in a leak detector)

Debugger-based testing#

If we want to do something in a test that the product isn’t capable of doing, we can use a debugger to read or modify the memory, or hook into the code at arbitrary points.

This is a very powerful approach, but it comes with limitations:

  • The debugger may introduce behavior changes (e.g. timing). If we modify data structures in memory, we may do so in a way that the code doesn’t expect.

  • Due to compiler optimizations, the memory may not have the layout that we expect.

  • Writing reliable debugger scripts is hard. We need to have confidence that we’re testing what we mean to test, even in the face of compiler optimizations. Languages such as gdb make it hard to automate even relatively simple things such as finding the place(s) in the binary corresponding to some place in the source code.

  • Debugger scripts are very much non-portable.

Requirement

Analysis

Coverage

++ The sky is the limit

Correctness

++ The code is unmodified, and tested as compiled (so we even detect compiler-induced bugs)

! Compiler optimizations may hinder

~ Modifying the execution may introduce divergence

Effacement

++ Zero impact on the code

Portability

!! Not all environments have a debugger, and even if they do, we’d need completely different scripts for every debugger

Maintainability

! Writing reliable debugger scripts is hard

!! Very tight coupling with the details of the source code and even with the compiler

Solutions#

This section lists some strategies that are currently used for invasive testing, or planned to be used. This list is not intended to be exhaustive.

Memory management#

Zeroization testing#

Goal: test that mbedtls_platform_zeroize does wipe the memory buffer.

Solution (debugger): implemented in framework/tests/programs/test_zeroize.gdb.

Rationale: this cannot be tested by adding C code, because the danger is that the compiler optimizes the zeroization away, and any C code that observes the zeroization would cause the compiler not to optimize it away.

Memory cleanup#

Goal: test the absence of memory leaks.

Solution (instrumentation): run tests with ASan. (We also use Valgrind, but it’s slower than ASan, so we favor ASan.)

Since we run many test jobs with a memory leak detector, each test function or test program must clean up after itself. Use the cleanup code (after the exit label in test functions) to free any memory that the function may have allocated.

Robustness against memory allocation failure#

Solution: TODO. We don’t test this at all at this point.

PSA key store memory cleanup#

Goal: test the absence of resource leaks in the PSA key store code, in particular that psa_close_key and psa_destroy_key work correctly.

Solution (internal interface): in most tests involving PSA functions, the cleanup code explicitly calls PSA_DONE() instead of mbedtls_psa_crypto_free(). PSA_DONE fails the test if the key store in memory is not empty.

Note there must also be tests that call mbedtls_psa_crypto_free with keys still open, to verify that it does close all keys.

PSA_DONE is a macro defined in psa_crypto_helpers.h which uses mbedtls_psa_get_stats() to get information about the keystore content before calling mbedtls_psa_crypto_free(). This feature is mostly but not exclusively useful for testing, and may be moved under MBEDTLS_TEST_HOOKS.

PSA storage#

PSA storage cleanup on success#

Goal: test that no stray files are left over in the key store after a test that succeeded.

Solution: TODO. Currently the various test suites do it differently.

PSA storage cleanup on failure#

Goal: ensure that no stray files are left over in the key store even if a test has failed (as that could cause other tests to fail).

Solution: TODO. Currently the various test suites do it differently.

PSA storage resilience#

Goal: test the resilience of PSA storage against power failures.

Solution: TODO.

See the secure element driver interface test strategy for more information.

Corrupted storage#

Goal: test the robustness against corrupted storage.

Solution (internal interface): call psa_its functions to modify the storage.

Storage read failure#

Goal: test the robustness against read errors.

Solution: TODO

Storage write failure#

Goal: test the robustness against write errors (STORAGE_FAILURE or INSUFFICIENT_STORAGE).

Solution: TODO

Storage format stability#

Goal: test that the storage format does not change between versions (or if it does, an upgrade path must be provided).

Solution (internal interface): call internal functions to inspect the content of the file.

Note that the storage format is defined not only by the general layout, but also by the numerical values of encodings for key types and other metadata. For numerical values, there is a risk that we would accidentally modify a single value or a few values, so the tests should be exhaustive. This probably requires some compile-time analysis (perhaps the automation for psa_constant_names can be used here). TODO

Other fault injection#

PSA crypto init failure#

Goal: test the failure of psa_crypto_init.

Solution (compile-time option): replace entropy initialization functions by functions that can fail. This is the only failure point for psa_crypto_init that is present in all builds.

When we implement the PSA entropy driver interface, this should be reworked to use the entropy driver interface.

PSA crypto data corruption#

The PSA crypto subsystem has a few checks to detect corrupted data in memory. We currently don’t have a way to exercise those checks.

Solution: TODO. To corrupt a multipart operation structure, we can do it by looking inside the structure content, but only when running without isolation. To corrupt the key store, we would need to add a function to the library or to use a debugger.