MCUXpresso SDK Documentation

Testing strategy for MBEDTLS_USE_PSA_CRYPTO#

This document records the testing strategy used so far in implementing MBEDTLS_USE_PSA_CRYPTO.

General considerations#

There needs to be at least one build in all.sh that enables MBEDTLS_USE_PSA_CRYPTO and runs the full battery of tests; currently that’s ensured by the fact that scripts/config.py full enables MBEDTLS_USE_PSA_CRYPTO. There needs to be at least one build with MBEDTLS_USE_PSA_CRYPTO disabled (as long as it’s optional); currently that’s ensured by the fact that it’s disabled in the default config.

Generally, code review is enough to ensure that PSA APIs are indeed used where they should be when MBEDTLS_USE_PSA_CRYPTO is enabled.

However, when it comes to TLS, we also have the option of using debug messages to confirm which code path is taken. This is generally unnecessary, except when a decision is made at run-time about whether to use the PSA or legacy code path. (For example, for record protection, previously (until 3.1), some ciphers were supported via PSA while some others weren’t, with a run-time fallback. In this case, it’s good to have a debug message checked by the test case to confirm that the right decision was made at run-time, i. e. that we didn’t use the fallback for ciphers that are supposed to be supported.)

New APIs meant for application use#

For example, mbedtls_pk_setup_opaque() is meant to be used by applications in order to create PK contexts that can then be passed to existing TLS and X.509 APIs (which remain unchanged).

In that case, we want:

  • unit testing of the new API and directly-related APIs - for example:

    • in test_suite_pk we have a new test function pk_psa_utils that exercises mbedtls_pk_setup_opaque() and checks that various utility functions (mbedtls_pk_get_type() etc.) work and the functions that are expected to fail (mbedtls_pk_verify() etc) return the expected error.

    • in test_suite_pk we modified the existing pk_psa_sign test function to check that signature generation works as expected

    • in test_suite_pkwrite we should have a new test function checking that exporting (writing out) the public part of the key works as expected and that exporting the private key fails as expected.

  • integration testing of the new API with each existing API which should accepts a context created this way - for example:

    • in programs/ssl/ssl_client2 a new option key_opaque that causes the new API to be used, and one or more tests in ssl-opt.sh using that. (We should have the same server-side.)

    • in test_suite_x509write we have a new test function x509_csr_check_opaque() checking integration of the new API with the existing mbedtls_x509write_csr_set_key(). (And also mbedtls_x509write_crt_set_issuer_key() since #5710.)

For some APIs, for example with mbedtls_ssl_conf_psk_opaque(), testing in test_suite_ssl was historically not possible, so we only have testing in ssl-opt.sh.

New APIs meant for internal use#

For example, mbedtls_cipher_setup_psa() (no longer used, soon to be deprecated - #5261) was meant to be used by the TLS layer, but probably not directly by applications.

In that case, we want:

  • unit testing of the new API and directly-related APIs - for example:

    • in test_suite_cipher, the existing test functions auth_crypt_tv and test_vec_crypt gained a new parameter use_psa and corresponding test cases

  • integration testing:

    • usually already covered by existing tests for higher-level modules:

      • for example simple use of mbedtls_cipher_setup_psa() in TLS is already covered by running the existing TLS tests in a build with MBEDTLS_USA_PSA_CRYPTO enabled

    • however if use of the new API in higher layers involves more logic that use of the old API, specific integrations test may be required

      • for example, the logic to fall back from mbedtls_cipher_setup_psa() to mbedtls_cipher_setup() in TLS is tested by run_test_psa in ssl-opt.sh.

Internal changes#

For example, use of PSA to compute the TLS 1.2 PRF.

Changes in this category rarely require specific testing, as everything should be already be covered by running the existing tests in a build with MBEDTLS_USE_PSA_CRYPTO enabled; however we need to make sure the existing test have sufficient coverage, and improve them if necessary.

However, if additional logic is involved, or there are run-time decisions about whether to use the PSA or legacy code paths, specific tests might be in order.