Migrating from Mbed TLS 2.x to Mbed TLS 3.0
This guide details the steps required to migrate from Mbed TLS version 2.x to Mbed TLS version 3.0 or greater. Unlike normal releases, Mbed TLS 3.0 breaks compatibility with previous versions, so users (and alt implementers) might need to change their own code in order to make it work with Mbed TLS 3.0.
Here’s the list of breaking changes; each entry should help you answer these two questions: (1) am I affected? (2) if yes, what’s my migration path?
The changes are detailed below, and include:
Removal of many insecure or obsolete features
Tidying up of configuration options (including removing some less useful options).
Changing function signatures, e.g. adding return codes, adding extra parameters, or making some arguments const.
Removal of functions, macros, and types previously marked as deprecated.
Much of the information needed to determine a migration path can be found in the Mbed TLS 2.x documentation.
Accessing the Mbed TLS 2.x documentation
For features previously marked as deprecated, Mbed TLS 2.x documentation may explain how to upgrade, and should be referred to when migrating code. Where a migration path is not provided in prior documentation, changes made and the upgrade steps required will be explained later in this guide.
It’s best to use the latest version of Mbed TLS 2.x for this purpose, which is the 2.28 LTS release.
So to generate the documentation, checkout the mbedtls-2.28 branch and follow
the instructions in the Documentation section of the README.
Then browse apidoc/deprecated.html for guidance on upgrading deprecated code.
For some deprecated functions, 2.x documentation will suggest using a variant
suffixed with _ret. In Mbed TLS 3.x, this change may not be required, as most
of these variants have been renamed without the suffix. The section
Rename mbedtls_*_ret…
has further detail on which functions this applies to.
General changes
Introduce a level of indirection and versioning in the config files
config.h was split into build_info.h and mbedtls_config.h.
In code, use
#include <mbedtls/build_info.h>. Don’t includembedtls/config.hand don’t refer toMBEDTLS_CONFIG_FILE.In build tools, edit
mbedtls_config.h, or editMBEDTLS_CONFIG_FILEas before.If you had a tool that parsed the library version from
include/mbedtls/version.h, this has moved toinclude/mbedtls/build_info.h. From C code, both headers now define theMBEDTLS_VERSION_xxxmacros.
Also, if you have a custom configuration file:
Don’t include
check_config.horconfig_psa.hanymore.Don’t define
MBEDTLS_CONFIG_Hanymore.
A config file version symbol, MBEDTLS_CONFIG_VERSION was introduced.
Defining it to a particular value will ensure that Mbed TLS interprets
the config file in a way that’s compatible with the config file format
used by the Mbed TLS release whose MBEDTLS_VERSION_NUMBER has the same
value.
The only value supported by Mbed TLS 3.0.0 is 0x03000000.
Most structure fields are now private
Direct access to fields of structures (struct types) declared in public headers is no longer supported. In Mbed TLS 3, the layout of structures is not considered part of the stable API, and minor versions (3.1, 3.2, etc.) may add, remove, rename, reorder or change the type of structure fields.
There is a small number of exceptions where some fields are guaranteed to remain stable throughout the lifetime of Mbed TLS 3.x. These fields are explicitly documented as public. Please note that even if all the fields of a structure are public, future versions may add new fields. Also, as before, some public fields should be considered read-only, since modifying them may make the structure inconsistent; check the documentation in each case.
Attempting to access a private field directly will result in a compilation error.
If you were accessing structure fields directly, and these fields are not documented as public, you need to change your code. If an accessor (getter/setter) function exists, use that. Direct accessor functions are usually called mbedtls_<MODULE>_{get,set}_<FIELD> or mbedtls_<MODULE>_<STRUCTURE>_{get,set}_<FIELD>. Accessor functions that change the format may use different verbs, for example read/write for functions that import/export data from/to a text or byte string.
If no accessor function exists, please open an enhancement request against Mbed TLS and describe your use case. The Mbed TLS development team is aware that some useful accessor functions are missing in the 3.0 release, and we expect to add them to the first minor release(s) (3.1, etc.).
As a last resort, you can access the field foo of a structure bar by writing bar.MBEDTLS_PRIVATE(foo). Note that you do so at your own risk, since such code is likely to break in a future minor version of Mbed TLS. In the Mbed TLS 3.6 LTS this will tend to be safer than in a normal minor release because LTS versions try to maintain ABI stability.
Move part of timing module out of the library
The change affects users who use any of the following functions:
mbedtls_timing_self_test(), mbedtls_hardclock_poll(),
mbedtls_timing_hardclock() and mbedtls_set_alarm().
If you were relying on these functions, you’ll now need to change to using your platform’s corresponding functions directly.
Deprecated net.h file was removed
The file include/mbedtls/net.h was removed because its only function was to
include mbedtls/net_sockets.h which now should be included directly.
Remove MBEDTLS_CHECK_PARAMS option
This change does not affect users who use the default configuration; it only affects users who enabled that option.
The option MBEDTLS_CHECK_PARAMS (disabled by default) enabled certain kinds
of “parameter validation”. It covered two kinds of validations:
In some functions that require a valid pointer, “parameter validation” checks that the pointer is non-null. With the feature disabled, a null pointer is not treated differently from any other invalid pointer, and typically leads to a runtime crash. 90% of the uses of the feature are of this kind.
In some functions that take an enum-like argument, “parameter validation” checks that the value is a valid one. With the feature disabled, an invalid value causes a silent default to one of the valid values.
The default reaction to a failed check was to call a function
mbedtls_param_failed() which the application had to provide. If this function
returned, its caller returned an error MBEDTLS_ERR_xxx_BAD_INPUT_DATA.
This feature was only used in some classic (non-PSA) cryptography modules. It was not used in X.509, TLS or in PSA crypto, and it was not implemented in all classic crypto modules.
This feature has been removed. The library no longer checks for NULL pointers; checks for enum-like arguments will be kept or re-introduced on a case-by-case basis, but their presence will no longer be dependent on a compile-time option.
Validation of enum-like values is somewhat useful, but not extremely important, because the parameters concerned are usually constants in applications.
For more information see issue #4313.
Remove the MBEDTLS_TEST_NULL_ENTROPY configuration option
This does not affect users who use the default mbedtls_config.h, as this option was
already off by default.
If you were using the MBEDTLS_TEST_NULL_ENTROPY option and your platform
doesn’t have any entropy source, you should use MBEDTLS_ENTROPY_NV_SEED
and make sure your device is provisioned with a strong random seed.
Alternatively, for testing purposes only, you can create and register a fake
entropy function.
Remove the HAVEGE module
This doesn’t affect people using the default configuration as it was already disabled by default.
This only affects users who called the HAVEGE modules directly (not
recommended), or users who used it through the entropy module but had it as the
only source of entropy. If you’re in that case, please declare OS or hardware
RNG interfaces with mbedtls_entropy_add_source() and/or use an entropy seed
file created securely during device provisioning. See
https://mbed-tls.readthedocs.io/en/latest/kb/how-to/add-entropy-sources-to-entropy-pool for more
information.
Remove helpers for the transition from Mbed TLS 1.3 to Mbed TLS 2.0
This only affects people who’ve been using Mbed TLS since before version 2.0
and still relied on compat-1.3.h in their code.
Please use the new names directly in your code; scripts/rename.pl (from any
of the 2.x releases — no longer included in 3.0) might help you do that.
Low-level crypto
Please also refer to the section High-level crypto for changes that could sit in either category.
Deprecated functions were removed from bignum
The function mbedtls_mpi_is_prime() was removed. Please use
mbedtls_mpi_is_prime_ext() instead which additionally allows specifying the
number of Miller-Rabin rounds.
Deprecated functions were removed from DRBGs
The functions mbedtls_ctr_drbg_update_ret() and mbedtls_hmac_drbg_update_ret()
were renamed to replace the corresponding functions without _ret appended. Please call
the name without _ret appended and check the return value.
Deprecated hex-encoded primes were removed from DHM
The macros MBEDTLS_DHM_RFC5114_MODP_2048_P, MBEDTLS_DHM_RFC5114_MODP_2048_G,
MBEDTLS_DHM_RFC3526_MODP_2048_P, MBEDTLS_DHM_RFC3526_MODP_2048_G,
MBEDTLS_DHM_RFC3526_MODP_3072_P, MBEDTLS_DHM_RFC3526_MODP_3072_G,
MBEDTLS_DHM_RFC3526_MODP_4096_P and MBEDTLS_DHM_RFC3526_MODP_4096_G were
removed. The primes from RFC 5114 are deprecated because their derivation is not
documented and therefore their usage constitutes a security risk; they are fully
removed from the library. Please use parameters from RFC 3526 (still in the
library, only in binary form) or RFC 7919 (also available in the library) or
other trusted sources instead.
Deprecated functions were removed from hashing modules
Modules: MD5, SHA1, SHA256, SHA512, MD.
The functions
mbedtls_xxx_starts_ret(),mbedtls_xxx_update_ret(),mbedtls_xxx_finish_ret()andmbedtls_xxx_ret()were renamed to replace the corresponding functions without_retappended. Please call the name without_retappended and check the return value.The function
mbedtls_md_init_ctx()was removed; please usembedtls_md_setup()instead.The functions
mbedtls_xxx_process()were removed. You normally don’t need to call that from application code. However if you do (or if you want to provide your own version of that function), please usembedtls_internal_xxx_process()instead, and check the return value.
Change MBEDTLS_ECP_FIXED_POINT_OPTIM behavior
The option MBEDTLS_ECP_FIXED_POINT_OPTIM now increases code size and it does
not increase peak RAM usage anymore.
If you are limited by code size, you can define MBEDTLS_ECP_FIXED_POINT_OPTIM
to 0 in your config file. The impact depends on the number and size of
enabled curves. For example, for P-256 the difference is 1KB; see the documentation
of this option for details.
Separated MBEDTLS_SHA224_C and MBEDTLS_SHA256_C
This does not affect users who use the default mbedtls_config.h. MBEDTLS_SHA256_C
was enabled by default. Now both MBEDTLS_SHA256_C and MBEDTLS_SHA224_C are
enabled.
If you were using custom config file with MBEDTLS_SHA256_C enabled, then
you will need to add #define MBEDTLS_SHA224_C option to your config.
Current version of the library does not support enabling MBEDTLS_SHA256_C
without MBEDTLS_SHA224_C.
Replaced MBEDTLS_SHA512_NO_SHA384 with MBEDTLS_SHA384_C
This does not affect users who use the default mbedtls_config.h.
MBEDTLS_SHA512_NO_SHA384 was disabled by default, now MBEDTLS_SHA384_C is
enabled by default.
If you were using a config file with both MBEDTLS_SHA512_C and
MBEDTLS_SHA512_NO_SHA384, then just remove the MBEDTLS_SHA512_NO_SHA384.
If you were using a config file with MBEDTLS_SHA512_C and without
MBEDTLS_SHA512_NO_SHA384 and you need the SHA-384 algorithm, then add
#define MBEDTLS_SHA384_C to your config file.
GCM multipart interface: application changes
The GCM module now supports arbitrary chunked input in the multipart interface.
This changes the interface for applications using the GCM module directly for multipart operations.
Applications using one-shot GCM or using GCM via the mbedtls_cipher_xxx or psa_aead_xxx interfaces do not require any changes.
mbedtls_gcm_starts()now only sets the mode and the nonce (IV). Call the new functionmbedtls_gcm_update_ad()to pass the associated data.mbedtls_gcm_update()now takes an extra parameter to indicate the actual output length. In Mbed TLS 2.x, applications had to pass inputs consisting of whole 16-byte blocks except for the last block (this limitation has been lifted). In this case:As long as the input remains block-aligned, the output length is exactly the input length, as before.
If the length of the last input is not a multiple of 16, alternative implementations may return the last partial block in the call to
mbedtls_gcm_finish()instead of returning it in the last call tombedtls_gcm_update().
mbedtls_gcm_finish()now takes an extra output buffer for the last partial block. This is needed for alternative implementations that can only process a whole block at a time.
GCM interface changes: impact for alternative implementations
The GCM multipart interface has changed as described in “GCM multipart interface: application changes”. The consequences for an alternative implementation of GCM (MBEDTLS_GCM_ALT) are as follows:
mbedtls_gcm_starts()now only sets the mode and the nonce (IV). The new functionmbedtls_gcm_update_ad()receives the associated data. It may be called multiple times.mbedtls_gcm_update()now allows arbitrary-length inputs, takes an extra parameter to indicate the actual output length. Alternative implementations may choose between two modes:Always return the partial output immediately, even if it does not consist of a whole number of blocks.
Buffer the data for the last partial block, to be returned in the next call to
mbedtls_gcm_update()ormbedtls_gcm_finish().
mbedtls_gcm_finish()now takes an extra output buffer for the last partial block if needed.
The configuration option MBEDTLS_ECP_NO_INTERNAL_RNG was removed
This doesn’t affect users of the default configuration; it only affects people who were explicitly setting this option.
This was a trade-off between code size and countermeasures; it is no longer relevant as the countermeasure is now always on at no cost in code size.
SHA-512 and SHA-256 output type change
The output parameter of mbedtls_sha256_finish(), mbedtls_sha256(), mbedtls_sha512_finish(), mbedtls_sha512() now has a pointer type rather than array type. This makes no difference in terms of C semantics, but removes spurious warnings in some compilers when outputting a SHA-384 hash into a 48-byte buffer or a SHA-224 hash into a 28-byte buffer.
This makes no difference to a vast majority of applications. If your code takes a pointer to one of these functions, you may need to change the type of the pointer.
Alternative implementations of the SHA256 and SHA512 modules must adjust their functions’ prototype accordingly.
Deprecated error codes for hardware failures were removed
The macros
MBEDTLS_ERR_xxx_FEATURE_UNAVAILABLEfrom various crypto modules were removed;MBEDTLS_ERR_PLATFORM_FEATURE_UNSUPPORTEDis now used instead.The macro
MBEDTLS_ERR_RSA_UNSUPPORTED_OPERATIONwas removed;MBEDTLS_ERR_PLATFORM_FEATURE_UNSUPPORTEDis now used instead.The macros
MBEDTLS_ERR_xxx_HW_ACCEL_FAILEDfrom various crypto modules were removed;MBEDTLS_ERR_PLATFORM_HW_ACCEL_FAILEDis now used instead.
Deprecated error codes for invalid input data were removed
The macros
MBEDTLS_ERR_xxx_INVALID_KEY_LENGTHfrom ARIA and Camellia modules were removed;MBEDTLS_ERR_xxx_BAD_INPUT_DATAis now used instead.
Remove the mode parameter from RSA functions
This affects all users who use the RSA encrypt, decrypt, sign and verify APIs.
The RSA module no longer supports private-key operations with the public key or
vice versa. As a consequence, RSA operation functions no longer have a mode
parameter. If you were calling RSA operations with the normal mode (public key
for verification or encryption, private key for signature or decryption), remove
the MBEDTLS_RSA_PUBLIC or MBEDTLS_RSA_PRIVATE argument. If you were calling
RSA operations with the wrong mode, which rarely makes sense from a security
perspective, this is no longer supported.
Deprecated functions were removed from AES
The functions mbedtls_aes_encrypt() and mbedtls_aes_decrypt() were
removed.
If you’re simply using the AES module, you should be calling the higher-level
functions mbedtls_aes_crypt_xxx().
If you’re providing an alternative implementation using
MBEDTLS_AES_ENCRYPT_ALT or MBEDTLS_AES_DECRYPT_ALT, you should be
replacing the removed functions with mbedtls_internal_aes_encrypt() and
mbedtls_internal_aes_decrypt() respectively.
Deprecated functions were removed from ECDSA
The functions mbedtls_ecdsa_write_signature_det() and
mbedtls_ecdsa_sign_det() were removed. They were superseded by
mbedtls_ecdsa_write_signature() and mbedtls_ecdsa_sign_det_ext()
respectively.
Rename mbedtls_*_ret() cryptography functions whose deprecated variants have been removed
This change affects users who were using the mbedtls_*_ret() cryptography
functions.
Those functions were created based on now-deprecated functions according to a requirement that a function needs to return a value. This change brings back the original names of those functions. The renamed functions are:
name before this change |
after the change |
|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
To migrate to this change the user can keep the *_ret names in their code
and include the compat_2.x.h header file which holds macros with proper
renaming or to rename those functions in their code according to the list from
mentioned header file.
Remove the RNG parameter from RSA verify functions
RSA verification functions also no longer take random generator arguments (this was only needed when using a private key). This affects all applications using the RSA verify functions.
Remove the padding parameters from mbedtls_rsa_init()
This affects all users who use the RSA encrypt, decrypt, sign and verify APIs.
The function mbedtls_rsa_init() no longer supports selecting the PKCS#1 v2.1
encoding and its hash. It just selects the PKCS#1 v1.5 encoding by default. If
you were using the PKCS#1 v2.1 encoding you now need, subsequently to the call
to mbedtls_rsa_init(), to call mbedtls_rsa_set_padding() to set it.
To choose the padding type when initializing a context, instead of
mbedtls_rsa_init(ctx, padding, hash_id);
use
mbedtls_rsa_init(ctx);
mbedtls_rsa_set_padding(ctx, padding, hash_id);
To use PKCS#1 v1.5 padding, instead of
mbedtls_rsa_init(ctx, MBEDTLS_RSA_PKCS_V15, <ignored>);
just use
mbedtls_rsa_init(ctx);
High-level crypto
Please also refer to the section Low-level crypto for changes that could sit in either category.
Calling mbedtls_cipher_finish() is mandatory for all multi-part operations
This only affects people who use the cipher module to perform AEAD operations using the multi-part API.
Previously, the documentation didn’t state explicitly if it was OK to call
mbedtls_cipher_check_tag() or mbedtls_cipher_write_tag() directly after
the last call to mbedtls_cipher_update() — that is, without calling
mbedtls_cipher_finish() in-between. If your code was missing that call,
please add it and be prepared to get as much as 15 bytes of output.
Currently the output is always 0 bytes, but it may be more when alternative implementations of the underlying primitives are in use, or with future versions of the library.
Remove MD2, MD4, RC4, Blowfish and XTEA algorithms
This change affects users of the MD2, MD4, RC4, Blowfish and XTEA algorithms.
They are already niche or obsolete and most of them are weak or broken. For those reasons possible users should consider switching to modern and safe alternatives to be found in the literature.
Deprecated functions were removed from cipher
The functions mbedtls_cipher_auth_encrypt() and
mbedtls_cipher_auth_decrypt() were removed. They were superseded by
mbedtls_cipher_auth_encrypt_ext() and mbedtls_cipher_auth_decrypt_ext()
respectively which additionally support key wrapping algorithms such as
NIST_KW.
Extra parameter for the output buffer size
The following functions now take an extra parameter indicating the size of the output buffer:
mbedtls_ecdsa_write_signature(),mbedtls_ecdsa_write_signature_restartable()mbedtls_pk_sign(),mbedtls_pk_sign_restartable()
The requirements for the output buffer have not changed, but passing a buffer that is too small now reliably causes the functions to return an error, rather than overflowing the buffer.
Signature functions now require the hash length to match the expected value
This affects users of the PK API as well as users of the low-level API in the RSA module. Users of the PSA API or of the ECDSA module are unaffected.
All the functions in the RSA module that accept a hashlen parameter used to
ignore it unless the md_alg parameter was MBEDTLS_MD_NONE, indicating raw
data was signed. The hashlen parameter is now always the size that is read
from the hash input buffer. This length must be equal to the output size of
the hash algorithm used when signing a hash. (The requirements when signing
raw data are unchanged.) This affects the following functions:
mbedtls_rsa_pkcs1_sign,mbedtls_rsa_pkcs1_verifymbedtls_rsa_rsassa_pkcs1_v15_sign,mbedtls_rsa_rsassa_pkcs1_v15_verifymbedtls_rsa_rsassa_pss_sign,mbedtls_rsa_rsassa_pss_verifymbedtls_rsa_rsassa_pss_sign_ext,mbedtls_rsa_rsassa_pss_verify_ext
The signature functions in the PK module no longer accept 0 as the hash_len parameter. The hash_len parameter is now always the size that is read from the hash input buffer. This affects the following functions:
mbedtls_pk_sign,mbedtls_pk_verifymbedtls_pk_sign_restartable,mbedtls_pk_verify_restartablembedtls_pk_verify_ext
The migration path is to pass the correct value to those functions.
Some function parameters were made const
Various functions in the PK and ASN.1 modules had a const qualifier added to
some of their parameters.
This normally doesn’t affect your code, unless you use pointers to reference those functions. In this case, you’ll need to update the type of your pointers in order to match the new signature.
The RNG parameter is now mandatory for all functions that accept one
This change affects all users who called a function accepting a f_rng
parameter with NULL as the value of this argument; this is no longer
supported.
The changed functions are: the X.509 CRT and CSR writing functions; the PK and
RSA sign and decrypt functions; mbedtls_rsa_private(); the functions in DHM
and ECDH that compute the shared secret; the scalar multiplication functions in
ECP.
You now need to pass a properly seeded, cryptographically secure RNG to all
functions that accept a f_rng parameter. It is of course still possible to
pass NULL as the context pointer p_rng if your RNG function doesn’t need a
context.
Alternative implementations of a module (enabled with the MBEDTLS_module_ALT
configuration options) may have their own internal and are free to ignore the
f_rng argument but must allow users to pass one anyway.
Some functions gained an RNG parameter
This affects users of the following functions: mbedtls_ecp_check_pub_priv(),
mbedtls_pk_check_pair(), mbedtls_pk_parse_key(), and
mbedtls_pk_parse_keyfile().
You now need to pass a properly seeded, cryptographically secure RNG when calling these functions. It is used for blinding, a countermeasure against side-channel attacks.
PSA
Deprecated names for PSA constants and types were removed
Some constants and types that were present in beta versions of the PSA Crypto API were removed from version 1.0 of specification. Please switch to the new names provided by the 1.0 specification instead.
Changes that only affect alternative implementations
Internal / alt-focused headers were moved to a private location
This shouldn’t affect users who took care not to include headers that were documented as internal, despite being in the public include directory.
If you’re providing alt implementations of ECP or RSA, you’ll need to add our
library directory to your include path when building your alt
implementations, and note that ecp_internal.h and rsa_internal.h have been
renamed to ecp_internal_alt.h and rsa_alt_helpers.h respectively.
If you’re a library user and used to rely on having access to a structure or function that’s now in a private header, please reach out on the mailing list and explain your need; we’ll consider adding a new API in a future version.
CCM interface changes: impact for alternative implementations
The CCM interface has changed with the addition of support for
multi-part operations. Five new API functions have been defined:
mbedtls_ccm_starts(), mbedtls_ccm_set_lengths(),
mbedtls_ccm_update_ad(), mbedtls_ccm_update() and mbedtls_ccm_finish().
Alternative implementations of CCM (MBEDTLS_CCM_ALT) have now to
implement those additional five API functions.
X.509
Remove the certs module from the library
This should not affect production use of the library, as the certificates and keys included there were never suitable for production use.
However it might affect you if you relied on them for testing purposes. In
that case, please embed your own test certificates in your test code; now that
certs.c is out of the library there is no longer any stability guaranteed
and it may change in incompatible ways at any time.
Change the API to allow adding critical extensions to CSRs
This affects applications that call the mbedtls_x509write_csr_set_extension
function.
The API is changed to include the parameter critical which enables marking an
extension included in a CSR as critical. To get the previous behavior pass 0.
Remove the config option MBEDTLS_X509_ALLOW_UNSUPPORTED_CRITICAL_EXTENSION
This change does not affect users of the default configuration; it only affects users who enable this option.
The X.509 standard says that implementations must reject critical extensions that they don’t recognize, and this is what Mbed TLS does by default. This option allowed to continue parsing those certificates but didn’t provide a convenient way to handle those extensions.
The migration path from that option is to use the
mbedtls_x509_crt_parse_der_with_ext_cb() function which is functionally
equivalent to mbedtls_x509_crt_parse_der(), and/or
mbedtls_x509_crt_parse_der_nocopy() but it calls the callback with every
unsupported certificate extension and additionally the “certificate policies”
extension if it contains any unsupported certificate policies.
Remove MBEDTLS_X509_CHECK_*_KEY_USAGE options from mbedtls_config.h
This change affects users who have chosen the configuration options to disable the
library’s verification of the keyUsage and extendedKeyUsage fields of X.509
certificates.
The MBEDTLS_X509_CHECK_KEY_USAGE and MBEDTLS_X509_CHECK_EXTENDED_KEY_USAGE
configuration options are removed and the X.509 code now behaves as if they were
always enabled. It is consequently not possible anymore to disable at compile
time the verification of the keyUsage and extendedKeyUsage fields of X.509
certificates.
The verification of the keyUsage and extendedKeyUsage fields is important,
disabling it can cause security issues and it is thus not recommended. If the
verification is for some reason undesirable, it can still be disabled by means
of the verification callback function passed to mbedtls_x509_crt_verify() (see
the documentation of this function for more information).
Remove the MBEDTLS_X509_ALLOW_EXTENSIONS_NON_V3 option
This change does not affect users who were using the default configuration, as this option was already disabled by default. Also, it does not affect users who are working with current V3 X.509 certificates.
Extensions were added in V3 of the X.509 specification, so pre-V3 certificates containing extensions were never compliant. Mbed TLS now rejects them with a parsing error in all configurations, as it did previously in the default configuration.
If you are working with the pre-V3 certificates you need to switch to the current ones.
Strengthen default algorithm selection for X.509
This is described in the section Strengthen default algorithm selection for X.509 and TLS.
Remove wrapper for libpkcs11-helper
This doesn’t affect people using the default configuration as it was already disabled by default.
If you used to rely on this module in order to store your private keys securely, please have a look at the key management facilities provided by the PSA crypto API. If you have a use case that’s not covered yet by this API, please reach out on the mailing list.
SSL
Remove support for TLS 1.0, 1.1 and DTLS 1.0
This change affects users of the TLS 1.0, 1.1 and DTLS 1.0 protocols.
These versions have been deprecated by RFC 8996. Keeping them in the library creates opportunities for misconfiguration and possibly downgrade attacks. More generally, more code means a larger attack surface, even if the code is supposedly not used.
The migration path is to adopt the latest versions of the protocol.
As a consequence of removing TLS 1.0, support for CBC record splitting was also removed, as it was a work-around for a weakness in this particular version. There is no migration path since the feature is no longer relevant.
As a consequence of currently supporting only one version of (D)TLS (and in the future 1.3 which will have a different version negotiation mechanism), support for fallback SCSV (RFC 7507) was also removed. There is no migration path as it’s no longer useful with TLS 1.2 and later.
As a consequence of currently supporting only one version of (D)TLS (and in the
future 1.3 which will have a different concept of ciphersuites), support for
configuring ciphersuites separately for each version via
mbedtls_ssl_conf_ciphersuites_for_version() was removed. Use
mbedtls_ssl_conf_ciphersuites() to configure ciphersuites to use with (D)TLS
1.2; in the future a different API will be added for (D)TLS 1.3.
Remove support for SSL 3.0
This doesn’t affect people using the default configuration as it was already disabled by default.
This only affects TLS users who explicitly enabled MBEDTLS_SSL_PROTO_SSL3
and relied on that version in order to communicate with peers that are not up
to date. If one of your peers is in that case, please try contacting them and
encouraging them to upgrade their software.
Remove support for parsing SSLv2 ClientHello
This doesn’t affect people using the default configuration as it was already disabled by default.
This only affects TLS servers that have clients who send an SSLv2 ClientHello. These days clients are very unlikely to do that. If you have a client that does, please try contacting them and encouraging them to upgrade their software.
Remove support for truncated HMAC
This affects users of truncated HMAC, that is, users who called
mbedtls_ssl_conf_truncated_hmac( ..., MBEDTLS_SSL_TRUNC_HMAC_ENABLED),
regardless of whether the standard version was used or compatibility version
(MBEDTLS_SSL_TRUNCATED_HMAC_COMPAT).
The recommended migration path for people who want minimal overhead is to use a CCM-8 ciphersuite.
Remove support for TLS record-level compression
This doesn’t affect people using the default configuration as it was already disabled by default.
This only affects TLS users who enabled MBEDTLS_ZLIB_SUPPORT. This will not
cause any failures however if you used to enable TLS record-level compression
you may find that your bandwidth usage increases without compression. There’s
no general solution to this problem; application protocols might have their
own compression mechanisms and are in a better position than the TLS stack to
avoid variants of the CRIME and BREACH attacks.
Remove support for TLS RC4-based ciphersuites
This does not affect people who used the default mbedtls_config.h and the default
list of ciphersuites, as RC4-based ciphersuites were already not negotiated in
that case.
Please switch to any of the modern, recommended ciphersuites (based on AES-GCM, AES-CCM or ChachaPoly for example) and if your peer doesn’t support any, encourage them to upgrade their software.
Remove support for TLS single-DES ciphersuites
This doesn’t affect people using the default configuration as it was already disabled by default.
Please switch to any of the modern, recommended ciphersuites (based on AES-GCM, AES-CCM or ChachaPoly for example) and if your peer doesn’t support any, encourage them to upgrade their software.
Remove support for TLS record-level hardware acceleration
This doesn’t affect people using the default configuration as it was already disabled by default.
This feature had been broken for a while so we doubt anyone still used it. However if you did, please reach out on the mailing list and let us know about your use case.
Remove config option MBEDTLS_SSL_DEFAULT_TICKET_LIFETIME
This doesn’t affect people using the default configuration.
This option has not had any effect for a long time. Please use the lifetime
parameter of mbedtls_ssl_ticket_setup() instead.
Combine the MBEDTLS_SSL_CID_PADDING_GRANULARITY and MBEDTLS_SSL_TLS1_3_PADDING_GRANULARITY options
This change affects users who modified the default mbedtls_config.h padding granularity
settings, i.e. enabled at least one of the options.
The mbedtls_config.h options MBEDTLS_SSL_CID_PADDING_GRANULARITY and
MBEDTLS_SSL_TLS1_3_PADDING_GRANULARITY were combined into one option because
they used exactly the same padding mechanism and hence their respective padding
granularities can be used in exactly the same way. This change simplifies the
code maintenance.
The new single option MBEDTLS_SSL_CID_TLS1_3_PADDING_GRANULARITY can be used
for both DTLS-CID and TLS 1.3.
TLS now favors faster curves over larger curves
The default preference order for curves in TLS now favors resource usage (performance and memory consumption) over size. The exact order is unspecified and may change, but generally you can expect 256-bit curves to be preferred over larger curves.
If you prefer a different order, call mbedtls_ssl_conf_groups() when configuring a TLS connection.
SSL key export interface change
This affects users of the SSL key export APIs:
mbedtls_ssl_conf_export_keys_cb()
mbedtls_ssl_conf_export_keys_ext_cb()
Those APIs have been removed and replaced by the new API
mbedtls_ssl_set_export_keys_cb(). This API differs from
the previous key export API in the following ways:
It is no longer bound to an SSL configuration, but to an SSL context. This allows users to more easily identify the connection an exported key belongs to.
It no longer exports raw keys and IV.
A secret type parameter has been added to identify which key is being exported. For TLS 1.2, only the master secret is exported, but upcoming TLS 1.3 support will add other kinds of keys.
The callback now specifies a void return type, rather than returning an error code. It is the responsibility of the application to handle failures in the key export callback, for example by shutting down the TLS connection.
For users which do not rely on raw keys and IV, adjusting to the new
callback type should be straightforward — see the example programs
programs/ssl/ssl_client2 and programs/ssl/ssl_server2 for callbacks
for NSSKeylog, EAP-TLS and DTLS-SRTP.
Users which require access to the raw keys used to secure application traffic may derive those by hand based on the master secret and the handshake transcript hashes which can be obtained from the raw data on the wire. Such users are also encouraged to reach out to the Mbed TLS team on the mailing list, to let the team know about their use case.
Remove MaximumFragmentLength (MFL) query API
This affects users which use the MFL query APIs
mbedtls_ssl_get_{input,output}_max_frag_len() to
infer upper bounds on the plaintext size of incoming and
outgoing record.
Users should switch to mbedtls_ssl_get_max_{in,out}_record_payload()
instead, which also provides such upper bounds but takes more factors
than just the MFL configuration into account.
Relaxed semantics for PSK configuration
This affects users which call the PSK configuration APIs
mbedtls_ssl_conf_psk() and mbedtls_ssl_conf_psk_opaque()
multiple times on the same SSL configuration.
In Mbed TLS 2.x, users would observe later calls overwriting
the effect of earlier calls, with the prevailing PSK being
the one that has been configured last. In Mbed TLS 3.0,
calling mbedtls_ssl_conf_psk[_opaque]() multiple times
will return an error, leaving the first PSK intact.
To achieve equivalent functionality when migrating to Mbed TLS 3.0,
users calling mbedtls_ssl_conf_psk[_opaque]() multiple times should
remove all but the last call, so that only one call to either
mbedtls_ssl_conf_psk() or mbedtls_ssl_conf_psk_opaque()
remains.
Remove the configuration to enable weak ciphersuites in SSL / TLS
This does not affect users who use the default mbedtls_config.h, as this option was
already off by default.
If you were using a weak cipher, please switch to any of the modern, recommended ciphersuites (based on AES-GCM, AES-CCM or ChachaPoly for example) and if your peer doesn’t support any, encourage them to upgrade their software.
If you were using a ciphersuite without encryption, you just have to
enable MBEDTLS_CIPHER_NULL_CIPHER now.
Remove the MBEDTLS_SSL_MAX_CONTENT_LEN configuration option
This affects users who use the MBEDTLS_SSL_MAX_CONTENT_LEN option to
set the maximum length of incoming and outgoing plaintext fragments,
which can save memory by reducing the size of the TLS I/O buffers.
This option is replaced by the more fine-grained options
MBEDTLS_SSL_IN_CONTENT_LEN and MBEDTLS_SSL_OUT_CONTENT_LEN that set
the maximum incoming and outgoing plaintext fragment lengths, respectively.
Remove the SSL API mbedtls_ssl_get_session_pointer()
This affects two classes of users:
Users who manually inspect parts of the current session through direct structure field access.
Users of session resumption who query the current session via
mbedtls_ssl_get_session_pointer()prior to saving or exporting it viambedtls_ssl_session_copy()ormbedtls_ssl_session_save(), respectively.
Migration paths:
Mbed TLS 3.0 does not offer a migration path for the use case 1: Like many other Mbed TLS structures, the structure of
mbedtls_ssl_sessionis no longer part of the public API in Mbed TLS 3.0, and direct structure field access is no longer supported. Please see the section on private structure fields for more details.Users should replace calls to
mbedtls_ssl_get_session_pointer()by calls tombedtls_ssl_get_session()as demonstrated in the example programprograms/ssl/ssl_client2.c.
Remove MBEDTLS_SSL_DTLS_BADMAC_LIMIT option
This change does not affect users who used the default mbedtls_config.h, as the option
MBEDTLS_SSL_DTLS_BADMAC_LIMIT was already on by default.
This option was a trade-off between functionality and code size: it allowed users who didn’t need that feature to avoid paying the cost in code size, by disabling it.
This option is no longer present, but its functionality is now always enabled.
Deprecated functions were removed from SSL
The function mbedtls_ssl_conf_dh_param() was removed. Please use
mbedtls_ssl_conf_dh_param_bin() or mbedtls_ssl_conf_dh_param_ctx() instead.
The function mbedtls_ssl_get_max_frag_len() was removed. Please use
mbedtls_ssl_get_max_out_record_payload() and
mbedtls_ssl_get_max_in_record_payload()
instead.
Remove MBEDTLS_SSL_RECORD_CHECKING option and enable its action by default
This change does not affect users who use the default mbedtls_config.h, as the
option MBEDTLS_SSL_RECORD_CHECKING was already on by default.
This option was added only to control compilation of one function,
mbedtls_ssl_check_record(), which is only useful in some specific cases, so it
was made optional to allow users who don’t need it to save some code space.
However, the same effect can be achieved by using link-time garbage collection.
Users who changed the default setting of the option need to change the config/ build system to remove that change.
Session Cache API Change
This affects users who use mbedtls_ssl_conf_session_cache()
to configure a custom session cache implementation different
from the one Mbed TLS implements in library/ssl_cache.c.
Those users will need to modify the API of their session cache
implementation to that of a key-value store with keys being
session IDs and values being instances of mbedtls_ssl_session:
typedef int mbedtls_ssl_cache_get_t( void *data,
unsigned char const *session_id,
size_t session_id_len,
mbedtls_ssl_session *session );
typedef int mbedtls_ssl_cache_set_t( void *data,
unsigned char const *session_id,
size_t session_id_len,
const mbedtls_ssl_session *session );
Since the structure of mbedtls_ssl_session is no longer public from 3.0
onwards, portable session cache implementations must not access fields of
mbedtls_ssl_session. See the corresponding migration guide. Users that
find themselves unable to migrate their session cache functionality without
accessing fields of mbedtls_ssl_session should describe their use case
on the Mbed TLS mailing list.
Changes in the SSL error code space
This affects users manually checking for the following error codes:
MBEDTLS_ERR_SSL_CERTIFICATE_REQUIREDMBEDTLS_ERR_SSL_INVALID_VERIFY_HASHMBEDTLS_ERR_SSL_CERTIFICATE_TOO_LARGEMBEDTLS_ERR_SSL_NO_CIPHER_CHOSENMBEDTLS_ERR_SSL_NO_USABLE_CIPHERSUITEMBEDTLS_ERR_SSL_BAD_HS_XXX
Migration paths:
MBEDTLS_ERR_SSL_CERTIFICATE_TOO_LARGEhas been removed, andMBEDTLS_ERR_SSL_BUFFER_TOO_SMALLis returned instead if the user’s own certificate is too large to fit into the output buffers.Users should check for
MBEDTLS_ERR_SSL_BUFFER_TOO_SMALLinstead, and potentially compare the size of their own certificate against the configured size of the output buffer to understand if the error is due to an overly large certificate.MBEDTLS_ERR_SSL_NO_CIPHER_CHOSENandMBEDTLS_ERR_SSL_NO_USABLE_CIPHERSUITEhave been replaced byMBEDTLS_ERR_SSL_HANDSHAKE_FAILURE.All codes of the form
MBEDTLS_ERR_SSL_BAD_HS_XXXhave been replaced by various alternatives, which give more information about the type of error raised.Users should check for the newly introduced generic error codes
MBEDTLS_ERR_SSL_DECODE_ERRORMBEDTLS_ERR_SSL_ILLEGAL_PARAMETER,MBEDTLS_ERR_SSL_HANDSHAKE_FAILUREMBEDTLS_ERR_SSL_BAD_PROTOCOL_VERSIONMBEDTLS_ERR_SSL_BAD_CERTIFICATEMBEDTLS_ERR_SSL_UNRECOGNIZED_NAMEMBEDTLS_ERR_SSL_UNSUPPORTED_EXTENSIONMBEDTLS_ERR_SSL_NO_APPLICATION_PROTOCOL
and the pre-existing generic error codes
MBEDTLS_ERR_SSL_UNEXPECTED_MESSAGEMBEDTLS_ERR_SSL_INTERNAL_ERROR
instead.
Modified semantics of mbedtls_ssl_{get,set}_session()
This affects users who call mbedtls_ssl_get_session() or
mbedtls_ssl_set_session() multiple times on the same SSL context
representing an established TLS 1.2 connection.
Those users will now observe the second call to fail with
MBEDTLS_ERR_SSL_FEATURE_UNAVAILABLE.
Migration path:
Exporting the same TLS 1.2 connection multiple times via
mbedtls_ssl_get_session()leads to multiple copies of the same session. This use ofmbedtls_ssl_get_session()is discouraged, and the following should be considered:If the various session copies are later loaded into fresh SSL contexts via
mbedtls_ssl_set_session(), export viambedtls_ssl_get_session()only once and load the same session into different contexts viambedtls_ssl_set_session(). Sincembedtls_ssl_set_session()makes a copy of the session that’s being loaded, this is functionally equivalent.If the various session copies are later serialized via
mbedtls_ssl_session_save(), export and serialize the session only once viambedtls_ssl_get_session()andmbedtls_ssl_session_save()and make copies of the raw data instead.
Calling
mbedtls_ssl_set_session()multiple times in Mbed TLS 2.x is not useful since subsequent calls overwrite the effect of previous calls. Applications achieve equivalent functional behavior by issuing only the very last call tombedtls_ssl_set_session().
Turn MBEDTLS_SSL_SRV_RESPECT_CLIENT_PREFERENCE configuration option into a runtime option
This change affects users who were enabling MBEDTLS_SSL_SRV_RESPECT_CLIENT_PREFERENCE
option in the mbedtls_config.h
This option has been removed and a new function with similar functionality has been introduced into the SSL API.
This new function mbedtls_ssl_conf_preference_order() can be used to
change the preferred order of ciphersuites on the server to those used on the client,
e.g.: mbedtls_ssl_conf_preference_order(ssl_config, MBEDTLS_SSL_SRV_CIPHERSUITE_ORDER_CLIENT)
has the same effect as enabling the removed option. The default state is to use
the server order of suites.
Strengthen default algorithm selection for X.509 and TLS
The default X.509 verification profile (mbedtls_x509_crt_profile_default) and the default curve and hash selection in TLS have changed. They are now aligned, except that the X.509 profile only lists curves that support signature verification.
Hashes and curves weaker than 255 bits (security strength less than 128 bits) are no longer accepted by default. The following hashes have been removed: SHA-1 (formerly only accepted for key exchanges but not for certificate signatures), SHA-224 (weaker hashes were already not accepted). The following curves have been removed: secp192r1, secp224r1, secp192k1, secp224k1.
The compile-time options MBEDTLS_TLS_DEFAULT_ALLOW_SHA1_IN_CERTIFICATES and MBEDTLS_TLS_DEFAULT_ALLOW_SHA1_IN_KEY_EXCHANGE are no longer available.
The curve secp256k1 has also been removed from the default X.509 and TLS profiles. RFC 8422 deprecates it in TLS, and it is very rarely used, although it is not known to be weak at the time of writing.
If you still need to accept certificates signed with algorithms that have been removed from the default profile, call mbedtls_x509_crt_verify_with_profile instead of mbedtls_x509_crt_verify and pass a profile that allows the curves and hashes you want. For example, to allow SHA-224:
mbedtls_x509_crt_profile my_profile = mbedtls_x509_crt_profile_default;
my_profile.allowed_mds |= MBEDTLS_X509_ID_FLAG( MBEDTLS_MD_SHA224 );
If you still need to allow hashes and curves in TLS that have been removed from the default configuration, call mbedtls_ssl_conf_sig_hashes() and mbedtls_ssl_conf_groups() with the desired lists.
Remove 3DES ciphersuites
This change does not affect users using default settings for 3DES in mbedtls_config.h
because the 3DES ciphersuites were disabled by that.
3DES has weaknesses/limitations and there are better alternatives, and more and more standard bodies are recommending against its use in TLS.
The migration path here is to chose from the alternatives recommended in the literature, such as AES.