Explore Contents
This section helps you build basic understanding of current fundamental project content and guides you how to build and run the provided example project in whole SDK delivery.
Folder View
The whole MCUXpresso SDK project, after you have done the west init and west update operations follow the guideline at Getting Started Guide, have below folder structure:
Folder |
Description |
|---|---|
manifests |
Manifest repo, contains the manifest file to initialize and update the west workspace. |
mcuxsdk |
The MCUXpresso SDK source code, examples, middleware integration and script files. |
All the projects record in the Manifest repo are checked out to the folder mcuxsdk/, the layout of mcuxsdk folder is shown as below:
Folder |
Description |
|---|---|
arch |
Arch related files such as ARM CMSIS core files, RISC-V files and the build files related to the architecture. |
cmake |
The cmake modules, files which organize the build system. |
components |
Software components. |
devices |
Device support package which categorized by device series. For each device, header file, feature file, startup file and linker files are provided, also device specific drivers are included. |
docs |
Documentation source and build configuration for this sphinx built online documentation. |
drivers |
Peripheral drivers. |
examples |
Various demos and examples, support files on different supported boards. For each board support, there are board configuration files. |
middleware |
Middleware components integrated into SDK. |
rtos |
Rtos components integrated into SDK. |
scripts |
Script files for the west extension command and build system support. |
svd |
Svd files for devices, this is optional because of large size. Customers run |
Examples Project
The examples project is part of the whole SDK delivery, and locates in the folder mcuxsdk/examples of west workspace.
Examples files are placed in folder of <example_category>, these examples include (but are not limited to)
demo_apps: Basic demo set to start using SDK, including hello_world and led_blinky.
driver_examples: Simple applications that show how to use the peripheral drivers for a single use case. These applications typically only use a single peripheral but there are cases where multiple peripherals are used (for example, SPI transfer using DMA).
Board porting layers are placed in folder of _boards/<board_name> which aims at providing the board specific parts for examples code mentioned above.