TwinCAT project setup#
Import the EtherCAT Subdevice Information (ESI) file of the EoE example.
Copy the ESI file named ‘ECAT-EOE.xml’ generated by SSC tool from the SSC project folder to the <TwinCAT_installation_folder>/<Version>/Config/io/EtherCAT/ folder.
Create a new project.
Select File > New > Project.

The New Project dialog box appears.
Select TwinCAT Projects.
Click OK.

Scan the for subdevices.
In the Solution Explorer view, expand I/O.
Right-click on Device and select Scan.

The scanned devices appear in the I/O devices found dialog box.
Select the network interface connected with the MIMXRT1180-EVK board.
Click OK.

Configure the subdevice.
Click the DC tab.
From the Operation Mode field, select the SM-Synchron or DC option.

Program the PLC code.
In the Solution Explorer view, right-click on PLC and select Add New Item.

The Add New Item dialog box appears.
From the Installed list in the left pane, select PLC Templates.
Select Standard PLC Project.
Click OK.

To open the PLC edit page, select MAIN (PRG) under PLC.
Copy the code below and paste it in the MAIN view.
PROGRAM MAIN VAR Delay : TON; LedIn AT %I* : BOOL; LedOut AT %Q* : BOOL; END_VAR
Delay(IN := TRUE, PT := T#1S); IF Delay.Q THEN LedOut := NOT LedIn; Delay(IN := FALSE); END_IF;

Build the PLC code.
Right-click on the PLC project and select Build.

Map the PLC variables to the subdevice IO channel. 1. Right-click on MAIN.LedIn, select Change Link.

The Attach Variable MAIN.LedIn (Input) dialog box appears.
2. Select **LED**.
3. Click **OK**.
")
4. In the **Solution Explorer**, under **PlcTask Outputs**, right-click on **MAIN.LedOut** and select **Change Link**.

The **Attach Variable MAIN.LedOut \(Output\)** dialog box appears.
5. Select **LED**.
6. Click **OK**.
")
Configure the PC IP address.
ip address: 192.168.1.102subnet mask: 255.255.255.0gateway: 192.168.1.0
Configure the board IP address.
Under Device, double-click **Box1.**The TwinCAT Project dialog box appears.
Click the EtherCAT tab.
Click the Advanced Settings button.

The Advanced Settings dialog box appears.
Click Mailbox > EOE > IP Port.
Set the address of the board.
ip address: 192.168.1.66subnet mask: 255.255.255.0gateway: 192.168.1.102
Activate the configuration.
To activate the configuration, select TwinCAT > Restart TwinCAT (Config Mode)..

After activaing the configuration, the serial port prints the following.
Start the SSC EoE example... Hardware init success... EoE interface init success... *********************************************************** HTTP Server example *********************************************************** IPv4 Address : 192.168.1.66 IPv4 Subnet mask : 255.255.255.0 IPv4 Gateway : 192.168.1.102 mDNS hostname : lwip-eoe ***********************************************************
Test ping and the http server.
Open cmd.exe and execute “ping 192.168.1.66”.
Make sure to disable the browser proxy and open the browser to access http://192.168.1.66.

Note: To modify the html of http server, refer tolwip_examples/lwip_httpsrv example.