tsi_v4_low_power_mode#
Overview#
The tsi_v4_low_power example shows how to use TSI_V4 driver in low power modes:
In this example , we make use of the available electrodes on board to show driver usage.
Firstly, we get the non-touch calibration results as baseline electrode counter;
Then, we start the Hardware-Trigger scan using interrupt method to wakeup from low power modes through pad touch;
Note: you can select which low power mode you want to enter into.
Running the demo#
When running successfully, the log output in terminal shall be similar as below:
TSI_V4 Low_Power_Modes Example Start! Please don’t touch the touchpad. Press anykey to start TSI low power example. Start calibartion…. Calibrated counters for channel 0 is: 2772 Calibrated counters for channel 1 is: 65535 Calibrated counters for channel 2 is: 65535 Calibrated counters for channel 3 is: 65535 Calibrated counters for channel 4 is: 65535 Calibrated counters for channel 5 is: 65535 Calibrated counters for channel 6 is: 2965 Calibrated counters for channel 7 is: 2642 Calibrated counters for channel 8 is: 2682 Calibrated counters for channel 9 is: 2901 Calibrated counters for channel 10 is: 65535 Calibrated counters for channel 11 is: 2708 Calibrated counters for channel 12 is: 2958 Calibrated counters for channel 13 is: 5072 Calibrated counters for channel 14 is: 421 Calibrated counters for channel 15 is: 5073
Let’s move to the low power modes world!!!
Press specific key to enter stop mode. After enter stop modes, touch PAD XX to wakeup.
Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into STOP MODE! Great!!! You touched it!!!
Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into VLPS MODE! Great!!! You touched it!!!
Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into LLS MODE! Wakeup will lead to a interrupt flow, pay attention to it!!! Great!!! You touched it!!!
Please input the mode you want to enter! 0 ——> STOP MODE 1 ——> VLPS MODE 2 ——> LLS MODE 3 ——> VLLS1 MODE 4 ——> VLLS2 MODE 5 ——> VLLS3 MODE About to enter into VLLS1 MODE! Wakeup will lead to a reset flow, pay attention to it!!!
Wake up from VLLSx modes…
TSI_V4 Low_Power_Modes Example Start! Please don’t touch the touchpad. Press anykey to start TSI low power example. …… ……
Supported Boards#
FRDM-K32L2A4S
Hardware requirements
Mini/micro USB cable
FRDM-K32L2A4S board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
Download the code to device flash, do not using debug mode.
Power-off then power-on the board.
Open serial terminal utility with specific COM number, then press “Reset Button” on board.
Do as the message shown in terminal guides.
When the example runs successfully, you can see the similar information from the terminal as below.
Note: The message shown below will different depends on your input character.
============= TSI_V4 Low_Power_Modes Example Start! =============
Please don't touch the touchpad
Press anykey to start TSI low power example
Start calibartion....
Calibrated counters for channel 0 is: 757
Calibrated counters for channel 1 is: 65535
Calibrated counters for channel 2 is: 65535
Calibrated counters for channel 3 is: 65535
Calibrated counters for channel 4 is: 65535
Calibrated counters for channel 5 is: 65535
Calibrated counters for channel 6 is: 805
Calibrated counters for channel 7 is: 666
Calibrated counters for channel 8 is: 607
Calibrated counters for channel 9 is: 1583
Calibrated counters for channel 10 is: 1588
Calibrated counters for channel 11 is: 649
Calibrated counters for channel 12 is: 628
Calibrated counters for channel 13 is: 652
Calibrated counters for channel 14 is: 65535
Calibrated counters for channel 15 is: 747
Let's move to the low power modes world!!!
Press specific key to enter stop mode.
After enter stop modes, touch PAD E1 to wakeup.
Please input the mode you want to enter!
0 ------> STOP MODE
1 ------> VLPS MODE
2 ------> LLS MODE
3 ------> VLLS1 MODE
4 ------> VLLS2 MODE
5 ------> VLLS3 MODE