spi_interrupt_b2b_transfer_slave#
Overview#
The spi_interrupt_board2board_slave example shows how to use spi driver as slave to do board to board transfer with interrupt:
In this example, one spi instance as slave and another spi instance on other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from master is correct.