MCUXpresso SDK Documentation

queued_spi_edma_b2b_transfer_slave

queued_spi_edma_b2b_transfer_slave#

Overview#

The queued_spi_edma_b2b_transfer example shows how to use QUEUEDSPI driver in edma way:

In this example, we need two boards, one board is used as QUEUEDSPI master and another board is used as QUEUEDSPI slave. The file ‘queued_spi_edma_b2b_transfer_slave.c’ includes the DSPI slave code.

  1. QUEUEDSPI master sends/receives data to/from QUEUEDSPI slave in edma way. (QUEUEDSPI Slave uses edma way to receive/send the data)

Supported Boards#

MC56F80000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F80000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2

  2. Reset pin setting:

    Connect J11 pin2 and pin3

  3. Debugger setting:

    Connect J13 pin 1-2, 3-4, 5-6, 7-8

Board settings

Master/Slave board connection as below:

Master Board                             Slave Board
INSTANCE0(QSPI0)     CONNECTS TO         INSTANCE1(QSPI0)
Pin Name   Board Location      Pin Name  Board Location
SS0        J1 pin 3            SS0       J1 pin 3
MOSI       J2 pin 8            MOSI      J2 pin 8
MISO       J2 pin 10           MISO      J2 pin 10
SCK        J2 pin 12           SCK       J2 pin 12
GND        J2 pin 14           GND       J2 pin 14

Note: Don’t use GC7 as SS since GC7 is used for onboard MX25

Prepare the Demo
  1. Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with Multilink debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

QUEUEDSPI board to board EDMA example.

 Slave example is running...
This is QUEUEDSPI slave transfer completed callback. 
It's a successful transfer. 

 Slave receive:
      1  2  3  4  5  6  7  8  9  A  B  C  D  E  F 10
     11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20
     21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30
     31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F 40

 Slave example is running...
MC56F81000-EVK
Hardware requirements
  • 2 x Micro USB cable

  • MC56F81000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J8 pin2 and pin3 Connect J5 pin1 and pin2 Connect J6 pin1 and pin2

  2. Onboard PnE U-MultiLink debugger setting:

    Connet J11 pin2 and pin3 Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink. Note: when use external debugger(connected to J10), leave all J13 pins open.

Board settings

Master/Slave board connection as below:

Master Board                             Slave Board
INSTANCE0(QSPI0)     CONNECTS TO         INSTANCE1(QSPI0)
Pin Name   Board Location      Pin Name  Board Location
SS0        J1 pin 3            SS0       J1 pin 3
MOSI       J2 pin 8            MOSI      J2 pin 8
MISO       J2 pin 10           MISO      J2 pin 10
SCK        J2 pin 12           SCK       J2 pin 12
GND        J2 pin 14           GND       J2 pin 14

Note: Don’t use GC7 as SS since GC7 is used for onboard MX25

Prepare the Demo
  1. Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.

  2. Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board with PnE U-MultiLink debug configuration.

  5. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted default FCF(flash configuration field) makes the MCU boot from flash.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

QUEUEDSPI board to board EDMA example.

 Slave example is running...
This is QUEUEDSPI slave transfer completed callback. 
It's a successful transfer. 

 Slave receive:
      1  2  3  4  5  6  7  8  9  A  B  C  D  E  F 10
     11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20
     21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30
     31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F 40

 Slave example is running...
MC56F83000-EVK
Hardware requirements
  • Micro USB cable

  • MC56F83000-EVK board

  • Personal Computer

Board hardware common setting
  1. Power setting:

    Connect J19 pin2 and pin3 Connect J12 pin1 and pin2 Connect J13 pin1 and pin2 Connect J15 pin1 and pin2 Connect J16 pin2 and pin3 Connect J17 pin1 and pin2

  2. Onboard OSJTAG debugger setting:

    Leave J5 open Leave J6 open Note: J6 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J11 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J10), leave all J11 pins open.

Board settings

Master/Slave board connection as below:

Master Board                             Slave Board
INSTANCE0(QSPI0)     CONNECTS TO         INSTANCE1(QSPI0)
Pin Name   Board Location      Pin Name  Board Location
SS0        J2 pin 6            SS0       J2 pin 6
MOSI       J2 pin 8            MOSI      J2 pin 8
MISO       J2 pin 10           MISO      J2 pin 10
SCK        J2 pin 12           SCK       J2 pin 12
GND        J2 pin 14           GND       J2 pin 14
Prepare the Demo
  1. Connect USB cable between the host PC and the JM60 USB(J8) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted that default FCF(flash configuration field) setting makes MCU boot from bootloader. So after reset button press, it will wait 5s(wait in bootloader) to run the application code.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

QUEUEDSPI board to board EDMA example.

 Slave example is running...
This is QUEUEDSPI slave transfer completed callback. 
It's a successful transfer. 

 Slave receive:
      1  2  3  4  5  6  7  8  9  A  B  C  D  E  F 10
     11 12 13 14 15 16 17 18 19 1A 1B 1C 1D 1E 1F 20
     21 22 23 24 25 26 27 28 29 2A 2B 2C 2D 2E 2F 30
     31 32 33 34 35 36 37 38 39 3A 3B 3C 3D 3E 3F 40

 Slave example is running...