lpspi_3wire_polling_transfer_slave#
Overview#
The lpspi_3wire_polling_transfer example shows how to use LPSPI’s 3-wire mode in polling way:
In this example , we need two boards, one board used as LPSPI master and another board used as LPSPI slave. The file ‘lpspi_3wire_polling_transfer_slave.c’ includes the LPSPI slave code.
LPSPI master send/received data to/from LPSPI slave in polling . (LPSPI Slave using interrupt to receive/send the data)
LPSPI master will use SOUT pin as input/output pin, and slave will use SIN pin as input/output pin.
Supported Boards#
EVK-MIMXRT1015
Hardware requirements
Mini/micro USB cable
Two EVK-MIMXRT1015 boards
Personal Computer
Board settings
Remove R293 SPI one board: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board
MASTER connect to SLAVE
Pin Name Board Location Pin Name Board Location
SOUT J19-4 SIN J19-5
SCK J19-6 SCK J19-6
PCS0 J19-3 PCS0 J19-3
GND J19-7 GND J19-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Note: It’s better to use short dupont lines for ideal connection, error may occur if using long lines.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPSPI 3-wire board to board polling example.
Slave example is running...
Slave starts to receive data from master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave board receive data complete!
Slave received:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
Please input any character to continue!
Note that, slave should start first.So, please input character for slave first!
Slave starts to transmit data to master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave transmit data completed!
Slave example is running...
Slave starts to receive data from master.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
EVK-MIMXRT1020
Hardware requirements
Mini/micro USB cable
Two EVK-MIMXRT1020 board
Personal Computer
Board settings
SPI one board: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board
MASTER connect to SLAVE
Pin Name Board Location Pin Name Board Location
SOUT J19-4 SIN J19-5
SCK J19-6 SCK J19-6
PCS0 J19-3 PCS0 J19-3
GND J19-7 GND J19-7
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Note: It’s better to use short dupont lines for ideal connection, error may occur if using long lines.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPSPI 3-wire board to board polling example.
Slave example is running...
Slave starts to receive data from master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave board receive data complete!
Slave received:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
Please input any character to continue!
Note that, slave should start first.So, please input character for slave first!
Slave starts to transmit data to master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave transmit data completed!
Slave example is running...
Slave starts to receive data from master.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
MIMXRT1024-EVK
Hardware requirements
Mini/micro USB cable
Two MIMXRT1024-EVK boards
Personal Computer
Board settings
SPI one board: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board
MASTER connect to SLAVE
Pin Name Board Location Pin Name Board Location
SOUT J19-8 SIN J19-10
SCK J19-12 SCK J19-12
PCS0 J19-6 PCS0 J19-6
GND J19-14 GND J19-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPSPI 3-wire board to board polling example.
Slave example is running...
Slave starts to receive data from master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave board receive data complete!
Slave received:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
Please input any character to continue!
Note that, slave should start first.So, please input character for slave first!
Slave starts to transmit data to master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave transmit data completed!
Slave example is running...
Slave starts to receive data from master.
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.
FRDM-KE15Z
Hardware requirements
Micro USB cable
Two FRDM-KE15Z boards
Personal Computer
Board settings
SPI one board: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board
Master Board(SPI0) CONNECTS TO Slave Board(SPI0)
Pin Name Board Location Pin Name Board Location
SOUT J2 pin 8 SIN J2 pin 10
SCK J2 pin 12 SCK J2 pin 12
PCS3 J2 pin 6 PCS3 J2 pin 6
GND J2 pin 14 GND J2 pin 14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPSPI 3-wire board to board polling example.
Slave example is running...
Slave starts to receive data from master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave board receive data complete!
Slave received:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
Please input any character to continue!
Note that, slave should start first.So, please input character for slave first!
Slave starts to transmit data to master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave transmit data completed!
Slave example is running...
Slave starts to receive data from master.
FRDM-KE17Z
Hardware requirements
Micro USB cable
Two FRDM-KE17Z boards
Personal Computer
Board settings
SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board
Master Board(SPI0) CONNECTS TO Slave Board(SPI0)
Pin Name Board Location Pin Name Board Location
SOUT J2 pin 8 SIN J2 pin 10
SCK J2 pin 12 SCK J2 pin 12
PCS1 J2 pin 6 PCS1 J2 pin 6
GND J2 pin 14 GND J2 pin 14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPSPI 3-wire board to board polling example.
Slave example is running...
Slave starts to receive data from master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave board receive data complete!
Slave received:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
Please input any character to continue!
Note that, slave should start first.So, please input character for slave first!
Slave starts to transmit data to master.
This is LPSPI slave transfer completed callback.
It's a successful transfer.
Slave transmit data completed!
Slave example is running...
Slave starts to receive data from master.
FRDM-KE17Z512
Hardware requirements
Micro USB cable
Two FRDM-KE17Z512 boards
Personal Computer
Board settings
SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board
Master Board(SPI0) CONNECTS TO Slave Board(SPI0)
Pin Name Board Location Pin Name Board Location
SOUT J2 pin 8 SIN J2 pin 10
SCK J2 pin 12 SCK J2 pin 12
PCS2 J2 pin 6 PCS2 J2 pin 6
GND J2 pin 14 GND J2 pin 14
Prepare the Demo
Connect a USB cable between the PC host and the MCU-LINK USB port on the board.
Open a serial terminal on PC for MCU-LINK serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:
LPSPI 3-wire board to board edma example.
This example use one board as master and another as slave.
Master and slave uses EDMA way. Slave should start first.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
GND -- GND
Master transmit:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
This is LPSPI master edma transfer completed callback.
Master transmit data complete! Please input any character to continue!
Before you input any character, please make sure the slave board is ready to transmit data.
This is LPSPI master edma transfer completed callback.
LPSPI transfer all data matched!
Master received:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
Press any key to run again
FRDM-MCXE247
Hardware requirements
USB-C cable
Two FRDM-MCXE247 boards
Personal Computer
Board settings
SPI two boards: Transfer data from one board instance to another board’s instance. SPI0 pins are connected with SPI0 pins of another board
Master Board(SPI0) CONNECTS TO Slave Board(SPI0)
Pin Name Board Location Pin Name Board Location
SOUT J6 pin 6 SIN J6 pin 5
SCK J6 pin 4 SCK J6 pin 4
PCS2 J6 pin 3 PCS2 J6 pin 3
GND J6 pin 8 GND J6 pin 8
Prepare the Demo
Connect a USB cable between the PC host and the MCU-LINK USB port on the board.
Open a serial terminal on PC for MCU-LINK serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-LINK terminal like:
LPSPI 3-wire board to board edma example.
This example use one board as master and another as slave.
Master and slave uses EDMA way. Slave should start first.
Please make sure you make the correct line connection. Basically, the connection is:
LPSPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
GND -- GND
Master transmit:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
This is LPSPI master edma transfer completed callback.
Master transmit data complete! Please input any character to continue!
Before you input any character, please make sure the slave board is ready to transmit data.
This is LPSPI master edma transfer completed callback.
LPSPI transfer all data matched!
Master received:
0x01 0x02 0x03 0x04 0x05 0x06 0x07 0x08 0x09 0x0A 0x0B 0x0C 0x0D 0x0E 0x0F 0x10
0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1A 0x1B 0x1C 0x1D 0x1E 0x1F 0x20
0x21 0x22 0x23 0x24 0x25 0x26 0x27 0x28 0x29 0x2A 0x2B 0x2C 0x2D 0x2E 0x2F 0x30
0x31 0x32 0x33 0x34 0x35 0x36 0x37 0x38 0x39 0x3A 0x3B 0x3C 0x3D 0x3E 0x3F 0x40
Press any key to run again