spi_half_duplex_polling_master#
Overview#
The lpc_spi_half_duplex_polling_transfer_master example shows how to use driver API to transfer in half-duplex way.
In this example, one spi instance as master and another spi instance on the othere board as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct. Besides, master will transfer data in polling way.